This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/LAUNCHCC3220MODASF: RTOS/CC3220

Part Number: LAUNCHCC3220MODASF

Tool/software: TI-RTOS

Hi there,

I am using CC3220 launch pad, which has total 4MB space when I have connected this to the uniflash 4.5 version, its showing that only 1.5MB space is available to other files, I want to delete all files which are there and not useful for me. Tell me how I can delete all these files.

Thanks. 

  • Hi Anand,

    With a new UniFlash Image Creator configuration, use the "Simple" view without an MCU Image or ServicePack file specified (even though you will want to set these eventually). Then Connect to the device and select "Burn" -> "Program Image (Create & Program)".

    The tool will format the serial flash and program the minimal set of system files. You should see much closer to the 4MB available after that completes and you reconnect.

    Best Regards,
    Ben M