This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WL1837MOD: if use single antenna solution, ANT1 can support WIFI(2.4G+5G) and Bluetooth at the same time?

Part Number: WL1837MOD

When using WL1837MOD, if I use single antenna solution, does ANT1 can support WIFI(2.4G+5G) and Bluetooth at the same time?

Thanks.

  • Lexy,

    Yes RF_ANT1 supports dual-band WiFi, as well as Bluetooth. However, Please note, WiLink8 does not support WLAN operation on 2.4GHz and on 5GHz at the same time. The option to support operation on 2.4GHz in parallel to 5GHz is by using WiLink8 multi-role which is a TDM solution.

    BR,
    Seong