Is there any guidance available for the CC3220MODA (with an Integral Antenna) keepout? I see 1mm overhang of the module from the edge of a PCB and 6mm keepout of metal based on the CC3220MODA datasheet, 7.3.3 CC3220MODAx RF Recommendations. I wanted to know whether or not any keepouts from the overhanging edge of the CC3220MODA against plastic (such as enclosures) and metal (such as screws) are necessary. I appreciate it if you would provide me with keepouts for both materials (plastic and metal) if they are needed and different.
Thank you.