Tool/software: TI-RTOS
Our new project needs to use CC3220SF. According to CC3220SF LAUNCHXL, we have made a new CC3220SF test board.
It is now impossible to connect the newly made boards using the XDS110 or serial port on the CC3220SF LAUNCHXL with UniFlash4.1.2.1329
The 40M crystal vibration waveform is good, and the measured voltage of the hardware is basically consistent with CC3220SF LAUNCHXL, as follows:
VIN_IO1 | 3.3V |
VIN_IO2 | 3.3V |
VIN_DCDC_DIG | 3.3V |
VIN_DCDC_PA | 3.3V |
VIN_DCDC_ANA | 3.3V |
DCDC_ANA_SW | 1.9V |
VDD_ANA1 | 1.9V |
LDO_IN1 | 1.9V |
LDO_IN2 | 1.9V |
DCDC_PA_OUT | 0V |
VDD_PA_IN | 0V |
DCDC_DIG_SW | 1.2V |
VDD_DIG1 | 1.2V |
VDD_DIG2 | 1.2V |
DCDC_ANA2_SW_P | 1.6V |
DCDC_ANA2_SW_N | 1.6V |
VDD_ANA2 | 3.2V |
VDD_RAN | 1.2V |
VDD_PLL | 0V |