Other Parts Discussed in Thread: UNIFLASH
Hi Experts
I can successfully reprogram the LaunchPad RevA Board with the 'out of the box' example program, using UnitFlash v3.4.1. The programs still works after power off.
In addition, I can successfully load the own program for debugging, using IAR command line and CMake files. But after reseting the MCU the program is lost. I proceeded according this link:
http://dev.ti.com/tirex/explore/content/simplelink_academy_cc32xxsdk_3_10_01_00/modules/wifi/wifi_imagecreator/wifi_imagecreator.html#program-an-image
With the only difference that I selected my own .bin file in the MCU img field. The image can successfully be burned, but nothing works.
Additional Information:
I set the jumpers as described in SWRU463B – February 2017 – Revised August 2018, Figure 11.
I use UniFlash v3.4.1 because the link for v5.0.0 is broken.
Any documentation linked to the UniFlash website below 'Additional Information' is broken.
The 'help' link in UniFlash itself does not work.
The documents I found did not provide the needed information.
I appreciate your help
Htkbwud