Other Parts Discussed in Thread: UNIFLASH
Tool/software: Code Composer Studio
Hello, everybody!
Is it possible programm cc3220sf chip via uart. If there is example?
Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Sorry, I don't understand your question. Do you want to say that you are not able connect by Uniflash software? Please make sure that you have properly set SOP lines. Do you use own hardware or do you use CC3220SF LaunchPad? Please share high-res photo of your connection and jumper configuration.
Additional resources you find at TI Resource explorer - SimpleLink Academy.
Jan
Hi Farid,
Could you outline the steps you are taking to program the device via UART and provide screenshots.
Thanks
Jesu
Hi Jesu !
In order to program the chip through Uart, as I understood, it is enough to use Tx, Rx and Reset. I made my board on ss3220sf to check if xds110 works on the lunchpad board, but when i connected via launchpad to my board the same error. Perhaps i need to change something? I made a board according to the scheme that I sent.
Thank you for help!!!
Hi,
And what about GND. Do you have connected it?
In case you have new board which was not tested yet, it may to be possible that you have a manufacturing or design issue. Maybe you should check DC-DC voltages at for CC3220SF chip and compare with LaunchPad (VSS_ANA = ~1.8V, VDD_DIG = 1.2V). Also you can share schematic and layout of your board.
BTW ... do you use at least four layer board?
Jan