This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Wifi Suggestion

Other Parts Discussed in Thread: CC3235MODS

Hi

  Kindly suggest the wireless module with the following specifications

1. It shall have 10 bit parallel DVP (from 1Megapixel resolution CMOS image sensor) input

2. It shall send live video stream from image sensor in wireless

3. It shall have TCP/IP stack

4. I had checked the CC3235MODS module, but in which the maximum pixel clock frequency is 2 MHz. But image sensor has resolution of upto 1 Megapixel. Hence 2 MHz pixel clock is not sufficient for live video streaming from image sensor. So minimum pixel clock required is 5MHz for 160K resolution and 30 Mhz for 1 Megapixel resolution.

Thanks and regards,

R.Sivasuryan