Part Number: CC3235SF
Other Parts Discussed in Thread: UNIFLASH, CC3220SF, CC3235S, CC3230SF
Hello,
I am facing an error while debugging on our custom boards based on CC3235SF.
I am able to download the program using Uniflash and it runs perfectly.
And I am able to debug the code also after changing the SOP to 2 wire debug.
The trouble comes when I change even a single line of code and try to debug over SWD without programming the device using Uniflash.
Then if I program using Uniflash the updated code I am able to debug it again.
Below are the exact observation during debugging:
After showing some progress during program upload it ends with below error.
This problem I am observing on custom board and not on Launchpad.
The custom board has exactly the same layout and schematics as the launchpad.
Regards