Other Parts Discussed in Thread: WL1831, WL1835
1: Is the firmware the same for WL1831 and WL1835 ?
2: Whats change require if migrating WL1831 to WL1835
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Utsavi,
Utsavi Bharuchwala said:1: Is the firmware the same for WL1831 and WL1835 ?
Yes the FW is same for both
Utsavi Bharuchwala said:2: Whats change require if migrating WL1831 to WL1835
As stated above there is no change required for the FW. In the host SW you will have to create a new configuration based on the device that you are using.
Regards,
Sudharshan K N