Other Parts Discussed in Thread: UNIFLASH
I've been digging into max file sizes for non-secure and secure files on the file system. One thing I noticed is that the file header space for each file is 512 bytes, not 500 as TI documentation claims. Beyond this, it seems like secure files are treated differently (again, no signature). Either there are additional bytes stored with each file or files are saved as fail-safe even if the fail-safe flag is not set (this all I can think of). So, why if I set my maximum file size to be (4096 - 512) bytes is the total space taken up in file system land 8192 bytes?