This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3120MOD: Host UART/SPI baud rate?

Part Number: CC3120MOD

Hello Team,

I need some help understanding the speed's at which an MCU can write to the CC3120mod over UART or SPI to speed out in WIFI ? I see the UART can support up to 3MBps baud rate and SPI is a 20MHz clock so does that mean is 20Mbps? Im unsure on how to evaluate if i can use this module for providing it data at 600kbps  over SPI. It looks like UART is an option but the SPI interface is not very clear to me.