This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WL1837MOD: WL1837MOD EMI FAILING AT 4.8 GZ

Part Number: WL1837MOD
Other Parts Discussed in Thread: WL1837

We have purchased which has WL1837 MOD with+bt The Radiatied emission testes failing as below kindly suggest any update on firmware will reduce this emissions 

7

Radiated Emission/Susceptibility

CISPR 32/IEC 61000-4-3

09-Aug-19

RE failed at 4.8Ghz at margin of -7db@4.8Ghz. RS passed

 which has

  • pls find the results

    Horizontal Results

    Frequency

    Avg

    Limit

    Margin

    MHz

    dBuV/m

    dBuV/m

    dB

    1.125

    30.59

    50

    19.41

    1.584

    27.84

    50

    22.16

    2.331

    44.33

    50

    5.67

    2.41

    81.4

    50

    -31.4

    3.414

    40.3

    54

    13.7

    4.824

    61.33

    54

    -7.33

  • Hi Giridhar,

    Can you tell me what configuration you are testing in? Is this with the host using calibrator? Or is it with RTTT using the RS232 interface?

    Can you please confirm the FW version that you are using? What is your set-up? 1 or 2 antennas? Please follow the wlconfig app note to ensure that you are setting up the radio as required. The app note can be found here:

    Thanks,

    Riz

  • Hi Giridhar,

    I have not heard from you on this issue for over a week. I will go ahead and close the issue for now. If you are still having an issue, please feel free to open up the thread again and provide the requested information.

    Thanks,

    Riz