I've successfully added WL1271 support (v03.00.01.06-WL6.1.6.0) to our custom OMAP 3530 board. Working through the bluetooth capabilities as setup in the release, it doesn't appear that the Serial Port Profile is active. In the file bluetooth/etc/bluetooth/serial.conf it appears there are options to obtain a /dev/ttyX device for SPP support. With that though, I'm not clear on what the required steps are to activate SPP bluetooth support. on the wl1271. Any help/advice would be much appreciated.
Thanks,
Bill Riba