Other Parts Discussed in Thread: CC3135, CC3120, , CC3200
Hi Team SimpleLink WiFi,
For CC3x20/CC3x35.. I see that you can be notified (using a programmable trigger level) of a change in quality/RSSI of the WiFi connection.
According to “CC3x20, CC3x35 SimpleLink™ Wi-Fi® and Internet of Things Network Processor Programmer's Guide” (http://www.ti.com/lit/ug/swru455h/swru455h.pdf ) “4.3.5 RSSI Trigger This feature allows the host to define a trigger that can generate an asynchronous event when there is a change in the conditions and quality level of the active connection. RSSI triggers are supported on all device types with one exception, CC3120 and CC3220 parts support only a single index and CC3135 and CC3235 parts support two indices. In addition, CC3120 and CC3220 parts support RSSI trigger starting from service pack v3.10.0.5. The trigger can be enabled or disabled when needed, and can be updated with new values at runtime.”.
Is this feature available on/for CC3100?
Thanks, Merril