Other Parts Discussed in Thread: UNIFLASH,
Hello,
I am trying to bring-up CC3220SF (actually CC3220MODSF) on a custom board. UART0 of CC3220SF is connected directly to an Atmel D51 MCU which will be the host/master of our device.
So far I was not able to load any code to the CC3220SF. I tried to load code using J-link but it fails to connect to the MCU (I tried SOP=000 and SOP=001). This is I think because my chip is in production mode by default.
I did not find enough lot of details on how to enable develop vs production besides the option in UNIFLASH (5.1.0.2397)
Using UNFLASH as explain in the bring-up guide for CC3220SF launchpad is not possible for me because my board is simply not recognized.
I tried selecting CC3220SF / CC3220SF_SWD / CC3220SF(BOOTLOADER) but the window is very different from 'Image Creator" you can open when selecting the CC3220SF-LAUNCHXL and I am not sure how to generate a valid images that enables developer mode.
1. Is JTAG/SWD access controlled by this devlopper/production mode or only SOP pins ?
2. Is there any way to enable developer without UNIFLASH (using a bootloader command for example) ?
3. Assuming I rework my board to connect a FTDI cable to CC3220 UART0, what would be the action to perform in UNIFLASH to unlock the board and update the service pack ?
Thanks for your help!