Other Parts Discussed in Thread: CC3120
Hello ,
I am trying to make a transmission of 10,000 BYTES, what is the maximum data that I can Transmit in a single packet using CC3120 module and what is the maximum packet size that I can define for both TCP/IP & UDP TX.
In addition, what is the minimum packet size that's to be defined. For example: if i have only 40 BYTES of data to be transmitted, can I define the Packet size of 40 BYTES.
Kindly help me out as I'm new to this.
Thanks