Hi
Our customer has question of APP_EVENT DISCONNECT.
I attach logs.
The both logs offer "Device disconnected from the AP on an ERROR".
In left logs, it succeeds to reset and reboot the system using platform reset.
In right logs, it repeats "Device disconnected from the AP on an ERROR" with 204 and 208 alternately after using platform reset.
I don't know why there are differences between upper two cases.
Could it be possible that there are differences in behavior after platform reset depending on the connecting router?
If yes, could you tell me the router function that will cause to above differences in behavior?
BestRegards