Other Parts Discussed in Thread: WL1835MOD
There is an issue with the test library for WL18 or the WL18 firmware itself. With our firmware booted in PLT mode PLT_ON (Rev 8.9.0.0.79), and with these parameters as per the link below:
“
calibrator wlan0 wl18xx_plt stop_tx
calibrator wlan0 wl18xx_plt tune_channel 1 0 1
calibrator wlan0 wl18xx_plt set_tx_power 20000 0 0 1 0 0 0 1 0 0 0 0
calibrator wlan0 wl18xx_plt start_tx 0 4 500 0 0 1 0 0 00:11:22:33:44:55 01:02:03:04:05:06 0
“
We are not getting 100mW/20dBm (20000 setting), but instead 1mW/0dBm.
Please inform how to set the output power to 100mW/20dBm.
We wasted half a day at the test institute looking for Spurious which was not there, due to this issue.
Changing the 20000 parameter changes the output value correspondingly, but maximum is 20000 and there we only get 1mW/0dBm out of the module.
It seems that you are attenuating the output 20dBm
The module is placed on a DART-MX6Q_800C_2048R_8G_WB_CT_LO_REV1.31A from Variscite.