Other Parts Discussed in Thread: UNIFLASH
Tool/software: Code Composer Studio
Hi,
I am getting the error -102 while communicating with "HTTPS" server. I have attached the CA certificate (let's encrypt).
Please check the code and correct me. The url and host name is given there. I am using the secure method is SL_SO_SEC_METHOD_SSLv3_TLSV1_2 and secure mask is SL_SEC_MASK_SECURE_DEFAULT.
#include <string.h>
// SimpleLink includes
#include "simplelink.h"
// driverlib includes
#include "hw_ints.h"
#include "hw_types.h"
#include "rom.h"
#include "rom_map.h"
#include "prcm.h"
#include "utils.h"
#include "interrupt.h"
// common interface includes
#include "uart_if.h"
#include "common.h"
#include "pinmux.h"
// HTTP Client lib
#include <http/client/httpcli.h>
#include <http/client/common.h>
// JSON Parser
#include "jsmn.h"
#define APPLICATION_VERSION "1.1.1"
#define APP_NAME "HTTPS Client"
#define POST_REQUEST_URI "/api/sessions"
#define POST_DATA "{\n\"email\":\"mohit.tripathi@thethingscloud.com\",\n\"password\":\"things123\"\n}"
#define DELETE_REQUEST_URI "/delete"
#define PUT_REQUEST_URI "/api/sessions"
#define PUT_DATA "PUT request."
#define GET_REQUEST_URI "/api/sessions"
#define HOST_NAME "api2.thingsai.io" //"<host name>"
#define HOST_PORT 443
#define PROXY_IP <proxy_ip>
#define PROXY_PORT <proxy_port>
#define SL_SSL_CA_CERT "/cert/129.der"
#define READ_SIZE 1450
#define MAX_BUFF_SIZE 1460
// Application specific status/error codes
typedef enum{
/* Choosing this number to avoid overlap with host-driver's error codes */
DEVICE_NOT_IN_STATION_MODE = -0x7D0,
DEVICE_START_FAILED = DEVICE_NOT_IN_STATION_MODE - 1,
INVALID_HEX_STRING = DEVICE_START_FAILED - 1,
TCP_RECV_ERROR = INVALID_HEX_STRING - 1,
TCP_SEND_ERROR = TCP_RECV_ERROR - 1,
FILE_NOT_FOUND_ERROR = TCP_SEND_ERROR - 1,
INVALID_SERVER_RESPONSE = FILE_NOT_FOUND_ERROR - 1,
FORMAT_NOT_SUPPORTED = INVALID_SERVER_RESPONSE - 1,
FILE_OPEN_FAILED = FORMAT_NOT_SUPPORTED - 1,
FILE_WRITE_ERROR = FILE_OPEN_FAILED - 1,
INVALID_FILE = FILE_WRITE_ERROR - 1,
SERVER_CONNECTION_FAILED = INVALID_FILE - 1,
GET_HOST_IP_FAILED = SERVER_CONNECTION_FAILED - 1,
STATUS_CODE_MAX = -0xBB8
}e_AppStatusCodes;
//*****************************************************************************
// GLOBAL VARIABLES -- Start
//*****************************************************************************
volatile unsigned long g_ulStatus = 0;//SimpleLink Status
unsigned long g_ulDestinationIP; // IP address of destination server
unsigned long g_ulGatewayIP = 0; //Network Gateway IP address
unsigned char g_ucConnectionSSID[SSID_LEN_MAX+1]; //Connection SSID
unsigned char g_ucConnectionBSSID[BSSID_LEN_MAX]; //Connection BSSID
unsigned char g_buff[MAX_BUFF_SIZE+1];
long bytesReceived = 0; // variable to store the file size
#if defined(ccs) || defined(gcc)
extern void (* const g_pfnVectors[])(void);
#endif
#if defined(ewarm)
extern uVectorEntry __vector_table;
#endif
//*****************************************************************************
// GLOBAL VARIABLES -- End
//*****************************************************************************
//*****************************************************************************
// SimpleLink Asynchronous Event Handlers -- Start
//*****************************************************************************
//*****************************************************************************
//
//! \brief The Function Handles WLAN Events
//!
//! \param[in] pWlanEvent - Pointer to WLAN Event Info
//!
//! \return None
//!
//*****************************************************************************
void SimpleLinkWlanEventHandler(SlWlanEvent_t *pWlanEvent)
{
switch(pWlanEvent->Event)
{
case SL_WLAN_CONNECT_EVENT:
{
SET_STATUS_BIT(g_ulStatus, STATUS_BIT_CONNECTION);
//
// Information about the connected AP (like name, MAC etc) will be
// available in 'slWlanConnectAsyncResponse_t'-Applications
// can use it if required
//
// slWlanConnectAsyncResponse_t *pEventData = NULL;
// pEventData = &pWlanEvent->EventData.STAandP2PModeWlanConnected;
//
// Copy new connection SSID and BSSID to global parameters
memcpy(g_ucConnectionSSID,pWlanEvent->EventData.
STAandP2PModeWlanConnected.ssid_name,
pWlanEvent->EventData.STAandP2PModeWlanConnected.ssid_len);
memcpy(g_ucConnectionBSSID,
pWlanEvent->EventData.STAandP2PModeWlanConnected.bssid,
SL_BSSID_LENGTH);
UART_PRINT("[WLAN EVENT] STA Connected to the AP: %s ,"
" BSSID: %x:%x:%x:%x:%x:%x\n\r",
g_ucConnectionSSID,g_ucConnectionBSSID[0],
g_ucConnectionBSSID[1],g_ucConnectionBSSID[2],
g_ucConnectionBSSID[3],g_ucConnectionBSSID[4],
g_ucConnectionBSSID[5]);
}
break;
case SL_WLAN_DISCONNECT_EVENT:
{
slWlanConnectAsyncResponse_t* pEventData = NULL;
CLR_STATUS_BIT(g_ulStatus, STATUS_BIT_CONNECTION);
CLR_STATUS_BIT(g_ulStatus, STATUS_BIT_IP_AQUIRED);
pEventData = &pWlanEvent->EventData.STAandP2PModeDisconnected;
// If the user has initiated 'Disconnect' request,
//'reason_code' is SL_USER_INITIATED_DISCONNECTION
if(SL_USER_INITIATED_DISCONNECTION == pEventData->reason_code)
{
UART_PRINT("[WLAN EVENT]Device disconnected from the AP: %s,"
"BSSID: %x:%x:%x:%x:%x:%x on application's request \n\r",
g_ucConnectionSSID,g_ucConnectionBSSID[0],
g_ucConnectionBSSID[1],g_ucConnectionBSSID[2],
g_ucConnectionBSSID[3],g_ucConnectionBSSID[4],
g_ucConnectionBSSID[5]);
}
else
{
UART_PRINT("[WLAN ERROR]Device disconnected from the AP AP: %s,"
"BSSID: %x:%x:%x:%x:%x:%x on an ERROR..!! \n\r",
g_ucConnectionSSID,g_ucConnectionBSSID[0],
g_ucConnectionBSSID[1],g_ucConnectionBSSID[2],
g_ucConnectionBSSID[3],g_ucConnectionBSSID[4],
g_ucConnectionBSSID[5]);
}
memset(g_ucConnectionSSID,0,sizeof(g_ucConnectionSSID));
memset(g_ucConnectionBSSID,0,sizeof(g_ucConnectionBSSID));
}
break;
default:
{
UART_PRINT("[WLAN EVENT] Unexpected event [0x%x]\n\r",
pWlanEvent->Event);
}
break;
}
}
//*****************************************************************************
//
//! \brief This function handles network events such as IP acquisition, IP
//! leased, IP released etc.
//!
//! \param[in] pNetAppEvent - Pointer to NetApp Event Info
//!
//! \return None
//!
//*****************************************************************************
void SimpleLinkNetAppEventHandler(SlNetAppEvent_t *pNetAppEvent)
{
switch(pNetAppEvent->Event)
{
case SL_NETAPP_IPV4_IPACQUIRED_EVENT:
{
SlIpV4AcquiredAsync_t *pEventData = NULL;
SET_STATUS_BIT(g_ulStatus, STATUS_BIT_IP_AQUIRED);
//Ip Acquired Event Data
pEventData = &pNetAppEvent->EventData.ipAcquiredV4;
//Gateway IP address
g_ulGatewayIP = pEventData->gateway;
UART_PRINT("[NETAPP EVENT] IP Acquired: IP=%d.%d.%d.%d , "
"Gateway=%d.%d.%d.%d\n\r",
SL_IPV4_BYTE(pNetAppEvent->EventData.ipAcquiredV4.ip,3),
SL_IPV4_BYTE(pNetAppEvent->EventData.ipAcquiredV4.ip,2),
SL_IPV4_BYTE(pNetAppEvent->EventData.ipAcquiredV4.ip,1),
SL_IPV4_BYTE(pNetAppEvent->EventData.ipAcquiredV4.ip,0),
SL_IPV4_BYTE(pNetAppEvent->EventData.ipAcquiredV4.gateway,3),
SL_IPV4_BYTE(pNetAppEvent->EventData.ipAcquiredV4.gateway,2),
SL_IPV4_BYTE(pNetAppEvent->EventData.ipAcquiredV4.gateway,1),
SL_IPV4_BYTE(pNetAppEvent->EventData.ipAcquiredV4.gateway,0));
}
break;
default:
{
UART_PRINT("[NETAPP EVENT] Unexpected event [0x%x] \n\r",
pNetAppEvent->Event);
}
break;
}
}
//*****************************************************************************
//
//! \brief This function handles HTTP server events
//!
//! \param[in] pServerEvent - Contains the relevant event information
//! \param[in] pServerResponse - Should be filled by the user with the
//! relevant response information
//!
//! \return None
//!
//****************************************************************************
void SimpleLinkHttpServerCallback(SlHttpServerEvent_t *pHttpEvent,
SlHttpServerResponse_t *pHttpResponse)
{
// Unused in this application
}
//*****************************************************************************
//
//! \brief This function handles General Events
//!
//! \param[in] pDevEvent - Pointer to General Event Info
//!
//! \return None
//!
//*****************************************************************************
void SimpleLinkGeneralEventHandler(SlDeviceEvent_t *pDevEvent)
{
//
// Most of the general errors are not FATAL are are to be handled
// appropriately by the application
//
UART_PRINT("[GENERAL EVENT] - ID=[%d] Sender=[%d]\n\n",
pDevEvent->EventData.deviceEvent.status,
pDevEvent->EventData.deviceEvent.sender);
}
//*****************************************************************************
//
//! This function handles socket events indication
//!
//! \param[in] pSock - Pointer to Socket Event Info
//!
//! \return None
//!
//*****************************************************************************
void SimpleLinkSockEventHandler(SlSockEvent_t *pSock)
{
//
// This application doesn't work w/ socket - Events are not expected
//
switch( pSock->Event )
{
case SL_SOCKET_TX_FAILED_EVENT:
switch( pSock->socketAsyncEvent.SockTxFailData.status )
{
case SL_ECLOSE:
UART_PRINT("[SOCK ERROR] - close socket (%d) operation "
"failed to transmit all queued packets\n\n",
pSock->socketAsyncEvent.SockAsyncData.sd);
break;
default:
UART_PRINT("[SOCK ERROR] - TX FAILED : socket %d , reason"
"(%d) \n\n",
pSock->socketAsyncEvent.SockAsyncData.sd,
pSock->socketAsyncEvent.SockTxFailData.status);
}
break;
default:
UART_PRINT("[SOCK EVENT] - Unexpected Event [%x0x]\n\n",pSock->Event);
}
}
//*****************************************************************************
// SimpleLink Asynchronous Event Handlers -- End
//*****************************************************************************
//*****************************************************************************
//
//! \brief This function initializes the application variables
//!
//! \param None
//!
//! \return None
//!
//*****************************************************************************
static void InitializeAppVariables()
{
g_ulStatus = 0;
g_ulGatewayIP = 0;
memset(g_ucConnectionSSID,0,sizeof(g_ucConnectionSSID));
memset(g_ucConnectionBSSID,0,sizeof(g_ucConnectionBSSID));
}
//*****************************************************************************
//! \brief This function puts the device in its default state. It:
//! - Set the mode to STATION
//! - Configures connection policy to Auto and AutoSmartConfig
//! - Deletes all the stored profiles
//! - Enables DHCP
//! - Disables Scan policy
//! - Sets Tx power to maximum
//! - Sets power policy to normal
//! - Unregister mDNS services
//! - Remove all filters
//!
//! \param none
//! \return On success, zero is returned. On error, negative is returned
//*****************************************************************************
static long ConfigureSimpleLinkToDefaultState()
{
SlVersionFull ver = {0};
_WlanRxFilterOperationCommandBuff_t RxFilterIdMask = {0};
unsigned char ucVal = 1;
unsigned char ucConfigOpt = 0;
unsigned char ucConfigLen = 0;
unsigned char ucPower = 0;
long lRetVal = -1;
long lMode = -1;
lMode = sl_Start(0, 0, 0);
ASSERT_ON_ERROR(lMode);
// If the device is not in station-mode, try configuring it in station-mode
if (ROLE_STA != lMode)
{
if (ROLE_AP == lMode)
{
// If the device is in AP mode, we need to wait for this event
// before doing anything
while(!IS_IP_ACQUIRED(g_ulStatus))
{
#ifndef SL_PLATFORM_MULTI_THREADED
_SlNonOsMainLoopTask();
#endif
}
}
// Switch to STA role and restart
lRetVal = sl_WlanSetMode(ROLE_STA);
ASSERT_ON_ERROR(lRetVal);
lRetVal = sl_Stop(0xFF);
ASSERT_ON_ERROR(lRetVal);
lRetVal = sl_Start(0, 0, 0);
ASSERT_ON_ERROR(lRetVal);
// Check if the device is in station again
if (ROLE_STA != lRetVal)
{
// We don't want to proceed if the device is not coming up in STA-mode
return DEVICE_NOT_IN_STATION_MODE;
}
}
// Get the device's version-information
ucConfigOpt = SL_DEVICE_GENERAL_VERSION;
ucConfigLen = sizeof(ver);
lRetVal = sl_DevGet(SL_DEVICE_GENERAL_CONFIGURATION, &ucConfigOpt,
&ucConfigLen, (unsigned char *)(&ver));
ASSERT_ON_ERROR(lRetVal);
UART_PRINT("Host Driver Version: %s\n\r",SL_DRIVER_VERSION);
UART_PRINT("Build Version %d.%d.%d.%d.31.%d.%d.%d.%d.%d.%d.%d.%d\n\r",
ver.NwpVersion[0],ver.NwpVersion[1],ver.NwpVersion[2],ver.NwpVersion[3],
ver.ChipFwAndPhyVersion.FwVersion[0],ver.ChipFwAndPhyVersion.FwVersion[1],
ver.ChipFwAndPhyVersion.FwVersion[2],ver.ChipFwAndPhyVersion.FwVersion[3],
ver.ChipFwAndPhyVersion.PhyVersion[0],ver.ChipFwAndPhyVersion.PhyVersion[1],
ver.ChipFwAndPhyVersion.PhyVersion[2],ver.ChipFwAndPhyVersion.PhyVersion[3]);
// Set connection policy to Auto + SmartConfig
// (Device's default connection policy)
lRetVal = sl_WlanPolicySet(SL_POLICY_CONNECTION,
SL_CONNECTION_POLICY(1, 0, 0, 0, 1), NULL, 0);
ASSERT_ON_ERROR(lRetVal);
// Remove all profiles
lRetVal = sl_WlanProfileDel(0xFF);
ASSERT_ON_ERROR(lRetVal);
//
// Device in station-mode. Disconnect previous connection if any
// The function returns 0 if 'Disconnected done', negative number if already
// disconnected Wait for 'disconnection' event if 0 is returned, Ignore
// other return-codes
//
lRetVal = sl_WlanDisconnect();
if(0 == lRetVal)
{
// Wait
while(IS_CONNECTED(g_ulStatus))
{
#ifndef SL_PLATFORM_MULTI_THREADED
_SlNonOsMainLoopTask();
#endif
}
}
// Enable DHCP client
lRetVal = sl_NetCfgSet(SL_IPV4_STA_P2P_CL_DHCP_ENABLE,1,1,&ucVal);
ASSERT_ON_ERROR(lRetVal);
// Disable scan
ucConfigOpt = SL_SCAN_POLICY(0);
lRetVal = sl_WlanPolicySet(SL_POLICY_SCAN , ucConfigOpt, NULL, 0);
ASSERT_ON_ERROR(lRetVal);
// Set Tx power level for station mode
// Number between 0-15, as dB offset from max power - 0 will set max power
ucPower = 0;
lRetVal = sl_WlanSet(SL_WLAN_CFG_GENERAL_PARAM_ID,
WLAN_GENERAL_PARAM_OPT_STA_TX_POWER, 1, (unsigned char *)&ucPower);
ASSERT_ON_ERROR(lRetVal);
// Set PM policy to normal
lRetVal = sl_WlanPolicySet(SL_POLICY_PM , SL_NORMAL_POLICY, NULL, 0);
ASSERT_ON_ERROR(lRetVal);
// Unregister mDNS services
lRetVal = sl_NetAppMDNSUnRegisterService(0, 0);
ASSERT_ON_ERROR(lRetVal);
// Remove all 64 filters (8*8)
memset(RxFilterIdMask.FilterIdMask, 0xFF, 8);
lRetVal = sl_WlanRxFilterSet(SL_REMOVE_RX_FILTER, (_u8 *)&RxFilterIdMask,
sizeof(_WlanRxFilterOperationCommandBuff_t));
ASSERT_ON_ERROR(lRetVal);
lRetVal = sl_Stop(SL_STOP_TIMEOUT);
ASSERT_ON_ERROR(lRetVal);
InitializeAppVariables();
return SUCCESS;
}
//****************************************************************************
//
//! \brief Connecting to a WLAN Accesspoint
//!
//! This function connects to the required AP (SSID_NAME) with Security
//! parameters specified in te form of macros at the top of this file
//!
//! \param Status value
//!
//! \return None
//!
//! \warning If the WLAN connection fails or we don't aquire an IP
//! address, It will be stuck in this function forever.
//
//****************************************************************************
static long WlanConnect()
{
SlSecParams_t secParams = {0};
long lRetVal = 0;
secParams.Key = (signed char *)SECURITY_KEY;
secParams.KeyLen = strlen(SECURITY_KEY);
secParams.Type = SECURITY_TYPE;
lRetVal = sl_WlanConnect((signed char *)SSID_NAME,
strlen((const char *)SSID_NAME), 0, &secParams, 0);
ASSERT_ON_ERROR(lRetVal);
// Wait for WLAN Event
while((!IS_CONNECTED(g_ulStatus)) || (!IS_IP_ACQUIRED(g_ulStatus)))
{
// wait till connects to an AP
_SlNonOsMainLoopTask();
}
return SUCCESS;
}
//*****************************************************************************
//
//! \brief Flush response body.
//!
//! \param[in] httpClient - Pointer to HTTP Client instance
//!
//! \return 0 on success else error code on failure
//!
//*****************************************************************************
static int FlushHTTPResponse(HTTPCli_Handle httpClient)
{
const char *ids[2] = {
HTTPCli_FIELD_NAME_CONNECTION, /* App will get connection header value. all others will skip by lib */
NULL
};
char buf[128];
int id;
int len = 1;
bool moreFlag = 0;
char ** prevRespFilelds = NULL;
/* Store previosly store array if any */
prevRespFilelds = HTTPCli_setResponseFields(httpClient, ids);
/* Read response headers */
while ((id = HTTPCli_getResponseField(httpClient, buf, sizeof(buf), &moreFlag))
!= HTTPCli_FIELD_ID_END)
{
if(id == 0)
{
if(!strncmp(buf, "close", sizeof("close")))
{
UART_PRINT("Connection terminated by server\n\r");
}
}
}
/* Restore previosuly store array if any */
HTTPCli_setResponseFields(httpClient, (const char **)prevRespFilelds);
while(1)
{
/* Read response data/body */
/* Note:
moreFlag will be set to 1 by HTTPCli_readResponseBody() call, if more
data is available Or in other words content length > length of buffer.
The remaining data will be read in subsequent call to HTTPCli_readResponseBody().
Please refer HTTP Client Libary API documenation @ref HTTPCli_readResponseBody
for more information.
*/
HTTPCli_readResponseBody(httpClient, buf, sizeof(buf) - 1, &moreFlag);
ASSERT_ON_ERROR(len);
if ((len - 2) >= 0 && buf[len - 2] == '\r' && buf [len - 1] == '\n'){
break;
}
if(!moreFlag)
{
/* There no more data. break the loop. */
break;
}
}
return 0;
}
//*****************************************************************************
//
//! \brief Handler for parsing JSON data
//!
//! \param[in] ptr - Pointer to http response body data
//!
//! \return 0 on success else error code on failure
//!
//*****************************************************************************
int ParseJSONData(char *ptr)
{
long lRetVal = 0;
int noOfToken;
jsmn_parser parser;
jsmntok_t *tokenList;
/* Initialize JSON PArser */
jsmn_init(&parser);
/* Get number of JSON token in stream as we we dont know how many tokens need to pass */
noOfToken = jsmn_parse(&parser, (const char *)ptr, strlen((const char *)ptr), NULL, 10);
if(noOfToken <= 0)
{
UART_PRINT("Failed to initialize JSON parser\n\r");
return -1;
}
/* Allocate memory to store token */
tokenList = (jsmntok_t *) malloc(noOfToken*sizeof(jsmntok_t));
if(tokenList == NULL)
{
UART_PRINT("Failed to allocate memory\n\r");
return -1;
}
/* Initialize JSON Parser again */
jsmn_init(&parser);
noOfToken = jsmn_parse(&parser, (const char *)ptr, strlen((const char *)ptr), tokenList, noOfToken);
if(noOfToken < 0)
{
UART_PRINT("Failed to parse JSON tokens\n\r");
lRetVal = noOfToken;
}
else
{
UART_PRINT("Successfully parsed %ld JSON tokens\n\r", noOfToken);
}
free(tokenList);
return lRetVal;
}
/*!
\brief This function read respose from server and dump on console
\param[in] httpClient - HTTP Client object
\return 0 on success else -ve
\note
\warning
*/
static int readResponse(HTTPCli_Handle httpClient)
{
long lRetVal = 0;
int bytesRead = 0;
int id = 0;
unsigned long len = 0;
int json = 0;
char *dataBuffer=NULL;
bool moreFlags = 1;
const char *ids[4] = {
HTTPCli_FIELD_NAME_CONTENT_LENGTH,
HTTPCli_FIELD_NAME_CONNECTION,
HTTPCli_FIELD_NAME_CONTENT_TYPE,
NULL
};
/* Read HTTP POST request status code */
lRetVal = HTTPCli_getResponseStatus(httpClient);
if(lRetVal > 0)
{
switch(lRetVal)
{
case 200:
{
UART_PRINT("HTTP Status 200\n\r");
/*
Set response header fields to filter response headers. All
other than set by this call we be skipped by library.
*/
HTTPCli_setResponseFields(httpClient, (const char **)ids);
/* Read filter response header and take appropriate action. */
/* Note:
1. id will be same as index of fileds in filter array setted
in previous HTTPCli_setResponseFields() call.
2. moreFlags will be set to 1 by HTTPCli_getResponseField(), if field
value could not be completely read. A subsequent call to
HTTPCli_getResponseField() will read remaining field value and will
return HTTPCli_FIELD_ID_DUMMY. Please refer HTTP Client Libary API
documenation @ref HTTPCli_getResponseField for more information.
*/
while((id = HTTPCli_getResponseField(httpClient, (char *)g_buff, sizeof(g_buff), &moreFlags))
!= HTTPCli_FIELD_ID_END)
{
switch(id)
{
case 0: /* HTTPCli_FIELD_NAME_CONTENT_LENGTH */
{
len = strtoul((char *)g_buff, NULL, 0);
}
break;
case 1: /* HTTPCli_FIELD_NAME_CONNECTION */
{
}
break;
case 2: /* HTTPCli_FIELD_NAME_CONTENT_TYPE */
{
if(!strncmp((const char *)g_buff, "application/json",
sizeof("application/json")))
{
json = 1;
}
else
{
/* Note:
Developers are advised to use appropriate
content handler. In this example all content
type other than json are treated as plain text.
*/
json = 0;
}
UART_PRINT(HTTPCli_FIELD_NAME_CONTENT_TYPE);
UART_PRINT(" : ");
UART_PRINT("application/json\n\r");
}
break;
default:
{
UART_PRINT("Wrong filter id\n\r");
lRetVal = -1;
goto end;
}
}
}
bytesRead = 0;
if(len > sizeof(g_buff))
{
dataBuffer = (char *) malloc(len);
if(dataBuffer)
{
UART_PRINT("Failed to allocate memory\n\r");
lRetVal = -1;
goto end;
}
}
else
{
dataBuffer = (char *)g_buff;
}
/* Read response data/body */
/* Note:
moreFlag will be set to 1 by HTTPCli_readResponseBody() call, if more
data is available Or in other words content length > length of buffer.
The remaining data will be read in subsequent call to HTTPCli_readResponseBody().
Please refer HTTP Client Libary API documenation @ref HTTPCli_readResponseBody
for more information
*/
bytesRead = HTTPCli_readResponseBody(httpClient, (char *)dataBuffer, len, &moreFlags);
if(bytesRead < 0)
{
UART_PRINT("Failed to received response body\n\r");
lRetVal = bytesRead;
goto end;
}
else if( bytesRead < len || moreFlags)
{
UART_PRINT("Mismatch in content length and received data length\n\r");
goto end;
}
dataBuffer[bytesRead] = '\0';
if(json)
{
/* Parse JSON data */
lRetVal = ParseJSONData(dataBuffer);
if(lRetVal < 0)
{
goto end;
}
}
else
{
/* treating data as a plain text */
}
}
break;
case 404:
UART_PRINT("File not found. \r\n");
/* Handle response body as per requirement.
Note:
Developers are advised to take appopriate action for HTTP
return status code else flush the response body.
In this example we are flushing response body in default
case for all other than 200 HTTP Status code.
*/
default:
/* Note:
Need to flush received buffer explicitly as library will not do
for next request.Apllication is responsible for reading all the
data.
*/
FlushHTTPResponse(httpClient);
break;
}
}
else
{
UART_PRINT("Failed to receive data from server.\r\n");
goto end;
}
lRetVal = 0;
end:
if(len > sizeof(g_buff) && (dataBuffer != NULL))
{
free(dataBuffer);
}
return lRetVal;
}
//*****************************************************************************
//
//! \brief HTTP POST Demonstration
//!
//! \param[in] httpClient - Pointer to http client
//!
//! \return 0 on success else error code on failure
//!
//*****************************************************************************
static int HTTPPostMethod(HTTPCli_Handle httpClient)
{
bool moreFlags = 1;
bool lastFlag = 1;
char tmpBuf[4];
long lRetVal = 0;
HTTPCli_Field fields[4] = {
{HTTPCli_FIELD_NAME_HOST, HOST_NAME},
{HTTPCli_FIELD_NAME_ACCEPT, "*/*"},
{HTTPCli_FIELD_NAME_CONTENT_TYPE, "application/json"},
{NULL, NULL}
};
/* Set request header fields to be send for HTTP request. */
HTTPCli_setRequestFields(httpClient, fields);
/* Send POST method request. */
/* Here we are setting moreFlags = 1 as there are some more header fields need to send
other than setted in previous call HTTPCli_setRequestFields() at later stage.
Please refer HTTP Library API documentaion @ref HTTPCli_sendRequest for more information.
*/
moreFlags = 1;
lRetVal = HTTPCli_sendRequest(httpClient, HTTPCli_METHOD_POST, POST_REQUEST_URI, moreFlags);
if(lRetVal < 0)
{
UART_PRINT("Failed to send HTTP POST request header.\n\r");
return lRetVal;
}
sprintf((char *)tmpBuf, "%d", (sizeof(POST_DATA)-1));
/* Here we are setting lastFlag = 1 as it is last header field.
Please refer HTTP Library API documentaion @ref HTTPCli_sendField for more information.
*/
lastFlag = 1;
lRetVal = HTTPCli_sendField(httpClient, HTTPCli_FIELD_NAME_CONTENT_LENGTH, (const char *)tmpBuf, lastFlag);
if(lRetVal < 0)
{
UART_PRINT("Failed to send HTTP POST request header.\n\r");
return lRetVal;
}
/* Send POST data/body */
lRetVal = HTTPCli_sendRequestBody(httpClient, POST_DATA, (sizeof(POST_DATA)-1));
if(lRetVal < 0)
{
UART_PRINT("Failed to send HTTP POST request body.\n\r");
return lRetVal;
}
lRetVal = readResponse(httpClient);
return lRetVal;
}
//*****************************************************************************
//
//! \brief HTTP DELETE Demonstration
//!
//! \param[in] httpClient - Pointer to http client
//!
//! \return 0 on success else error code on failure
//!
//*****************************************************************************
static int HTTPDeleteMethod(HTTPCli_Handle httpClient)
{
long lRetVal = 0;
HTTPCli_Field fields[3] = {
{HTTPCli_FIELD_NAME_HOST, HOST_NAME},
{HTTPCli_FIELD_NAME_ACCEPT, "*/*"},
{NULL, NULL}
};
bool moreFlags;
/* Set request header fields to be send for HTTP request. */
HTTPCli_setRequestFields(httpClient, fields);
/* Send DELETE method request. */
/* Here we are setting moreFlags = 0 as there are no more header fields need to send
at later stage. Please refer HTTP Library API documentaion @ref HTTPCli_sendRequest
for more information.
*/
moreFlags = 0;
lRetVal = HTTPCli_sendRequest(httpClient, HTTPCli_METHOD_DELETE, DELETE_REQUEST_URI, moreFlags);
if(lRetVal < 0)
{
UART_PRINT("Failed to send HTTP DELETE request header.\n\r");
return lRetVal;
}
lRetVal = readResponse(httpClient);
return lRetVal;
}
//*****************************************************************************
//
//! \brief HTTP PUT Demonstration
//!
//! \param[in] httpClient - Pointer to http client
//!
//! \return 0 on success else error code on failure
//!
//*****************************************************************************
static int HTTPPutMethod(HTTPCli_Handle httpClient)
{
long lRetVal = 0;
HTTPCli_Field fields[4] = {
{HTTPCli_FIELD_NAME_HOST, HOST_NAME},
{HTTPCli_FIELD_NAME_ACCEPT, "*/*"},
{HTTPCli_FIELD_NAME_CONTENT_TYPE, "text/html"},
{NULL, NULL}
};
bool moreFlags = 1;
bool lastFlag = 1;
char tmpBuf[4];
/* Set request header fields to be send for HTTP request. */
HTTPCli_setRequestFields(httpClient, fields);
/* Send PUT method request. */
/* Here we are setting moreFlags = 1 as there are some more header fields need to send
other than setted in previous call HTTPCli_setRequestFields() at later stage.
Please refer HTTP Library API documentaion @ref HTTPCli_sendRequest for more information.
*/
moreFlags = 1;
lRetVal = HTTPCli_sendRequest(httpClient, HTTPCli_METHOD_PUT, PUT_REQUEST_URI, moreFlags);
if(lRetVal < 0)
{
UART_PRINT("Failed to send HTTP PUT request header.\n\r");
return lRetVal;
}
sprintf((char *)tmpBuf, "%d", (sizeof(PUT_DATA)-1));
/* Here we are setting lastFlag = 1 as it is last header field.
Please refer HTTP Library API documentaion @ref HTTPCli_sendField for more information.
*/
lastFlag = 1;
lRetVal = HTTPCli_sendField(httpClient, HTTPCli_FIELD_NAME_CONTENT_LENGTH, (char *)tmpBuf, lastFlag);
if(lRetVal < 0)
{
UART_PRINT("Failed to send HTTP PUT request header.\n\r");
return lRetVal;
}
/* Send PUT data/body */
lRetVal = HTTPCli_sendRequestBody(httpClient, PUT_DATA, (sizeof(PUT_DATA)-1));
if(lRetVal < 0)
{
UART_PRINT("Failed to send HTTP PUT request body.\n\r");
return lRetVal;
}
lRetVal = readResponse(httpClient);
return lRetVal;
}
//*****************************************************************************
//
//! \brief HTTP GET Demonstration
//!
//! \param[in] httpClient - Pointer to http client
//!
//! \return 0 on success else error code on failure
//!
//*****************************************************************************
static int HTTPGetMethod(HTTPCli_Handle httpClient)
{
long lRetVal = 0;
HTTPCli_Field fields[4] = {
{HTTPCli_FIELD_NAME_HOST, HOST_NAME},
{HTTPCli_FIELD_NAME_ACCEPT, "*/*"},
{HTTPCli_FIELD_NAME_CONTENT_LENGTH, "0"},
{NULL, NULL}
};
bool moreFlags;
/* Set request header fields to be send for HTTP request. */
HTTPCli_setRequestFields(httpClient, fields);
/* Send GET method request. */
/* Here we are setting moreFlags = 0 as there are no more header fields need to send
at later stage. Please refer HTTP Library API documentaion @ HTTPCli_sendRequest
for more information.
*/
moreFlags = 0;
lRetVal = HTTPCli_sendRequest(httpClient, HTTPCli_METHOD_GET, GET_REQUEST_URI, moreFlags);
if(lRetVal < 0)
{
UART_PRINT("Failed to send HTTP GET request.\n\r");
return lRetVal;
}
lRetVal = readResponse(httpClient);
return lRetVal;
}
//*****************************************************************************
//
//! Function to connect to AP
//!
//! \param none
//!
//! \return Error-code or SUCCESS
//!
//*****************************************************************************
static long ConnectToAP()
{
long lRetVal = -1;
//
// Following function configure the device to default state by cleaning
// the persistent settings stored in NVMEM (viz. connection profiles &
// policies, power policy etc)
//
// Applications may choose to skip this step if the developer is sure
// that the device is in its desired state at start of applicaton
//
// Note that all profiles and persistent settings that were done on the
// device will be lost
//
lRetVal = ConfigureSimpleLinkToDefaultState();
if(lRetVal < 0)
{
if (DEVICE_NOT_IN_STATION_MODE == lRetVal)
{
UART_PRINT("Failed to configure the device in its default state, "
"Error-code: %d\n\r", DEVICE_NOT_IN_STATION_MODE);
}
return -1;
}
UART_PRINT("Device is configured in default state \n\r");
//
// Assumption is that the device is configured in station mode already
// and it is in its default state
//
lRetVal = sl_Start(0, 0, 0);
if (lRetVal < 0 || ROLE_STA != lRetVal)
{
ASSERT_ON_ERROR(DEVICE_START_FAILED);
}
UART_PRINT("Device started as STATION \n\r");
// Connecting to WLAN AP - Set with static parameters defined at the top
// After this call we will be connected and have IP address
lRetVal = WlanConnect();
UART_PRINT("Connected to the AP: %s\r\n", SSID_NAME);
return 0;
}
//*****************************************************************************
//
//! Function to connect to HTTP server
//!
//! \param httpClient - Pointer to HTTP Client instance
//!
//! \return Error-code or SUCCESS
//**********************************************************
static int ConnectToHTTPServer(HTTPCli_Handle httpClient)
{
long lRetVal = -1;
struct sockaddr_in addr;
SlDateTime_t dt;
struct HTTPCli_SecureParams sparams;
/* Set current Date to validate certificate */
dt.sl_tm_day = 13;
dt.sl_tm_mon = 12;
dt.sl_tm_year = 2019;
dt.sl_tm_hour = 15;
dt.sl_tm_min = 04;
dt.sl_tm_sec = 0;
sl_DevSet(SL_DEVICE_GENERAL_CONFIGURATION,
SL_DEVICE_GENERAL_CONFIGURATION_DATE_TIME,
sizeof(SlDateTime_t), (unsigned char *)(&dt));
#ifdef USE_PROXY
struct sockaddr_in paddr;
paddr.sin_family = AF_INET;
paddr.sin_port = htons(PROXY_PORT);
paddr.sin_addr.s_addr = sl_Htonl(PROXY_IP);
HTTPCli_setProxy((struct sockaddr *)&paddr);
#endif
sparams.method.secureMethod = SL_SO_SEC_METHOD_SSLv3_TLSV1_2;
sparams.mask.secureMask = SL_SEC_MASK_SECURE_DEFAULT;
strncpy(sparams.cafile, SL_SSL_CA_CERT, sizeof(SL_SSL_CA_CERT));
sparams.privkey[0] = 0;
sparams.cert[0] = 0;
sparams.dhkey[0] = 0;
HTTPCli_setSecureParams(&sparams);
/* Resolve HOST NAME/IP */
lRetVal = sl_NetAppDnsGetHostByName((signed char *)HOST_NAME,
strlen((const char *)HOST_NAME),
&g_ulDestinationIP,SL_AF_INET);
if(lRetVal < 0)
{
ASSERT_ON_ERROR(GET_HOST_IP_FAILED);
}
/* Set up the input parameters for HTTP Connection */
addr.sin_family = AF_INET;
addr.sin_port = htons(HOST_PORT);
addr.sin_addr.s_addr = sl_Htonl(g_ulDestinationIP);
/* Testing HTTPCli open call: handle, address params only */
HTTPCli_construct(httpClient);
lRetVal = HTTPCli_connect(httpClient, (struct sockaddr *)&addr, HTTPCli_TYPE_TLS, NULL);
if (lRetVal < 0)
{
UART_PRINT("Connection to server failed. error(%d)\n\r", lRetVal);
ASSERT_ON_ERROR(SERVER_CONNECTION_FAILED);
}
else
{
UART_PRINT("Connection to server created successfully\r\n");
}
return 0;
}
//*****************************************************************************
//
//! Application startup display on UART
//!
//! \param none
//!
//! \return none
//!
//*****************************************************************************
static void
DisplayBanner(char * AppName)
{
UART_PRINT("\n\n\n\r");
UART_PRINT("\t\t *************************************************\n\r");
UART_PRINT("\t\t CC3200 %s Application \n\r", AppName);
UART_PRINT("\t\t *************************************************\n\r");
UART_PRINT("\n\n\n\r");
}
//*****************************************************************************
//
//! Board Initialization & Configuration
//!
//! \param None
//!
//! \return None
//
//*****************************************************************************
static void
BoardInit(void)
{
/* In case of TI-RTOS vector table is initialize by OS itself */
#ifndef USE_TIRTOS
//
// Set vector table base
//
#if defined(ccs) || defined(gcc)
MAP_IntVTableBaseSet((unsigned long)&g_pfnVectors[0]);
#endif
#if defined(ewarm)
MAP_IntVTableBaseSet((unsigned long)&__vector_table);
#endif
#endif
//
// Enable Processor
//
MAP_IntMasterEnable();
MAP_IntEnable(FAULT_SYSTICK);
PRCMCC3200MCUInit();
}
int main()
{
long lRetVal = -1;
HTTPCli_Struct httpClient;
//
// Board Initialization
//
BoardInit();
//
// Configure the pinmux settings for the peripherals exercised
//
PinMuxConfig();
//
// Configuring UART
//
InitTerm();
//
// Display banner
//
DisplayBanner(APP_NAME);
InitializeAppVariables();
lRetVal = ConnectToAP();
if(lRetVal < 0)
{
LOOP_FOREVER();
}
UART_PRINT("post data: %s",POST_DATA);
lRetVal = ConnectToHTTPServer(&httpClient);
if(lRetVal < 0)
{
LOOP_FOREVER();
}
UART_PRINT("\n\r");
UART_PRINT("HTTP Post Begin:\n\r");
lRetVal = HTTPPostMethod(&httpClient);
if(lRetVal < 0)
{
UART_PRINT("HTTP Post failed.\n\r");
}
UART_PRINT("HTTP Post End:\n\r");
UART_PRINT("\n\r");
UART_PRINT("HTTP Delete Begin:\n\r");
lRetVal = HTTPDeleteMethod(&httpClient);
if(lRetVal < 0)
{
UART_PRINT("HTTP Delete failed.\n\r");
}
UART_PRINT("HTTP Delete End:\n\r");
UART_PRINT("\n\r");
UART_PRINT("HTTP Put Begin:\n\r");
lRetVal = HTTPPutMethod(&httpClient);
if(lRetVal < 0)
{
UART_PRINT("HTTP Put failed.\n\r");
}
UART_PRINT("HTTP Put End:\n\r");
UART_PRINT("\n\r");
UART_PRINT("HTTP Get Begin:\n\r");
lRetVal = HTTPGetMethod(&httpClient);
if(lRetVal < 0)
{
UART_PRINT("HTTP Post Get failed.\n\r");
}
UART_PRINT("HTTP Get End:\n\r");
UART_PRINT("\n\r");
// Stop the CC3200 device
LOOP_FOREVER();
}