Other Parts Discussed in Thread: CC3220SF, ENERGIA, CC3220S
Hi,
I am following the adcsinglechannel_CC3220SF_LAUNCHXL_tirtos_ccs example and running it on a Launchpad. I didn't have a 0.1uF Cext as described in the appnote, but I provided a constant 1.1V to ADC1 (pin 60). The connection was made before CC3220SF was reset, and I also increased number of samples from 10 to 30. I would expect some error in the samples, and some sample should be close to 1.1V. However, all samples were around 0.476V. Would it be my device is broken? Or is this some kind of hardware limitation in CC3220SF?
By the way, valid ADC input range is 0V to 1.4V, but the instruction in README.html stated that "For quick testing, connect CONFIG_ADC_0 to GND and CONFIG_ADC_1 to 3V3."
Sample output:
Starting the acdsinglechannel example
ADC0 raw result: 5
ADC1 raw result (0): 1329
ADC0 convert result: 1791 uV
ADC1 convert result (0): 476103 uV
ADC1 raw result (1): 1329
ADC1 convert result (1): 476103 uV
ADC1 raw result (2): 1330
ADC1 convert result (2): 476461 uV
ADC1 raw result (3): 1332
ADC1 convert result (3): 477178 uV
ADC1 raw result (4): 1328
ADC1 convert result (4): 475745 uV
ADC1 raw result (5): 1329
ADC1 convert result (5): 476103 uV
ADC1 raw result (6): 1327
ADC1 convert result (6): 475386 uV
ADC1 raw result (7): 1330
ADC1 convert result (7): 476461 uV
ADC1 raw result (8): 1327
ADC1 convert result (8): 475386 uV
ADC1 raw result (9): 1329
ADC1 convert result (9): 476103 uV
Thanks,
Dennis