Hi,
How we can stop device once I start and configure as access point. I have used sl_Stop(0) to stop it but it not works properly.
My sequence is :-
1. Power ON
2. I have configure device as AP and sl_Start,
3. After this if I want to Off it then I call sl_Stop so it will stop device as AP,
4. But when I power it ON again then after initialization and sl_start it will not stop after calling sl_stop as well.
Can any one help me or share a code in which after configure and sl_start, it was again sl_stop as per user configuration
And will be stopped only till user again wants to start it in AP mode.
Regards,
Mahendra Rana