Hi,
I'm wondering, what are the default and maximum achievable output power levels for Bluetooth LE on the WL1835MOD ?
In the Vendor-Specific HCI Commands document, I've noticed the following lines about default ROM configuration (assuming VBat=3.3V)
#Set BT LE (BLE) HP Vectors Values (note the need to multiply the output power in dBm by '2' Send_HCI_VS_DRPb_Set_Power_Vector 0xFD82, 9, -19.5 *2, -14.5 *2, -9.5 *2, -4.5 *2, 0.5 *2, 5.5 *2, 10.5 *2, 15.5 *2, 0x3F, 0x00FF Send_HCI_VS_DRPb_Set_Class2_Single_Power 0xFD87, 5, 5, 5, 5, 5, 4, 5, 4, 4, 4
If my interpretation is correct, this would mean that by default, BLE Transmit power in HP mode is limited to level 5 which is 5.5 dBm, is that accurate?
The max value seems to be level 7 which is 15.5 dBm, is this achievable ?
Thanks