Hi team,
I successfully flashed OOB demo to CC3220x LaunchPad using guide in SimpleLink Academy. I use simplelink_cc32xx_sdk_3_40_00_05.
I connected to Lanchpad's Access Point and enter http://mysimplelink.net and found OOB - CC32xx site, I push "Start" button I go to TI-OOB Demo page. But this page is not functional: No Device info appeared, I can't control LED, and accelerometers values is 0.
I tried to use iPhone, Android and Windows PC (Firefox) as Station.
Can you please help me to make it works?
There is the log from terminal:
EVENT] IP Acquired: IP=10.123.45.1 , Gateway=10.123.45.1
============================================
out of box Example Ver: 1.00.00.09
============================================
CHIP: 0x30000018
MAC: 2.0.0.0
PHY: 2.2.0.7
NWP: 3.14.0.0
ROM: 0
HOST: 3.0.1.60
MAC address: 98:84:e3:4e:0f:e0
============================================
[Provisioning task] Wake up on Power ON
[NETAPP EVENT] IP Acquired: IP=10.123.45.1 , Gateway=10.123.45.1
[Provisioning task] Device started as STATION
[Provisioning task] Cannot connect to AP or profile does not exist
[Provisioning task] detected device is CC3220RS
[NETAPP EVENT] IP Acquired: IP=10.123.45.1 , Gateway=10.123.45.1
[Provisioning task] Device is configured in default state
[Provisioning task] Device started in AP role
[NETAPP EVENT] IP Acquired: IP=10.123.45.1 , Gateway=10.123.45.1
[Provisioning task] Host Driver Version: 3.0.1.60
[Provisioning task] Build Version 3.14.0.0.31.2.0.0.0.2.2.0.7
[Provisioning task] Starting Provisioning - [Provisioning task] in mode 2 (0 = A
P, 1 = SC, 2 = AP+SC)
[Provisioning task] Provisioning Started. Waiting to be provisioned..!!