Part Number: BOOSTXL-CC3135
Other Parts Discussed in Thread: CC3135, UNIFLASH, CC3120,
Hi TI Support,
I would like to ask some questions about flashing the service pack (or the CC3135 embedded firmware ) of my CC3135 :
- Should I only use the Uniflash tool ? Using UART connectivity ?
- Can I use the Host MCU ( an STM32 in my use case ) to flash the service pack of the CC3135 over the SPI ?
- Can I use the Serial Flash to upgrade the service pack of the CC3135 module ?
I want to update the service pack of the CC3135 using my STM32 microcontroler and it is connected only using SPI interface.
Regards,
Ghada.