I understand that the transmission rate cannot be changed, but Is there any way to limit the disconnection when connecting at a certain transmission rate or less? DSSS 1Mbps DSSS 2 Mbps DSSS 5.5 Mbps DSSS 11Mbps OFDM 6Mbps OFDM 9Mbps OFDM 12Mbps OFDM 18Mbps OFDM 24Mbps OFDM 36Mbps OFDM 48Mbps OFDM 54Mbps MCS 0-7 The module recognizes that it supports the above transmission rates * 1, but This is because even if you connect at 1Mbps or 2Mbps, it will not work properly. (* 1: Regarding the support rate, the description was not found in the data sheet. Please tell us separately if there is any error above.)