Other Parts Discussed in Thread: MSP432P401R, CC31XXEMUBOOST, CC3120, CC3235S, UNIFLASH, CC3220SF
I am making a wifi project using CC3120BOOST and MSP432P401R. In our applcation, we need to make the boards directly communicate with each others and I found out in the CC3120BOOST data sheet that the the Wifi in CC3120BOOST has a mode called wifi Direct that meets my project requirements. I downloaded the SDK for the boost and the MSP and I have several questions:
1. Is there an example that supports the wifi direct mode?
2. is the easiest way to program the CC3120BOOST is by using the CC31XXEMUBOOST?
3. Is there an example for the MSP432P401R that uses SPI protocol in communicating with CC3120BOOST?
4. What is the achieved data rate when I use the wifi direct mode?
UPDATE:
1. I found the network terminal example that includes wlan_cmd.