The original forum question under:
https://e2e.ti.com/support/wireless-connectivity/wifi/f/968/t/887569
is locked.
Was wondering if there was any progress in reproducing or further guidance/information can be provided?
Original question:
We have been using the CC3235S as a Wi-Fi Client to Connect to an Access Point utilizing EAP-TLS (Enterprise Security) with the SDK 3.20.00.06 (28 Jun 2019) without issue.
Upon upgrading the SimpleLink SDK to 3.40.00.05 (30 Jan 2020) we are now receiving the following abort/error information upon attempting to establish a connection (sl_WlanConnect) via the callback "SimpleLinkFatalErrorEventHandler":
[ERROR] - FATAL ERROR: Abort NWP event detected: AbortType=2, AbortData=0x24c (588)
[Note: We have not changed the Application software (MCU image) or the certificates (/sys/cert/ca.der, /sys/cert/client.der, /sys/cert/private.key) only the underlaying SDK bin.]
Thanks,
/David