Other Parts Discussed in Thread: UNIFLASH,
How does uniflash selects the serial (uart) interface which is used for the programming?
An error ocure when connect, see screenshot below.
I connected a FTDI-3v3 converter to the UART1_TX P46) and UART1_RX (P47)
This is the first time I try to program the CC3220MOD.
I connected the SOP1 with 1k pullup to 3v3 and no pull-down. On I/O pin after boot there is now 0.6V, is this okay?
SOP0 and SOP2 are open.