This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3200: 3200

Part Number: CC3200

hello sir

 in cc3200 datasheet,in hibernate mode, the leakage is just 4ua, is the  digital GPIO  leakage included? thanks. 

  • kui feng,

    No, this does not include any GPIO leakage as all I/Os are floating in hibernate mode. However, pin 17 is driven high during hibernate when device is operating in SOP mode "Fn2WJ(Functional mode with a 2-wire SWD mapped to fixed pins)". If this pin is used to connect some other device which has a conflicting drive then there could be current leakage in hibernate mode.

    BR,

    Seong