Part Number: WL1835MOD
Other Parts Discussed in Thread: WL1835,
Hi Team,
Need your help on below request.
Our customer is trying to run the standard BLE packet error tests required by the EU RED. For this test they are R&S CMW500 test instrument.
They have connected the device via a USB to serial cable to the instrument and try run the standard HCI based test using the instruments HCI UART mode (these tests requires using the BT UART to control the DUT). They are manually controlling the enable/disable pin of the device and using the default 115200 bitrate configuration. The instrument is connected directly to the DUT UART. The scope runs the test, but reports none / empty results.
It seems that it is not possible to use a test instrument that does not have a UART supporting hardware flow control as the WL1835 firmware configures its UART in this mode at power-on. Additionally, it seems the test instrument need to support initialization of the WL1835 using the bts file (or the xml equivalent).
Can you pls confirm if the understanding above is correct?
1) If it is a requirement that the test instrument has a UART interface supporting hardware flow control can you advise an instrument that can be used?
2) If test instrument UART hardware flow control support is not needed can you pls provide a quick description of how to get the WL1835 working to run the EU RED BLE tests (the R&S CMW provides a pre-defined test program which does not include the bts initialization of the DUT)?
3) Can you help provide a description of how they can perform the required EU RED BLE tests with a standard test instrument?
Thanks in advance!
Art