This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3220SF-LAUNCHXL: CC31XX/CC32XX Radio Tool v1.0.3.14 Connection error.[error -211]

Part Number: CC3220SF-LAUNCHXL
Other Parts Discussed in Thread: CC2541, CC2530, , CC3220SF

The ZIGBEE CC2530/BLUETOOTH CC2541 can be tested for RF without additional firmware through CC DEBUG/SMART RF STUDIO.
When running CC3220SF-LAUNCHXL/CC31XX/CC32XX Radio Tool v1.0.3.14, the following error message appears:

If you look at SWRA568 5PAGE, 

[The CC3220 program may have a built-in subroutine dedicated to RF testing.]

Why can't connect to the rf tool program?

Do I need other firmware/tool to connect RF TOOL?