Other Parts Discussed in Thread: UNIFLASH
I just got the Development board and downloaded all the SDK stuff. Wanted to put the new Service Pack on and the UniFlash claims that the memory is not writeable.
I try to erase the Flash and UniFlash (V6.0.0.2710) seems happy but the memory is not blank.
since this is all TI product I assume its User Error but cant for the life of figure out what it is. I have been able to run the Demo code that is on the board and attach to both the AP and our WiFi network and run the demo. Seems to be fine but does not support OTA programming.
Here is the output from TeraTerm:
============================================
out of box Example Ver: 1.00.00.09
============================================
CHIP: 0x31100019
MAC: 3.1.0.5
PHY: 3.1.0.17
NWP: 4.1.0.27
ROM: 8738
HOST: 3.0.1.45
MAC address: 34:03:de:11:37:45
============================================
[WLAN EVENT] STA Connected to the AP: 2WIRE339 ,BSSID: 0:21:7c:f1:2c:d1
[NETAPP EVENT] IP Acquired: IP=192.168.1.94 , Gateway=192.168.1.254
[Provisioning task] Connection to AP succeeded
[Provisioning task] IP address is 192.168.1.94
[Provisioning task] detected device is CC323xSF
Wanted to move to the service pack 4.6.0.1
Here is the Console from UniFlash when I try to use the "E:\TI\simplelink_cc32xx_sdk_4_10_00_07\tools\cc32xx_tools\servicepack-cc3x35\sp_4.6.0.1_3.1.0.5_3.1.0.25.bin" file:
But the code still boots on the Tera Term and dumping memory shows NOT all FF.
I have tried different USB cables. Different USB port (note that Terra Term seems to read fine and uniFlash can identify the board), I have tried to use SOP of 100 but uniflash has other issues with that:
Output of console with SOP 100: