This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WL1837MOD: Wi-Fi device is not detected

Part Number: WL1837MOD
Other Parts Discussed in Thread: AM5728, , BEAGLEBOARD-X15, DRA752, TMP102, PMP, WL1271

Hello,

We are testing WL1837MOD evaluation card with AM5728 EVM. When the WiFi card is attached to EVM and system is booted, the card is not detected and system goes in hang state when an ifconfig or any other Wifi related command is given. We have to reboot the system but the problem persists.

Is there any diagnostic application available for resolving this issue?

What could be the possible problem? We have also tried reinserting the WiFi card.

  • Are you using TI processor SDK? Can, you please provide console logs?

    Thanks

  • Hello Hari,

    Yes we are using Ti Linux SDK 6.03. The following is the console log :

    U-Boot SPL 2019.01-g333c3e72d3 (Apr 20 2020 - 05:48:48 +0000)
    DRA752-GP ES2.0
    no pinctrl state for default mode
    Trying to boot from MMC1
    no pinctrl state for default mode
    Loading Environment from FAT... *** Warning - bad CRC, using default environment

    Loading Environment from MMC... OK


    U-Boot 2019.01-g333c3e72d3 (Apr 20 2020 - 05:48:48 +0000)

    CPU  : DRA752-GP ES2.0
    Model: TI AM5728 BeagleBoard-X15
    Board: AM572x EVM REV A.3A
    DRAM:  2 GiB
    MMC:   OMAP SD/MMC: 0, OMAP SD/MMC: 1
    Loading Environment from FAT... *** Warning - bad CRC, using default environment

    Loading Environment from MMC... OK
    Net:
    Warning: ethernet@48484000 using MAC address from ROM
    eth0: ethernet@48484000
    Hit any key to stop autoboot:  2 ^H^H^H 1 ^H^H^H 0
    switch to partitions #0, OK
    mmc0 is current device
    SD/MMC found on device 0
    ** Unable to read file boot.scr **
    1490 bytes read in 1 ms (1.4 MiB/s)
    Loaded env from uEnv.txt
    Importing environment from mmc0 ...
    Running uenvcmd ...
    1 bytes read in 3 ms (0 Bytes/s)
    Already setup.
    switch to partitions #0, OK
    mmc0 is current device
    SD/MMC found on device 0
    4379136 bytes read in 197 ms (21.2 MiB/s)
    135669 bytes read in 8 ms (16.2 MiB/s)
    ## Flattened Device Tree blob at 88000000
       Booting using the fdt blob at 0x88000000
       Loading Device Tree to 8ffdb000, end 8ffff1f4 ... OK

    Starting kernel ...

    [    0.000000] Booting Linux on physical CPU 0x0
    [    0.000000] Linux version 4.19.94-rt39-ga242ccf3f1 (root@dti7de14-014) (gcc version 8.3.0 (GNU Toolchain for the A-profile Architecture 8.3-2019.03 (arm-rel-8.36))) #2 SMP PREEMPT RT Fri Jun 5 16:10:14 IST 2020
    [    0.000000] CPU: ARMv7 Processor [412fc0f2] revision 2 (ARMv7), cr=30c5387d
    [    0.000000] CPU: div instructions available: patching division code
    [    0.000000] CPU: PIPT / VIPT nonaliasing data cache, PIPT instruction cache
    [    0.000000] OF: fdt: Machine model: TI AM5728 EVM
    [    0.000000] Memory policy: Data cache writealloc
    [    0.000000] efi: Getting EFI parameters from FDT:
    [    0.000000] efi: UEFI not found.
    [    0.000000] Reserved memory: created CMA memory pool at 0x0000000095800000, size 56 MiB
    [    0.000000] OF: reserved mem: initialized node ipu2-memory@95800000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created CMA memory pool at 0x0000000099000000, size 64 MiB
    [    0.000000] OF: reserved mem: initialized node dsp1-memory@99000000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x000000009d000000, size 32 MiB
    [    0.000000] OF: reserved mem: initialized node ipu1-memory@9d000000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created CMA memory pool at 0x000000009f000000, size 8 MiB
    [    0.000000] OF: reserved mem: initialized node dsp2-memory@9f000000, compatible id shared-dma-pool
    [    0.000000] cma: Reserved 24 MiB at 0x00000000fe400000
    [    0.000000] OMAP4: Map 0x00000000ffd00000 to (ptrval) for dram barrier
    [    0.000000] DRA752 ES2.0
    [    0.000000] random: get_random_bytes called from start_kernel+0xb0/0x488 with crng_init=0
    [    0.000000] percpu: Embedded 15 pages/cpu s32224 r8192 d21024 u61440
    [    0.000000] Built 1 zonelists, mobility grouping on.  Total pages: 464192
    [    0.000000] Kernel command line: console=ttyS2,115200n8 root=PARTUUID=ffd64fa2-02 rw rootfstype=ext4 rootwait
    [    0.000000] Dentry cache hash table entries: 131072 (order: 8, 1048576 bytes)
    [    0.000000] Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
    [    0.000000] Memory: 1672432K/1863680K available (10240K kernel code, 343K rwdata, 2756K rodata, 2048K init, 276K bss, 35600K reserved, 155648K cma-reserved, 1283072K highmem)
    [    0.000000] Virtual kernel memory layout:
    [    0.000000]     vector  : 0xffff0000 - 0xffff1000   (   4 kB)
    [    0.000000]     fixmap  : 0xffc00000 - 0xfff00000   (3072 kB)
    [    0.000000]     vmalloc : 0xf0800000 - 0xff800000   ( 240 MB)
    [    0.000000]     lowmem  : 0xc0000000 - 0xf0000000   ( 768 MB)
    [    0.000000]     pkmap   : 0xbfe00000 - 0xc0000000   (   2 MB)
    [    0.000000]     modules : 0xbf000000 - 0xbfe00000   (  14 MB)
    [    0.000000]       .text : 0x(ptrval) - 0x(ptrval)   (12256 kB)
    [    0.000000]       .init : 0x(ptrval) - 0x(ptrval)   (2048 kB)
    [    0.000000]       .data : 0x(ptrval) - 0x(ptrval)   ( 344 kB)
    [    0.000000]        .bss : 0x(ptrval) - 0x(ptrval)   ( 277 kB)
    [    0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1
    [    0.000000] rcu: Preemptible hierarchical RCU implementation.
    [    0.000000] rcu:     RCU priority boosting: priority 1 delay 500 ms.
    [    0.000000]  No expedited grace period (rcu_normal_after_boot).
    [    0.000000]  Tasks RCU enabled.
    [    0.000000] NR_IRQS: 16, nr_irqs: 16, preallocated irqs: 16
    [    0.000000] GIC: Using split EOI/Deactivate mode
    [    0.000000] OMAP clockevent source: timer1 at 32786 Hz
    [    0.000000] arch_timer: cp15 timer(s) running at 6.14MHz (phys).
    [    0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x16af5adb9, max_idle_ns: 440795202250 ns
    [    0.000005] sched_clock: 56 bits at 6MHz, resolution 162ns, wraps every 4398046511023ns
    [    0.000012] Switching to timer-based delay loop, resolution 162ns
    [    0.000285] clocksource: 32k_counter: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 58327039986419 ns
    [    0.000288] OMAP clocksource: 32k_counter at 32768 Hz
    [    0.000795] Console: colour dummy device 80x30
    [    0.000936] Calibrating delay loop (skipped), value calculated using timer frequency.. 12.29 BogoMIPS (lpj=61475)
    [    0.000944] pid_max: default: 32768 minimum: 301
    [    0.001083] Mount-cache hash table entries: 2048 (order: 1, 8192 bytes)
    [    0.001092] Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes)
    [    0.001795] CPU: Testing write buffer coherency: ok
    [    0.001828] CPU0: Spectre v2: using ICIALLU workaround
    [    0.002073] /cpus/cpu@0 missing clock-frequency property
    [    0.002110] /cpus/cpu@1 missing clock-frequency property
    [    0.002121] CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
    [    0.059903] Setting up static identity map for 0x80200000 - 0x80200060
    [    0.0 rcu: Hierarchical SRCU implementation.
    [    0.160164] EFI services will not be available.
    [    0.180043] smp: Bringing up secondary CPUs ...
    [    0.320472] CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
    [    0.320476] CPU1: Spectre v2: using ICIALLU workaround
    [    0.320603] smp: Brought up 1 node, 2 CPUs
    [    0.320621] SMP: Total of 2 processors activated (24.59 BogoMIPS).
    [    0.320629] CPU: All CPU(s) started in HYP mode.
    [    0.320636] CPU: Virtualization extensions available.
    [    0.321265] devtmpfs: initialized
    [    0.350435] VFP support v0.3: implementor 41 architecture 4 part 30 variant f rev 0
    [    0.350712] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
    [    0.350732] futex hash table entries: 512 (order: 3, 32768 bytes)
    [    0.353353] pinctrl core: initialized pinctrl subsystem
    [    0.353935] DMI not present or invalid.
    [    0.354281] NET: Registered protocol family 16
    [    0.355600] DMA: preallocated 256 KiB pool for atomic coherent allocations
    [    0.356540] omap_hwmod: l3_main_2 using broken dt data from ocp
    [    0.462803] wkupaon_cm:clk:0068:0: failed to disable
    [    0.575149] OMAP GPIO hardware version 0.1
    [    0.579280] GPIO line 171 (cm-camen-gpio) hogged as output/high
    [    0.603535] hw-breakpoint: found 5 (+1 reserved) breakpoint and 4 watchpoint registers.
    [    0.603547] hw-breakpoint: maximum watchpoint size is 8 bytes.
    [    0.604672] OMAP DMA hardware revision 0.0
    [    0.633191] edma 43300000.edma: memcpy is disabled
    [    0.637222] edma 43300000.edma: TI EDMA DMA engine driver
    [    0.645932] omap-dma-engine 4a056000.dma-controller: OMAP DMA engine driver (LinkedList1/2/3 supported)
    [    0.647338] evm_5v0: supplied by main_12v0
    [    0.647805] com_3v6: supplied by evm_5v0
    [    0.651265] omap-iommu 40d01000.mmu: 40d01000.mmu registered
    [    0.651585] omap-iommu 40d02000.mmu: 40d02000.mmu registered
    [    0.651962] omap-iommu 58882000.mmu: 58882000.mmu registered
    [    0.652354] omap-iommu 55082000.mmu: 55082000.mmu registered
    [    0.652888] omap-iommu 41501000.mmu: 41501000.mmu registered
    [    0.653188] omap-iommu 41502000.mmu: 41502000.mmu registered
    [    0.653482] iommu: Adding device 58820000.ipu to group 1
    [    0.653562] iommu: Adding device 55020000.ipu to group 2
    [    0.653685] iommu: Adding device 40800000.dsp to group 0
    [    0.653909] iommu: Adding device 41000000.dsp to group 3
    [    0.655266] SCSI subsystem initialized
    [    0.656405] palmas 0-0058: Irq flag is 0x00000008
    [    0.682491] palmas 0-0058: Muxing GPIO 2f, PWM 0, LED 0
    [    0.684089] SMPS12: supplied by regulator-dummy
    [    0.685798] SMPS3: supplied by regulator-dummy
    [    0.687490] SMPS45: supplied by regulator-dummy
    [    0.689347] SMPS6: supplied by regulator-dummy
    [    0.690831] SMPS7: supplied by regulator-dummy
    [    0.692271] SMPS8: supplied by regulator-dummy
    [    0.693553] SMPS9: supplied by regulator-dummy
    [    0.694278] LDO1: supplied by regulator-dummy
    [    0.701598] LDO2: supplied by regulator-dummy
    [    0.711348] random: fast init done
    [    0.711496] LDO3: supplied by regulator-dummy
    [    0.721494] LDO4: supplied by regulator-dummy
    [    0.731518] LDO5: supplied by regulator-dummy
    [    0.732237] LDO6: supplied by regulator-dummy
    [    0.732975] LDO7: supplied by regulator-dummy
    [    0.733697] LDO8: supplied by regulator-dummy
    [    0.734439] LDO9: supplied by regulator-dummy
    [    0.741528] LDOLN: supplied by regulator-dummy
    [    0.751557] LDOUSB: supplied by regulator-dummy
    [    0.764194] omap_i2c 48070000.i2c: bus 0 rev0.12 at 400 kHz
    [    0.764842] omap_i2c 48060000.i2c: bus 2 rev0.12 at 400 kHz
    [    0.765570] omap_i2c 4807c000.i2c: bus 4 rev0.12 at 400 kHz
    [    0.765770] media: Linux media interface: v0.10
    [    0.765814] videodev: Linux video capture interface: v2.00
    [    0.765900] pps_core: LinuxPPS API ver. 1 registered
    [    0.765909] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
    [    0.765931] PTP clock support registered
    [    0.765968] EDAC MC: Ver: 3.0.0
    [    0.771615] omap-mailbox 48840000.mailbox: omap mailbox rev 0x400
    [    0.771894] omap-mailbox 48842000.mailbox: omap mailbox rev 0x400
    [    0.772437] Advanced Linux Sound Architecture Driver Initialized.
    [    0.773357] clocksource: Switched to clocksource arch_sys_counter
    [    0.783245] NET: Registered protocol family 2
    [    0.784039] tcp_listen_portaddr_hash hash table entries: 512 (order: 2, 16384 bytes)
    [    0.784079] TCP established hash table entries: 8192 (order: 3, 32768 bytes)
    [    0.784154] TCP bind hash table entries: 8192 (order: 5, 229376 bytes)
    [    0.784387] TCP: Hash tables configured (established 8192 bind 8192)
    [    0.784491] UDP hash table entries: 512 (order: 3, 32768 bytes)
    [    0.784549] UDP-Lite hash table entries: 512 (order: 3, 32768 bytes)
    [    0.784766] NET: Registered protocol family 1
    [    0.785388] RPC: Registered named UNIX socket transport module.
    [    0.785398] RPC: Registered udp transport module.
    [    0.785406] RPC: Registered tcp transport module.
    [    0.785414] RPC: Registered tcp NFSv4.1 backchannel transport module.
    [    0.786573] hw perfevents: no interrupt-affinity property for /pmu, guessing.
    [    0.786802] hw perfevents: enabled with armv7_cortex_a15 PMU driver, 7 counters available
    [    0.787963] Initialise system trusted keyrings
    [    0.788123] workingset: timestamp_bits=14 max_order=19 bucket_order=5
    [    0.794926] squashfs: version 4.0 (2009/01/31) Phillip Lougher
    [    0.795526] NFS: Registering the id_resolver key type
    [    0.795551] Key type id_resolver registered
    [    0.795561] Key type id_legacy registered
    [    0.795608] ntfs: driver 2.1.32 [Flags: R/O].
    [    0.797240] Key type asymmetric registered
    [    0.797253] Asymmetric key parser 'x509' registered
    [    0.797326] bounce: pool size: 64 pages
    [    0.797365] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 245)
    [    0.797376] io scheduler noop registered
    [    0.797385] io scheduler deadline registered
    [    0.797584] io scheduler cfq registered (default)
    [    0.797595] io scheduler mq-deadline registered
    [    0.797604] io scheduler kyber registered
    [    0.803695] pinctrl-single 4a003400.pinmux: 282 pins, size 1128
    [    0.808410] dra7-pcie 51000000.pcie: Linked as a consumer to phy-4a094000.pciephy.1
    [    0.808871] dra7-pcie 51000000.pcie: host bridge /ocp/axi@0/pcie@51000000 ranges:
    [    0.808911] dra7-pcie 51000000.pcie:    IO 0x20003000..0x20012fff -> 0x00000000
    [    0.808938] dra7-pcie 51000000.pcie:   MEM 0x20013000..0x2fffffff -> 0x20013000
    [    1.809203] dra7-pcie 51000000.pcie: Phy link never came up
    [    1.809359] dra7-pcie 51000000.pcie: PCI host bridge to bus 0000:00
    [    1.809375] pci_bus 0000:00: root bus resource [bus 00-ff]
    [    1.809387] pci_bus 0000:00: root bus resource [io  0x0000-0xffff]
    [    1.809397] pci_bus 0000:00: root bus resource [mem 0x20013000-0x2fffffff]
    [    1.816029] PCI: bus0: Fast back to back transfers disabled
    [    1.822148] PCI: bus1: Fast back to back transfers enabled
    [    1.822193] pci 0000:00:00.0: BAR 0: assigned [mem 0x20100000-0x201fffff 64bit]
    [    1.822213] pci 0000:00:00.0: PCI bridge to [bus 01-ff]
    [    1.822709] pcieport 0000:00:00.0: Signaling PME with IRQ 175
    [    1.822955] pcieport 0000:00:00.0: AER enabled with IRQ 175
    [    1.824110] pwm-backlight backlight: backlight supply power not found, using dummy regulator
    [    1.824194] pwm-backlight backlight: Linked as a consumer to regulator.0
    [    1.827874] vdd_3v3: supplied by regen1
    [    1.828129] aic_dvdd_fixed: supplied by vdd_3v3
    [    1.828207] vtt_fixed: supplied by smps3
    [    1.884603] Serial: 8250/16550 driver, 10 ports, IRQ sharing enabled
    [    1.888275] console [ttyS2] disabled
    [    1.888339] 48020000.serial: ttyS2 at MMIO 0x48020000 (irq = 45, base_baud = 3000000) is a 8250
    [    3.002241] console [ttyS2] enabled
    [    3.006631] 48422000.serial: ttyS7 at MMIO 0x48422000 (irq = 46, base_baud = 3000000) is a 8250
    [    3.017729] omap_rng 48090000.rng: Random Number Generator ver. 20
    [    3.018323] random: crng init done
    [    3.028216] omapdss_dss 58000000.dss: Linked as a consumer to regulator.24
    [    3.035346] omapdss_dss 58000000.dss: Dropping the link to regulator.24
    [    3.045463] panel-simple display: display supply power not found, using dummy regulator
    [    3.053581] panel-simple display: Linked as a consumer to regulator.0
    [    3.072877] brd: module loaded
    [    3.083966] loop: module loaded
    [    3.091570] libphy: Fixed MDIO Bus: probed
    [    3.153414] davinci_mdio 48485000.mdio: davinci mdio revision 1.6, bus freq 1000000
    [    3.161109] libphy: 48485000.mdio: probed
    [    3.169385] davinci_mdio 48485000.mdio: phy[1]: device 48485000.mdio:01, driver Micrel KSZ9031 Gigabit PHY
    [    3.179087] davinci_mdio 48485000.mdio: phy[2]: device 48485000.mdio:02, driver Micrel KSZ9031 Gigabit PHY
    [    3.189336] cpsw 48484000.ethernet: Detected MACID = 7c:38:66:7d:90:34
    [    3.195967] cpsw 48484000.ethernet: initialized cpsw ale version 1.4
    [    3.202350] cpsw 48484000.ethernet: ALE Table size 1024
    [    3.207643] cpsw 48484000.ethernet: cpts: overflow check period 500 (jiffies)
    [    3.215798] cpsw 48484000.ethernet: cpsw: Detected MACID = 7c:38:66:7d:90:35
    [    3.224596] i2c /dev entries driver
    [    3.592011] ov1063x 4-0030: ov1063x Product ID a6 Manufacturer ID 35
    [    3.604891] ov1063x 4-0030: ov1063x 4-0030 sensor driver registered !!
    [    3.613958] gpio-fan gpio_fan: GPIO fan initialized
    [    3.620095] tmp102 0-0048: initialized
    [    3.626335] sdhci: Secure Digital Host Controller Interface driver
    [    3.632543] sdhci: Copyright(c) Pierre Ossman
    [    3.637878] sdhci-pltfm: SDHCI platform and OF driver helper
    [    3.644526] omap_gpio 4805d000.gpio: Could not set line 27 debounce to 200000 microseconds (-22)
    [    3.653397] sdhci-omap 4809c000.mmc: Got CD GPIO
    [    3.658279] sdhci-omap 4809c000.mmc: Linked as a consumer to regulator.30
    [    3.665157] sdhci-omap 4809c000.mmc: 4809c000.mmc supply vqmmc not found, using dummy regulator
    [    3.673961] sdhci-omap 4809c000.mmc: Linked as a consumer to regulator.0
    [    3.680768] sdhci-omap 4809c000.mmc: Dropping the link to regulator.0
    [    3.687496] sdhci-omap 4809c000.mmc: Linked as a consumer to regulator.15
    [    3.694519] sdhci-omap 4809c000.mmc: no pinctrl state for ddr_3_3v mode
    [    3.726951] mmc0: SDHCI controller on 4809c000.mmc [4809c000.mmc] using ADMA
    [    3.734794] sdhci-omap 480b4000.mmc: Linked as a consumer to regulator.5
    [    3.741619] sdhci-omap 480b4000.mmc: Dropping the link to regulator.5
    [    3.748216] sdhci-omap 480b4000.mmc: Linked as a consumer to regulator.5
    [    3.780944] mmc1: SDHCI controller on 480b4000.mmc [480b4000.mmc] using ADMA
    [    3.788712] sdhci-omap 480ad000.mmc: Linked as a consumer to regulator.1
    [    3.795542] sdhci-omap 480ad000.mmc: Dropping the link to regulator.1
    [    3.802135] sdhci-omap 480ad000.mmc: Linked as a consumer to regulator.2
    [    3.808957] sdhci-omap 480ad000.mmc: Linked as a consumer to regulator.1
    [    3.815739] sdhci-omap 480ad000.mmc: no pinctrl state for sdr104 mode
    [    3.822242] sdhci-omap 480ad000.mmc: no pinctrl state for ddr50 mode
    [    3.828665] sdhci-omap 480ad000.mmc: no pinctrl state for hs200_1_8v mode
    [    3.843265] mmc0: host does not support reading read-only switch, assuming write-enable
    [    3.857893] mmc0: new high speed SDHC card at address aaaa
    [    3.863410] mmc2: SDHCI controller on 480ad000.mmc [480ad000.mmc] using PIO
    [    3.872502] sdhci-omap 480ad000.mmc: card claims to support voltages below defined range
    [    3.876080] ti-iodelay 4844a000.padconf: Set reg 0x18c Delay(a: 0 g: 120), Elements(C=0 F=2)0x29002
    [    3.876090] ti-iodelay 4844a000.padconf: Set reg 0x190 Delay(a: 0 g: 0), Elements(C=0 F=0)0x29000
    [    3.876099] ti-iodelay 4844a000.padconf: Set reg 0x194 Delay(a: 174 g: 0), Elements(C=0 F=4)0x29004
    [    3.876108] ti-iodelay 4844a000.padconf: Set reg 0x1a4 Delay(a: 265 g: 360), Elements(C=0 F=12)0x2900c
    [    3.876116] ti-iodelay 4844a000.padconf: Set reg 0x1a8 Delay(a: 0 g: 0), Elements(C=0 F=0)0x29000
    [    3.876123] ti-iodelay 4844a000.padconf: Set reg 0x1ac Delay(a: 168 g: 0), Elements(C=0 F=4)0x29004
    [    3.876131] ti-iodelay 4844a000.padconf: Set reg 0x1b0 Delay(a: 0 g: 120), Elements(C=0 F=2)0x29002
    [    3.876139] ti-iodelay 4844a000.padconf: Set reg 0x1b4 Delay(a: 0 g: 0), Elements(C=0 F=0)0x29000
    [    3.876147] ti-iodelay 4844a000.padconf: Set reg 0x1b8 Delay(a: 136 g: 0), Elements(C=0 F=3)0x29003
    [    3.876154] ti-iodelay 4844a000.padconf: Set reg 0x1bc Delay(a: 0 g: 120), Elements(C=0 F=2)0x29002
    [    3.876162] ti-iodelay 4844a000.padconf: Set reg 0x1c0 Delay(a: 0 g: 0), Elements(C=0 F=0)0x29000
    [    3.876170] ti-iodelay 4844a000.padconf: Set reg 0x1c4 Delay(a: 0 g: 0), Elements(C=0 F=0)0x29000
    [    3.876177] ti-iodelay 4844a000.padconf: Set reg 0x1c8 Delay(a: 287 g: 420), Elements(C=0 F=14)0x2900e
    [    3.876185] ti-iodelay 4844a000.padconf: Set reg 0x1d0 Delay(a: 879 g: 0), Elements(C=1 F=9)0x29029
    [    3.876193] ti-iodelay 4844a000.padconf: Set reg 0x1d4 Delay(a: 144 g: 240), Elements(C=0 F=7)0x29007
    [    3.876200] ti-iodelay 4844a000.padconf: Set reg 0x1d8 Delay(a: 0 g: 0), Elements(C=0 F=0)0x29000
    [    3.876208] ti-iodelay 4844a000.padconf: Set reg 0x1dc Delay(a: 0 g: 0), Elements(C=0 F=0)0x29000
    [    3.876215] ti-iodelay 4844a000.padconf: Set reg 0x1e0 Delay(a: 0 g: 0), Elements(C=0 F=0)0x29000
    [    3.876223] ti-iodelay 4844a000.padconf: Set reg 0x1e4 Delay(a: 0 g: 0), Elements(C=0 F=0)0x29000
    [    3.876230] ti-iodelay 4844a000.padconf: Set reg 0x1e8 Delay(a: 34 g: 0), Elements(C=0 F=0)0x29000
    [    3.876238] ti-iodelay 4844a000.padconf: Set reg 0x1ec Delay(a: 0 g: 120), Elements(C=0 F=2)0x29002
    [    3.876245] ti-iodelay 4844a000.padconf: Set reg 0x1f0 Delay(a: 0 g: 0), Elements(C=0 F=0)0x29000
    [    3.876253] ti-iodelay 4844a000.padconf: Set reg 0x1f4 Delay(a: 120 g: 0), Elements(C=0 F=3)0x29003
    [    3.876261] ti-iodelay 4844a000.padconf: Set reg 0x1f8 Delay(a: 120 g: 180), Elements(C=0 F=6)0x29006
    [    3.876268] ti-iodelay 4844a000.padconf: Set reg 0x1fc Delay(a: 0 g: 0), Elements(C=0 F=0)0x29000
    [    3.876276] ti-iodelay 4844a000.padconf: Set reg 0x200 Delay(a: 0 g: 0), Elements(C=0 F=0)0x29000
    [    3.876283] ti-iodelay 4844a000.padconf: Set reg 0x360 Delay(a: 0 g: 0), Elements(C=0 F=0)0x29000
    [    3.876291] ti-iodelay 4844a000.padconf: Set reg 0x364 Delay(a: 0 g: 0), Elements(C=0 F=0)0x29000
    [    3.876298] ti-iodelay 4844a000.padconf: Set reg 0x368 Delay(a: 11 g: 0), Elements(C=0 F=0)0x29000
    [    3.878156] mmcblk0: mmc0:aaaa JULIE 14.8 GiB
    [    3.878434] mmc1: new DDR MMC card at address 0001
    [    3.883218] NET: Registered protocol family 10
    [    3.890519] mmcblk1: mmc1:0001 S10004 3.56 GiB
    [    3.891035] mmcblk1boot0: mmc1:0001 S10004 partition 1 4.00 MiB
    [    3.891544] mmcblk1boot1: mmc1:0001 S10004 partition 2 4.00 MiB
    [    3.891736] mmcblk1rpmb: mmc1:0001 S10004 partition 3 4.00 MiB, chardev (244:0)
    [    3.894538] Segment Routing with IPv6
    [    3.894615] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
    [    3.895224] NET: Registered protocol family 17
    [    3.895502] Key type dns_resolver registered
    [    3.895658] Registering SWP/SWPB emulation handler
    [    3.895664] omap_voltage_late_init: Voltage driver support not added
    [    3.895667] Power Management for TI OMAP4+ devices.
    [    3.896157]  mmcblk0: p1 p2
    [    3.898086] Loading compiled-in X.509 certificates
    [    3.904897]  mmcblk1: p1 p2 p3 p4 p5 p6 p7 p8 p9
    [    3.945252] dmm 4e000000.dmm: workaround for errata i878 in use
    [    3.947417] dmm 4e000000.dmm: initialized all PAT entries
    [    3.948505] omapdss_dss 58000000.dss: Linked as a consumer to regulator.24
    [    3.948717] DSS: OMAP DSS rev 6.1
    [    3.950745] omapdss_hdmi5 58040000.encoder: Linked as a consumer to regulator.18
    [    3.950860] omapdss_hdmi5 58040000.encoder: Dropping the link to regulator.18
    [    3.952622] omapdss_hdmi5 58040000.encoder: Linked as a consumer to regulator.18
    [    3.953071] omapdss_dss 58000000.dss: bound 58001000.dispc (ops dispc_component_ops)
    [    3.953462] omapdss_dss 58000000.dss: bound 58040000.encoder (ops hdmi5_component_ops)
    [    4.314169] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
    [    4.318672] mmc2: new high speed SDIO card at address 0001
    [    4.326322] [drm] No driver support for vblank timestamp query.
    [    4.336399] [drm] Enabling DMM ywrap scrolling
    [    4.344299] Console: switching to colour frame buffer device 100x30
    [    4.353545] omapdrm omapdrm.0: fb0: omapdrm frame buffer device
    [    4.360586] [drm] Initialized omapdrm 1.0.0 20110917 for omapdrm.0 on minor 0
    [    4.369627] input: gpio_keys as /devices/platform/gpio_keys/input/input0
    [    4.376901] hctosys: unable to open rtc device (rtc0)
    [    4.382804] ALSA device list:
    [    4.385810]   No soundcards found.
    [    5.009938] EXT4-fs (mmcblk0p2): recovery complete
    [    5.017506] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
    [    5.025686] VFS: Mounted root (ext4 filesystem) on device 179:2.
    [    5.041893] devtmpfs: mounted
    [    5.046376] Freeing unused kernel memory: 2048K
    [    5.051077] Run /sbin/init as init process
    [    5.343221] systemd[1]: System time before build time, advancing clock.
    [    5.372844] systemd[1]: systemd 239 running in system mode. (+PAM -AUDIT -SELINUX +IMA -APPARMOR +SMACK +SYSVINIT +UTMP -LIBCRYPTSETUP -GCRYPT -GNUTLS +ACL +XZ -LZ4 -SECCOMP +BLKID -ELFUTILS +KMOD -IDN2 -IDN -PCRE2 default-hierarchy=hybrid)
    [    5.394670] systemd[1]: Detected architecture arm.

    Welcome to Arago 2019.11!

    [    5.436268] systemd[1]: Set hostname to <am57xx-evm>.
    [    5.675154] systemd[1]: File /lib/systemd/system/systemd-journald.service:36 configures an IP firewall (IPAddressDeny=any), but the local system does not support BPF/cgroup based firewalling.
    [    5.692285] systemd[1]: Proceeding WITHOUT firewalling in effect! (This warning is only shown for the first loaded unit using IP firewalling.)
    [    5.957355] systemd[1]: Listening on initctl Compatibility Named Pipe.
    [  OK  ] Listening on initctl Compatibility Named Pipe.

    [    6.074392] systemd[1]: Started Dispatch Password Requests to Console Directory Watch.
    [  OK  ] Started Dispatch Password Requests to Console Directory Watch.
    [    6.113923] systemd[1]: Listening on Network Service Netlink Socket.
    [  OK  ] Listening on Network Service Netlink Socket.
    [  OK  ] Listening on Journal Socket.
             Mounting POSIX Message Queue File System...
             Starting Load Kernel Modules...
    [  OK  ] Started Hardware RNG Entropy Gatherer Daemon.
    [    6.274718] cmemk: loading out-of-tree module taints kernel.
    [    6.281705] CMEMK module: reference Linux version 4.19.94
    [    6.287767] allocated heap buffer 0x40500000 of size 0x100000
    [    6.293600] cmemk initialized
    [  OK  ] Listening on udev Control Socket.
    [    6.306715] cryptodev: driver 1.9 loaded.
    [  OK  ] Listening on udev Kernel Socket.
    [  OK  ] Created slice system-serial\x2dgetty.slice.
    [    6.386745] usbcore: registered new interface driver usbfs
    [    6.392340] usbcore: registered new interface driver hub
    [    6.397817] usbcore: registered new device driver usb
    [  OK  ] Created slice User and Session Slice.
    [    6.419169] usbcore: registered new interface driver ftdi_sio
    [    6.425015] usbserial: USB Serial support registered for FTDI USB Serial Device
    [  OK  ] Reached target Slices.
             Starting udev Coldplug all Devices...
    [  OK  ] Created slice system-getty.slice.
             Starting Remount Root and Kernel File Systems...
    [  OK  ] Started Forward Password Requests to Wall Directory Watch.
    [    6.575964] EXT4-fs (mmcblk0p2): re-mounted. Opts: (null)
             Starting Create list of required st…ce nodes for the current kernel...
    [  OK  ] Reached target Paths.
    [  OK  ] Reached target Swap.
             Mounting Temporary Directory (/tmp)...
             Mounting Kernel Debug File System...
    [  OK  ] Listening on Journal Socket (/dev/log).
             Starting Journal Service...
    [  OK  ] Mounted POSIX Message Queue File System.
    [  OK  ] Started Load Kernel Modules.
    [  OK  ] Started Remount Root and Kernel File Systems.
    [  OK  ] Started Create list of required sta…vice nodes for the current kernel.
    [  OK  ] Mounted Temporary Directory (/tmp).
    [  OK  ] Mounted Kernel Debug File System.
             Starting Create Static Device Nodes in /dev...
             Starting Apply Kernel Variables...
             Mounting Kernel Configuration File System...
    [  OK  ] Started Journal Service.
    [  OK  ] Started Create Static Device Nodes in /dev.
    [  OK  ] Started Apply Kernel Variables.
    [  OK  ] Mounted Kernel Configuration File System.
             Starting udev Kernel Device Manager...
    [  OK  ] Reached target Local File Systems (Pre).
    [  OK  ] Reached target Containers.
             Mounting /var/volatile...
             Mounting /media/ram...
             Starting Flush Journal to Persistent Storage...
    [  OK  ] Started udev Kernel Device Manager.
    [  OK  ] Mounted /var/volatile.
    [  OK  ] Mounted /media/ram.
    [    7.744682] systemd-journald[152]: Received request to flush runtime journal from PID 1
             Starting Load/Save Random Seed...
    [  OK  ] Reached target Local File Systems.
    [  OK  ] Started Flush Journal to Persistent Storage.
    [  OK  ] Started Load/Save Random Seed.
             Starting Create Volatile Files and Directories...
    [  OK  ] Started Create Volatile Files and Directories.
             Starting Network Service...
             Starting Update UTMP about System Boot/Shutdown...
             Starting Network Time Synchronization...
    [  OK  ] Started Update UTMP about System Boot/Shutdown.
    [  OK  ] Started Network Service.
             Starting Network Name Resolution...
             Starting Wait for Network to be Configured...
    [    8.587624] omap-rproc 58820000.ipu: ignoring dependency for device, assuming no driver
    [    8.630090] omap-rproc 58820000.ipu: ignoring dependency for device, assuming no driver
    [    8.724631] omap-rproc 58820000.ipu: assigned reserved memory node ipu1-memory@9d000000
    [    8.732804] remoteproc remoteproc0: 58820000.ipu is available
    [  OK  ] Started Network Time Synchronization.
    [  OK  ] Reached target System Time Synchronized.[    8.818007] omap-rproc 55020000.ipu: ignoring dependency for device, assuming no driver

    [    8.832705] omap-rproc 55020000.ipu: ignoring dependency for device, assuming no driver
    [    8.842020] omap-rproc 55020000.ipu: assigned reserved memory node ipu2-memory@95800000
    [    8.867750] remoteproc remoteproc1: 55020000.ipu is available
    [    8.891940] omap-rproc 40800000.dsp: ignoring dependency for device, assuming no driver
    [    8.984829] omap-rproc 40800000.dsp: ignoring dependency for device, assuming no driver
    [    8.992879] omap-rproc 40800000.dsp: assigned reserved memory node dsp1-memory@99000000
    [    9.014252] remoteproc remoteproc2: 40800000.dsp is available
    [    9.032286] omap-rproc 41000000.dsp: ignoring dependency for device, assuming no driver
    [    9.060157] omap-rproc 41000000.dsp: ignoring dependency for device, assuming no driver
    [    9.068876] omap-rproc 41000000.dsp: assigned reserved memory node dsp2-memory@9f000000
    [    9.102410] remoteproc remoteproc3: 41000000.dsp is available
    [  OK  ] Found device /dev/ttyS2.
    [    9.454315] remoteproc remoteproc1: powering up 55020000.ipu
    [    9.460018] remoteproc remoteproc1: Booting fw image dra7-ipu2-fw.xem4, size 3747220
    [    9.481134] remoteproc remoteproc0: powering up 58820000.ipu
    [    9.481150] remoteproc remoteproc0: Booting fw image dra7-ipu1-fw.xem4, size 6887428
    [    9.517506] omap-iommu 55082000.mmu: 55082000.mmu: version 2.1
    [    9.539491] virtio_rpmsg_bus virtio0: rpmsg host is online
    [    9.539768] virtio_rpmsg_bus virtio0: creating channel rpmsg-proto addr 0x3d
    [    9.665311] remoteproc remoteproc0: registered virtio0 (type 7)
    [    9.741525] remoteproc remoteproc0: remote processor 58820000.ipu is now up
    [    9.792455] remoteproc remoteproc2: powering up 40800000.dsp
    [    9.802358] remoteproc remoteproc2: Booting fw image dra7-dsp1-fw.xe66, size 4679976
    [  OK  ] Started Network Name Resolution.
    [    9.828062] remoteproc remoteproc3: powering up 41000000.dsp
    [  OK  ] [    9.835736] remoteproc remoteproc3: Booting fw image dra7-dsp2-fw.xe66, size 4432580
    [    9.862468] omap-iommu 40d01000.mmu: 40d01000.mmu: version 3.0
    Reached target Network.
    [    9.862513] omap-iommu 40d02000.mmu: 40d02000.mmu: version 3.0
    [    9.862959] Error: Driver 'ov1063x' is already registered, aborting...
    [    9.873181] tlv320aic3x-codec 0-0018: Linked as a consumer to regulator.5
    [    9.873912] tlv320aic3x-codec 0-0018: Linked as a consumer to regulator.6
    [    9.929542] rtc-ds1307 2-006f: registered as rtc0
    [    9.988685] Error: Driver 'ov1063x' is already registered, aborting...
    [   10.034742] virtio_rpmsg_bus virtio1: rpmsg host is online
    [   10.034793] remoteproc remoteproc2: registered virtio1 (type 7)
    [   10.034800] remoteproc remoteproc2: remote processor 40800000.dsp is now up
    [   10.034913] virtio_rpmsg_bus virtio1: creating channel rpmsg-proto addr 0x3d
    [   10.085263] Driver for 1-wire Dallas network protocol.
    [   10.143424] omap_hdq 480b2000.1w: OMAP HDQ Hardware Rev 0.:. Driver in Interrupt mode

    [   10.158394] virtio_rpmsg_bus virtio2: rpmsg host is online
    [   10.158457] remoteproc remoteproc1: registered virtio2 (type 7)
    [   10.158471] remoteproc remoteproc1: remote processor 55020000.ipu is now up
    [   10.165960] virtio_rpmsg_bus virtio2: creating channel rpmsg-rpc addr 0x65
    [  OK  ] [   10.226375] omap-iommu 41501000.mmu: 41501000.mmu: version 3.0
    Reached target Host and Network Name Lookups.
    [   10.233107] omap-iommu 41502000.mmu: 41502000.mmu: version 3.0
    [   10.246698] virtio_rpmsg_bus virtio2: creating channel rpmsg-rpc addr 0x66
    [   10.279103] virtio_rpmsg_bus virtio3: rpmsg host is online
    [   10.279356] virtio_rpmsg_bus virtio3: creating channel rpmsg-proto addr 0x3d
    [   10.308230] at24 0-0050: 4096 byte 24c32 EEPROM, writable, 1 bytes/write
    [   10.323155] palmas-rtc 48070000.i2c:tps659038@58:tps659038_rtc: rtc core: registered 48070000.i2c:tps659038@58:tps659038_rtc as rtc1
    [   10.334028] remoteproc remoteproc3: registered virtio3 (type 7)
    [   10.334198] remoteproc remoteproc3: remote processor 41000000.dsp is now up
    [   10.394747] w1_master_driver w1_bus_master1: Attaching one wire slave 01.000000000000 crc 3d
    [   10.401397] w1_master_driver w1_bus_master1: Family 1 for 01.000000000000.3d is not registered.
    [  OK  ] Started udev Coldplug all Devices.
    [   10.476784] omap-des 480a5000.des: OMAP DES hw accel rev: 2.2
    [   10.488141] input: pixcir_tangoc as /devices/platform/44000000.ocp/4807c000.i2c/i2c-4/4-005c/input/input1
    [   10.522287] omap-des 480a5000.des: will run requests pump with realtime priority
    [  OK  ] Reached target System Initialization.
    [  OK  ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket.
    [  OK  ] Started Daily rotation of log files.
    [   10.772082] omap_rtc 48838000.rtc: registered as rtc2
    [  OK  ] Started Daily Cleanup of Temporary Directories.
    [  OK  ] Reached target Timers.
    [   10.864848] net eth0: initializing cpsw version 1.15 (0)
    [   10.884059] vpe 489d0000.vpe: loading firmware vpdma-1b8.bin
    [   10.924617] vpe 489d0000.vpe: Device registered as /dev/video0
    [   10.987252] vip 48990000.vip: loading firmware vpdma-1b8.bin
             Starting Reboot and dump vmcore via kexec...
    [   11.016939] Micrel KSZ9031 Gigabit PHY 48485000.mdio:01: attached PHY driver [Micrel KSZ9031 Gigabit PHY] (mii_bus:phy_addr=48485000.mdio:01, irq=POLL)
    [   11.023441] vip 48990000.vip: VPDMA firmware loaded
    [   11.023544] vin3a: Port A: Using subdev ov1063x 4-0030 for capture
    [   11.023857] vin3a-0: device registered as video1
    [  OK  ] Listening on D-Bus System Message Bus Socket.
    [   11.096768] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
    [  OK  ] Listening on RPCbind Server Activation Socket.
    [  OK  ] Listening on dropbear.socket.
    [  OK  ] Reached target Sockets.
    [  OK  ] Reached target Basic System.
    [   11.320854] net eth1: initializing cpsw version 1.15 (0)
             Starting Lightning Fast Webserver With Light System Requirements...
    [  OK  ] Started Periodic Command Scheduler.
    [  OK  ] Started Job spooling tools.
    [   11.468123] Micrel KSZ9031 Gigabit PHY 48485000.mdio:02: attached PHY driver [Micrel KSZ9031 Gigabit PHY] (mii_bus:phy_addr=48485000.mdio:02, irq=POLL)
             Starting TI MultiCore Tools Daemon...
    [   11.584789] IPv6: ADDRCONF(NETDEV_UP): eth1: link is not ready
             Starting TI IPC Daemon...
             Starting Avahi mDNS/DNS-SD Stack...
             Starting Print notice about GPLv3 packages...
             Starting Enable and configure wl18xx bluetooth stack...
             Starting Permit User Sessions...
             Starting Login Service...
             Starting RPC Bind Service...
    [  OK  ] Started D-Bus System Message Bus.
             Starting Simple Network Management Protocol (SNMP) Daemon....
    [  OK  ] Started Redis In-Memory Data Store.
             Starting rc.pvr.service...

    [  OK  ] Started Reboot and dump vmcore via kexec.
    [  OK  ] Started Lightning Fast Webserver With Light System Requirements.
    [  OK  ] Started TI MultiCore Tools Daemon.
    [  OK  ] Started TI IPC Daemon.
    [  OK  ] Started Permit User Sessions.
    [  OK  ] Started RPC Bind Service.
    [   12.687685] [drm] Initialized pvr 1.17.4948957 20110701 for 56000000.gpu on minor 1
    [   12.859874] PVR_K: UM DDK-(4948957) and KM DDK-(4948957) match. [ OK ]
    [  OK  ] Started rc.pvr.service.
    [   13.484356] phy phy-4a084000.phy.3: Linked as a consumer to regulator.25
    [   13.491492] phy phy-4a085000.phy.4: Linked as a consumer to regulator.25
    [   13.685166] omap-aes 4b500000.aes: OMAP AES hw accel rev: 3.3
    [   13.699960] omap_wdt: OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
    [   13.715561] omap-aes 4b500000.aes: will run requests pump with realtime priority
    [   13.716598] omap-sham 4b101000.sham: hw accel on OMAP rev 4.3
    [   13.790823] omap-aes 4b700000.aes: OMAP AES hw accel rev: 3.3
    [   13.806441] omap-aes 4b700000.aes: will run requests pump with realtime priority
    [   13.972771] omap-hdmi-audio omap-hdmi-audio.0.auto: snd-soc-dummy-dai <-> 58040000.encoder mapping ok
    [   13.983299] omap-hdmi-audio omap-hdmi-audio.0.auto: ASoC: no DMI vendor name!
    [  OK  ] Started Enable and configure wl18xx bluetooth stack.
    [   14.378843] ahci 4a140000.sata: controller can't do 64bit DMA, forcing 32bit
    [   14.393464] ahci 4a140000.sata: forcing port_map 0x0 -> 0x1
    [   14.411615] ahci 4a140000.sata: AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl platform mode
    [   14.420557] asoc-simple-card sound0: tlv320aic3x-hifi <-> 48468000.mcasp mapping ok
    [   14.420593] asoc-simple-card sound0: ASoC: no DMI vendor name!
    [   14.501682] ahci 4a140000.sata: flags: ncq sntf pm led clo only pmp pio slum part ccc apst
    [   14.580722] scsi host0: ahci
    [   14.584463] ata1: SATA max UDMA/133 mmio [mem 0x4a140000-0x4a1410ff] port 0x100 irq 83
    [  OK  ] Started Simple Network Management Protocol (SNMP) Daemon..
    [   14.946036] ata1: SATA link down (SStatus 0 SControl 300)
    [   16.958126] NET: Registered protocol family 45
    [   17.817757] rpmsg_rpc virtio2.rpmsg-rpc.-1.101: probing service dce-callback with src 1024 dst 101
    [   17.862847] rpmsg_rpc virtio2.rpmsg-rpc.-1.101: published functions = 4
    [   17.871791] rpmsg_rpc virtio2.rpmsg-rpc.-1.102: probing service rpmsg-dce with src 1025 dst 102
    [   17.896896] dwc3 48890000.usb: Failed to get clk 'ref': -2
    [   17.903560] rpmsg_rpc virtio2.rpmsg-rpc.-1.102: published functions = 9
    [   17.928085] cfg80211: Loading compiled-in X.509 certificates for regulatory database
    [   17.928090] dwc3 488d0000.usb: Failed to get clk 'ref': -2
    [   18.189524] cfg80211: Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7'
    [   18.583085] wl18xx_driver wl18xx.1.auto: Direct firmware load for ti-connectivity/wl1271-nvs.bin failed with error -2
    [   18.769403] xhci-hcd xhci-hcd.2.auto: xHCI Host Controller
    [   18.782377] xhci-hcd xhci-hcd.2.auto: new USB bus registered, assigned bus number 1
    [   18.789130] remoteproc remoteproc4: 4b234000.pru is available
    [   18.789245] pru-rproc 4b234000.pru: PRU rproc node pru@4b234000 probed successfully
    [   18.816342] remoteproc remoteproc5: 4b238000.pru is available
    [   18.816455] pru-rproc 4b238000.pru: PRU rproc node pru@4b238000 probed successfully
    [   18.854724] remoteproc remoteproc6: 4b2b4000.pru is available
    [   18.854845] pru-rproc 4b2b4000.pru: PRU rproc node pru@4b2b4000 probed successfully
    [   18.886065] remoteproc remoteproc7: 4b2b8000.pru is available
    [   18.886175] pru-rproc 4b2b8000.pru: PRU rproc node pru@4b2b8000 probed successfully
    [   18.976120] xhci-hcd xhci-hcd.2.auto: hcc params 0x0220f04c hci version 0x100 quirks 0x0000000002010010
    [   18.991856] xhci-hcd xhci-hcd.2.auto: irq 193, io mem 0x48890000
    [   19.005990] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002, bcdDevice= 4.19
    [   19.023218] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
    [   19.028291] wlcore: wl18xx HW: 183x or 180x, PG 2.2 (ROM 0x11)
    [   19.053281] usb usb1: Product: xHCI Host Controller
    [   19.064615] usb usb1: Manufacturer: Linux 4.19.94-rt39-ga242ccf3f1 xhci-hcd
    [   19.093312] usb usb1: SerialNumber: xhci-hcd.2.auto
    [   19.118699] wlcore: loaded

    [   19.120185] hub 1-0:1.0: USB hub found
    [   19.120236] hub 1-0:1.0: 1 port detected
    [   19.121801] xhci-hcd xhci-hcd.2.auto: xHCI Host Controller
    [   19.121821] xhci-hcd xhci-hcd.2.auto: new USB bus registered, assigned bus number 2
    [   19.121836] xhci-hcd xhci-hcd.2.auto: Host supports USB 3.0 SuperSpeed
    [   19.121991] usb usb2: We don't know the algorithms for LPM for this host, disabling LPM.
    [   19.122178] usb usb2: New USB device found, idVendor=1d6b, idProduct=0003, bcdDevice= 4.19
    [   19.122186] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
    [   19.122192] usb usb2: Product: xHCI Host Controller
    [   19.122198] usb usb2: Manufacturer: Linux 4.19.94-rt39-ga242ccf3f1 xhci-hcd
    [   19.122204] usb usb2: SerialNumber: xhci-hcd.2.auto
    [   19.135161] hub 2-0:1.0: USB hub found
    [   19.135232] hub 2-0:1.0: 1 port detected
    [   19.483523] usb 1-1: new high-speed USB device number 2 using xhci-hcd
    [   19.664002] usb 1-1: New USB device found, idVendor=0451, idProduct=8142, bcdDevice= 1.00
    [   19.672234] usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=1
    [   19.681052] usb 1-1: SerialNumber: 0F0728410AF3
    [   19.730183] hub 1-1:1.0: USB hub found
    [   19.734421] hub 1-1:1.0: 4 ports detected
    [   19.813674] usb 2-1: new SuperSpeed Gen 1 USB device number 2 using xhci-hcd
    [   19.843914] usb 2-1: New USB device found, idVendor=0451, idProduct=8140, bcdDevice= 1.00
    [   19.854983] usb 2-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
    [   19.906287] hub 2-1:1.0: USB hub found
    [   19.910516] hub 2-1:1.0: 4 ports detected
    [   19.990557] wlcore: PHY firmware version: Rev 8.2.0.0.240
    ***************************************************************
    ***************************************************************
    NOTICE: This file system contains the following GPLv3 packages:
            autoconf
            bash-dev
            bash
            bc
            binutils-dev
            binutils
            bison-dev
            bison
            cifs-utils
            cpio
            cpp-symlinks
            cpp
            dosfstools
            elfutils-dev
            elfutils
            findutils
            g++-symlinks
            g++
            gawk
            gcc-symlinks
            gcc
            gdb
            gdbc6x
            gdbserver
            gettext
            glmark2
            gstreamer1.0-libav
            gzip
            hidapi
            libasm1
            libbfd

            libcairo-perf-utils
            libdw1
            libelf1
            libgdbm-compat4
            libgdbm-dev
            libgdbm6
            libgettextlib
            libgettextsrc
            libgmp10
            libidn2-0
            libmavconn
            libmpc3
            libmpfr6
            libreadline-dev
            libreadline7
            libunistring2
            m4-dev
            m4
            make
            mavlink
            mavros-extras
            mavros-msgs
            mavros
            nettle
            parted
            pdm-anomaly-detection
            socketcan-interface
            swig-dev
            swig
            which

    If you do not wish to distribute GPLv3 components please remove
    the above packages prior to distribution.  This can be done using
    the opkg remove command.  i.e.:
        opkg remove <package>
    Where <package> is the name printed in the list above

    NOTE: If the package is a dependency of another package you
          will be notified of the dependent packages.  You should
          use the --force-removal-of-dependent-packages option to
          also remove the dependent packages as well
    ***************************************************************
    ***************************************************************
    [  OK  ] Started Print notice about GPLv3 packages.
             Starting Save/Restore Sound Card State...
    [  OK  ] Listening on Load/Save RF Kill Switch Status /dev/rfkill Watch.
    [  OK  ] Created slice system-systemd\x2dbacklight.slice.
             Starting Load/Save Screen Backlight…ightness of backlight:backlight...
    [  OK  ] Created slice system-systemd\x2dfsck.slice.
             Starting File System Check on /dev/mmcblk0p1...
             Starting File System Check on /dev/mmcblk1p9...
             Starting File System Check on /dev/mmcblk1p7...
             Starting File System Check on /dev/mmcblk1p8...
             Starting weston.service...
    [  OK  ] Started NFS status monitor for NFSv2/3 locking..
    [  OK  ] Started Getty on tty1.
    [  OK  ] Started Serial Getty on ttyS2.
    [  OK  ] Reached target Login Prompts.
             Starting Synchronize System and HW clocks...
    [  OK  ] Started Save/Restore Sound Card State.
    [  OK  ] Started Load/Save Screen Backlight Brightness of backlight:backlight.
             Starting Load/Save RF Kill Switch Status...
    [  OK  ] Reached target Sound Card.
    [  OK  ] Started Avahi mDNS/DNS-SD Stack.
    [  OK  ] Started Login Service.
    [  OK  ] Started Synchronize System and HW clocks.
    [  OK  ] Started Load/Save RF Kill Switch Status.
    [  OK  ] Started File System Check on /dev/mmcblk0p1.
             Mounting /run/media/mmcblk0p1...
    [  OK  ] Started weston.service.
             Starting Matrix GUI...
    vendor: fsck 0.0% complete...         Starting telnetd.service...
    [  OK  ] Started File System Check on /dev/mmcblk1p9.
    [  OK  ] Mounted /run/media/mmcblk0p1.
    vendor: fsck 35.0% complete...vendor: fsck 76.4% complete...         Mounting /run/media/mmcblk1p9...
    vendor: fsck 97.5% complete...                                [  OK  ] Started File System Check on /dev/mmcblk1p8.
    system: fsck 90.0% complete...         Mounting /run/media/mmcblk1p8...
    system: fsck 97.5% complete...                                [   24.901731] EXT4-fs (mmcblk1p9): Filesystem with quota feature cannot be mounted RDWR without CONFIG_QUOTA
    [  OK  ] Started File System Check on /dev/mmcblk1p7.
    [FAILED] Failed to mount /run/media/mmcblk1p9.
    See 'systemctl status run-media-mmcblk1p9.mount' for details.
    [  OK  ] Started telnetd.service.
    [   25.050807] EXT4-fs (mmcblk1p8): mounted filesystem without journal. Opts: (null)
    [  OK  ] Started Matrix GUI.
    [  OK  ] Mounted /run/media/mmcblk1p8.
             Starting thttpd.service...
             Mounting /run/media/mmcblk1p7...
    [   25.282655] EXT4-fs (mmcblk1p7): mounted filesystem without journal. Opts: (null)
    [  OK  ] Mounted /run/media/mmcblk1p7.

     _____                    _____           _         _
    |  _  |___ ___ ___ ___   |  _  |___ ___  |_|___ ___| |_
    |     |  _| .'| . | . |  |   __|  _| . | | | -_|  _|  _|
    |__|__|_| |__,|_  |___|  |__|  |_| |___|_| |___|___|_|
                  |___|                    |___|

    Arago Project http://arago-project.org am57xx-evm ttyS2

    Arago 2019.11 am57xx-evm ttyS2

    am57xx-evm login: root
    root@am57xx-evm:~# [   41.183353] rcu: INFO: rcu_sched detected stalls on CPUs/tasks:
    [   41.183368] rcu:     1-...!: (2102 ticks this GP) idle=332/1/0x40000000 softirq=0/0 fqs=0
    [   41.183371] rcu:     (detected by 0, t=2102 jiffies, g=1533, q=332)
    [   41.183382] Sending NMI from CPU 0 to CPUs 1:
    [   41.185389] NMI backtrace for cpu 1
    [   41.185393] CPU: 1 PID: 178 Comm: systemd-network Tainted: G           O      4.19.94-rt39-ga242ccf3f1 #2
    [   41.185396] Hardware name: Generic DRA74X (Flattened Device Tree)
    [   41.185398] PC is at hrtimer_active+0x0/0x80
    [   41.185401] LR is at hrtimer_try_to_cancel+0x28/0xc8
    [   41.185403] pc : [<c02a3010>]    lr : [<c02a3df8>]    psr: 600d0113
    [   41.185406] sp : ecc775f8  ip : ecc77620  fp : ecc7761c
    [   41.185408] r10: 24a9e004  r9 : ecc776d0  r8 : c1207488
    [   41.185410] r7 : 00000000  r6 : ecc77648  r5 : c1207488  r4 : ecc77648
    [   41.185413] r3 : facb368e  r2 : 00000001  r1 : 200d0113  r0 : ecc77648
    [   41.185416] Flags: nZCv  IRQs on  FIQs on  Mode SVC_32  ISA ARM  Segment user
    [   41.185418] Control: 30c5387d  Table: ad7d9800  DAC: 55555555
    [   41.185421] CPU: 1 PID: 178 Comm: systemd-network Tainted: G           O      4.19.94-rt39-ga242ccf3f1 #2

    [   41.185424] Hardware name: Generic DRA74X (Flattened Device Tree)
    [   41.185426] Backtrace:
    [   41.185431] [<c020c6a4>] (dump_backtrace) from [<c020c9dc>] (show_stack+0x18/0x1c)
    [   41.185433]  r7:fa212000 r6:600d0193 r5:00000000 r4:c1253ddc
    [   41.185436] [<c020c9c4>] (show_stack) from [<c09f378c>] (dump_stack+0x9c/0xb0)
    [   41.185438] [<c09f36f0>] (dump_stack) from [<c0208dcc>] (show_regs+0x14/0x18)
    [   41.185440]  r7:fa212000 r6:00000001 r5:ecc775a8 r4:00000001
    [   41.185443] [<c0208db8>] (show_regs) from [<c09fa340>] (nmi_cpu_backtrace+0xc0/0xc4)
    [   41.185446] [<c09fa280>] (nmi_cpu_backtrace) from [<c020f03c>] (handle_IPI+0xe0/0x22c)
    [   41.185448]  r5:00000000 r4:c1062c04
    [   41.185451] [<c020ef5c>] (handle_IPI) from [<c0555684>] (gic_handle_irq+0x94/0x98)
    [   41.185453]  r6:fa21200c r5:c122714c r4:c120796c
    [   41.185455] [<c05555f0>] (gic_handle_irq) from [<c02019f8>] (__irq_svc+0x58/0xa0)
    [   41.185458] Exception stack(0xecc775a8 to 0xecc775f0)
    [   41.185461] 75a0:                   ecc77648 200d0113 00000001 facb368e ecc77648 c1207488
    [   41.185463] 75c0: ecc77648 00000000 c1207488 ecc776d0 24a9e004 ecc7761c ecc77620 ecc775f8
    [   41.185466] 75e0: c02a3df8 c02a3010 600d0113 ffffffff
    [   41.185468]  r9:ecc76000 r8:c1207488 r7:ecc775dc r6:ffffffff r5:600d0113 r4:c02a3010
    [   41.185471] [<c02a3dd0>] (hrtimer_try_to_cancel) from [<c02a3ee4>] (hrtimer_cancel+0x1c/0x54)
    [   41.185473]  r6:0000c350 r5:c121ba18 r4:ecc77648
    [   41.185476] [<c02a3ec8>] (hrtimer_cancel) from [<c0a0c3f4>] (schedule_hrtimeout_range_clock+0xdc/0x12c)
    [   41.185478]  r5:00000004 r4:b1a29fbe
    [   41.185481] [<c0a0c318>] (schedule_hrtimeout_range_clock) from [<c0a0c464>] (schedule_hrtimeout_range+0x20/0x28)
    [   41.185484]  r9:00000000 r8:ecc76000 r7:c1207488 r6:ecc776c8 r5:00000000 r4:0000c350
    [   41.185486] [<c0a0c444>] (schedule_hrtimeout_range) from [<c0a0bd04>] (usleep_range+0x70/0x94)
    [   41.185489] [<c0a0bc94>] (usleep_range) from [<c081aeb8>] (sdhci_omap_card_busy+0xa8/0x190)
    [   41.185492]  r8:00000001 r7:00ff0133 r6:ee15f380 r5:00018600 r4:ee15f000
    [   41.185494] [<c081ae10>] (sdhci_omap_card_busy) from [<c07f71b0>] (__mmc_start_request+0xc8/0x10c)
    [   41.185497]  r7:ec334040 r6:ecc777f4 r5:000001f4 r4:ee15f000
    [   41.185499] [<c07f70e8>] (__mmc_start_request) from [<c07f7eb4>] (mmc_start_request+0x8c/0xb0)
    [   41.185502]  r7:ec334040 r6:00000000 r5:ecc777f4 r4:ee15f000
    [   41.185504] [<c07f7e28>] (mmc_start_request) from [<c07f7f44>] (mmc_wait_for_req+0x6c/0xd8)
    [   41.185507]  r7:ec334040 r6:ee15f000 r5:00080000 r4:ecc777f4
    [   41.185510] [<c07f7ed8>] (mmc_wait_for_req) from [<c0803a10>] (mmc_io_rw_extended+0x250/0x30c)
    [   41.185512]  r7:ec334040 r6:c1207488 r5:00080000 r4:ee07b000
    [   41.185515] [<c08037c0>] (mmc_io_rw_extended) from [<c08051f4>] (sdio_io_rw_ext_helper+0x13c/0x1b8)
    [   41.185517]  r10:00000000 r9:000054f0 r8:00000001 r7:ec334044 r6:ede16400 r5:00000000
    [   41.185519]  r4:00000004
    [   41.185522] [<c08050b8>] (sdio_io_rw_ext_helper) from [<c0805294>] (sdio_memcpy_fromio+0x24/0x2c)
    [   41.185525]  r10:00000000 r9:00000004 r8:ec334040 r7:ecd23c10 r6:000054f0 r5:c1207488
    [   41.185526]  r4:ede16400
    [   41.185529] [<c0805270>] (sdio_memcpy_fromio) from [<bf18f3f0>] (wl12xx_sdio_raw_read+0x78/0x150 [wlcore_sdio])
    [   41.185533] [<bf18f378>] (wl12xx_sdio_raw_read [wlcore_sdio]) from [<bf49d5ec>] (wlcore_cmd_send_failsafe+0x3e0/0x4e8 [wlcore])
    [   41.185535]  r10:00000000 r9:ffff92b0 r8:c1205100 r7:ec2b2140 r6:bf18f378 r5:ec334040
    [   41.185537]  r4:ec2b1140
    [   41.185540] [<bf49d20c>] (wlcore_cmd_send_failsafe [wlcore]) from [<bf49ed94>] (wlcore_cmd_configure_failsafe+0x78/0xd0 [wlcore])
    [   41.185543]  r10:ec2b2140 r9:00000000 r8:ec2b1190 r7:bf4b7d00 r6:ec2b2140 r5:00000027
    [   41.185545]  r4:ec2b1140
    [   41.185548] [<bf49ed1c>] (wlcore_cmd_configure_failsafe [wlcore]) from [<bf49ee08>] (wl1271_cmd_configure+0x1c/0x28 [wlcore])
    [   41.185550]  r5:ec334040 r4:ec2b1140
    [   41.185553] [<bf49edec>] (wl1271_cmd_configure [wlcore]) from [<bf4a6798>] (wl1271_acx_init_rx_interrupt+0x94/0xc4 [wlcore])
    [   41.185556] [<bf4a6704>] (wl1271_acx_init_rx_interrupt [wlcore]) from [<bf4a9584>] (wl1271_hw_init+0xbc/0x164 [wlcore])
    [   41.185558]  r5:00000000 r4:ec2b1140
    [   41.185561] [<bf4a94c8>] (wl1271_hw_init [wlcore]) from [<bf49a130>] (wl1271_op_add_interface+0x57c/0x968 [wlcore])
    [   41.185563]  r7:bf4b7d00 r6:c1207488 r5:ec2b1140 r4:00000003
    [   41.185566] [<bf499bb4>] (wl1271_op_add_interface [wlcore]) from [<bf41c438>] (drv_add_interface+0x38/0x80 [mac80211])
    [   41.185569]  r10:00000000 r9:00000001 r8:ed9fd6d8 r7:ed9fd580 r6:ec2b04e0 r5:ed9fd000
    [   41.185571]  r4:ed9fd580
    [   41.185574] [<bf41c400>] (drv_add_interface [mac80211]) from [<bf42fc80>] (ieee80211_do_open+0x474/0x920 [mac80211])

    [   41.185576]  r5:ed9fd000 r4:ed9fd588
    [   41.185579] [<bf42f80c>] (ieee80211_do_open [mac80211]) from [<bf430178>] (ieee80211_open+0x4c/0x58 [mac80211])
    [   41.185581]  r10:00000000 r9:ecd7ba10 r8:ed9fd02c r7:bf463674 r6:00000000 r5:c1207488
    [   41.185583]  r4:ed9fd580
    [   41.185586] [<bf43012c>] (ieee80211_open [mac80211]) from [<c08b5ad0>] (__dev_open+0xd4/0x158)
    [   41.185588]  r5:c1207488 r4:ed9fd000
    [   41.185591] [<c08b59fc>] (__dev_open) from [<c08b5ec8>] (__dev_change_flags+0x16c/0x1cc)
    [   41.185593]  r8:00001002 r7:c1207488 r6:00001003 r5:00000001 r4:ed9fd000
    [   41.185596] [<c08b5d5c>] (__dev_change_flags) from [<c08b5f48>] (dev_change_flags+0x20/0x50)
    [   41.185598]  r9:ecd7ba10 r8:ecc77cfc r7:ed9fd144 r6:00000000 r5:00001002 r4:ed9fd000
    [   41.185601] [<c08b5f28>] (dev_change_flags) from [<c08cbcd4>] (do_setlink+0x2fc/0xa44)
    [   41.185603]  r9:ecd7ba10 r8:ecc77cfc r7:ec4da840 r6:ecc77c2c r5:c1207488 r4:ed9fd000
    [   41.185606] [<c08cb9d8>] (do_setlink) from [<c08cc510>] (rtnl_setlink+0xf4/0x140)
    [   41.185609]  r10:ecd7ba00 r9:ecd7ba10 r8:c124b980 r7:ec4da840 r6:ecc77d9c r5:ecd7ba00
    [   41.185611]  r4:c1207488
    [   41.185613] [<c08cc41c>] (rtnl_setlink) from [<c08c84c8>] (rtnetlink_rcv_msg+0x13c/0x308)
    [   41.185616]  r9:00000000 r8:00000000 r7:ec4da840 r6:c1294f1c r5:c1207488 r4:c08cc41c
    [   41.185619] [<c08c838c>] (rtnetlink_rcv_msg) from [<c08f604c>] (netlink_rcv_skb+0xc0/0x118)
    [   41.185621]  r10:00000000 r9:c1207488 r8:00000038 r7:ecd7ba00 r6:c08c838c r5:c1207488
    [   41.185623]  r4:ec4da840
    [   41.185626] [<c08f5f8c>] (netlink_rcv_skb) from [<c08c8388>] (rtnetlink_rcv+0x18/0x1c)
    [   41.185628]  r8:00000000 r7:ec4da840 r6:00000038 r5:ed9eb800 r4:eea6b000
    [   41.185631] [<c08c8370>] (rtnetlink_rcv) from [<c08f57a8>] (netlink_unicast+0x194/0x210)
    [   41.185634] [<c08f5614>] (netlink_unicast) from [<c08f5aa4>] (netlink_sendmsg+0x1b8/0x3a4)
    [   41.185636]  r9:006000c0 r8:ec4da840 r7:ed9eb800 r6:c1207488 r5:ecc77eb4 r4:00000008
    [   41.185639] [<c08f58ec>] (netlink_sendmsg) from [<c0890708>] (sock_sendmsg+0x1c/0x2c)
    [   41.185641]  r10:00000122 r9:ecc76000 r8:bef1b94c r7:00000000 r6:ee48da00 r5:c1207488
    [   41.185643]  r4:00000000
    [   41.185646] [<c08906ec>] (sock_sendmsg) from [<c0891804>] (__sys_sendto+0xcc/0x10c)
    [   41.185648] [<c0891738>] (__sys_sendto) from [<c0891868>] (sys_sendto+0x24/0x2c)
    [   41.185651]  r8:c0201204 r7:00000122 r6:0049b5c8 r5:00000010 r4:bef1b94c
    [   41.185654] [<c0891844>] (sys_sendto) from [<c0201000>] (ret_fast_syscall+0x0/0x54)
    [   41.185656] Exception stack(0xecc77fa8 to 0xecc77ff0)
    [   41.185659] 7fa0:                   bef1b94c 00000010 00000003 004b0b48 00000038 00000000
    [   41.185661] 7fc0: bef1b94c 00000010 0049b5c8 00000122 0044b215 004ae4b8 00000000 004b0b88
    [   41.185664] 7fe0: 00000000 bef1b928 b6e5e59d b6d66168
    [   41.185676] rcu: rcu_sched kthread starved for 2102 jiffies! g1533 f0x0 RCU_GP_WAIT_FQS(5) ->state=0x402 ->cpu=1
    [   41.185679] rcu: RCU grace-period kthread stack dump:
    [   41.185682] rcu_sched       I    0    12      2 0x00000000
    [   41.185689] Backtrace:
    [   41.185706] [<c0a08be0>] (__schedule) from [<c0a093c8>] (schedule+0x68/0x12c)
    [   41.185714]  r10:00000001 r9:c1205100 r8:c1207488 r7:eed5a740 r6:ee8bdecc r5:ffffe000
    [   41.185717]  r4:ee89dac0
    [   41.185726] [<c0a09360>] (schedule) from [<c0a0bec0>] (schedule_timeout+0x198/0x2e4)
    [   41.185730]  r5:eed5a740 r4:ffff92b2
    [   41.185746] [<c0a0bd28>] (schedule_timeout) from [<c029ac00>] (rcu_gp_kthread+0x59c/0xac0)
    [   41.185752]  r9:c121b380 r8:00000005 r7:c121b558 r6:c1205100 r5:ee8bc000 r4:00000001
    [   41.185763] [<c029a664>] (rcu_gp_kthread) from [<c024c27c>] (kthread+0x160/0x168)
    [   41.185766]  r7:ee8bc000
    [   41.185774] [<c024c11c>] (kthread) from [<c02010e0>] (ret_from_fork+0x14/0x34)
    [   41.185777] Exception stack(0xee8bdfb0 to 0xee8bdff8)
    [   41.185783] dfa0:                                     00000000 00000000 00000000 00000000
    [   41.185788] dfc0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
    [   41.185792] dfe0: 00000000 00000000 00000000 00000000 00000013 00000000
    [   41.185798]  r10:00000000 r9:00000000 r8:00000000 r7:00000000 r6:00000000 r5:c024c11c
    [   41.185801]  r4:ee877200
    [   41.193348] rcu: INFO: rcu_preempt detected stalls on CPUs/tasks:
    [   41.193355] rcu:     Tasks blocked on level-0 rcu_node (CPUs 0-1): P23
    [   41.193361] rcu:     (detected by 1, t=2102 jiffies, g=1529, q=240165)

    [   41.193370] ktimersoftd/1   R  running task        0    23      2 0x00000000
    [   41.193378] Backtrace:
    [   41.193392] [<c0a08be0>] (__schedule) from [<c0a094bc>] (preempt_schedule_common+0x30/0x60)
    [   41.193398]  r10:00000000 r9:eed5d080 r8:ee165034 r7:c1207488 r6:00000001 r5:00000001
    [   41.193401]  r4:ffffe000
    [   41.193411] [<c0a0948c>] (preempt_schedule_common) from [<c0a09544>] (preempt_schedule+0x58/0x5c)
    [   41.193415]  r5:00000001 r4:ee164a40
    [   41.193424] [<c0a094ec>] (preempt_schedule) from [<c0a0ccf8>] (_raw_spin_unlock_irqrestore+0x58/0x70)
    [   41.193439] [<c0a0cca0>] (_raw_spin_unlock_irqrestore) from [<c0255e98>] (try_to_wake_up+0x298/0x5d4)
    [   41.193448] [<c0255c00>] (try_to_wake_up) from [<c02561ec>] (wake_up_process+0x18/0x1c)
    [   41.193454]  r10:600d0113 r9:c02a3da0 r8:00000000 r7:eed5b840 r6:eed5b8e0 r5:ecc77648
    [   41.193457]  r4:eed5b938
    [   41.193468] [<c02561d4>] (wake_up_process) from [<c02a3dc8>] (hrtimer_wakeup+0x28/0x30)
    [   41.193476] [<c02a3da0>] (hrtimer_wakeup) from [<c02a4084>] (__hrtimer_run_queues+0x168/0x220)
    [   41.193485] [<c02a3f1c>] (__hrtimer_run_queues) from [<c02a41c4>] (hrtimer_run_softirq+0x88/0xbc)
    [   41.193491]  r10:00000008 r9:c105c464 r8:00000000 r7:eed5b9b0 r6:600d0113 r5:eed5b860
    [   41.193493]  r4:eed5b840
    [   41.193504] [<c02a413c>] (hrtimer_run_softirq) from [<c0231cf4>] (do_current_softirqs+0x200/0x2ac)
    [   41.193509]  r7:04208140 r6:00000020 r5:ffffe000 r4:c105c41c
    [   41.193516] [<c0231af4>] (do_current_softirqs) from [<c0231dd4>] (run_ksoftirqd+0x34/0x54)
    [   41.193522]  r10:00000000 r9:00000000 r8:c1207488 r7:c12174f0 r6:00000001 r5:ee877740
    [   41.193525]  r4:ffffe000
    [   41.193532] [<c0231da0>] (run_ksoftirqd) from [<c02504ac>] (smpboot_thread_fn+0x2d4/0x320)
    [   41.193536]  r5:ee877740 r4:ffffe000
    [   41.193544] [<c02501d8>] (smpboot_thread_fn) from [<c024c27c>] (kthread+0x160/0x168)
    [   41.193550]  r10:ee88fdac r9:c02501d8 r8:ee877740 r7:ee8e0000 r6:00000000 r5:ee8777c0
    [   41.193553]  r4:ee877800
    [   41.193560] [<c024c11c>] (kthread) from [<c02010e0>] (ret_from_fork+0x14/0x34)
    [   41.193564] Exception stack(0xee8e1fb0 to 0xee8e1ff8)
    [   41.193569] 1fa0:                                     00000000 00000000 00000000 00000000
    [   41.193574] 1fc0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
    [   41.193579] 1fe0: 00000000 00000000 00000000 00000000 00000013 00000000
    [   41.193585]  r10:00000000 r9:00000000 r8:00000000 r7:00000000 r6:00000000 r5:c024c11c
    [   41.193588]  r4:ee8777c0
    [   41.193592] ktimersoftd/1   R  running task        0    23      2 0x00000000
    [   41.193600] Backtrace:
    [   41.193612] [<c0a08be0>] (__schedule) from [<c0a094bc>] (preempt_schedule_common+0x30/0x60)
    [   41.193617]  r10:00000000 r9:eed5d080 r8:ee165034 r7:c1207488 r6:00000001 r5:00000001
    [   41.193620]  r4:ffffe000
    [   41.193630] [<c0a0948c>] (preempt_schedule_common) from [<c0a09544>] (preempt_schedule+0x58/0x5c)
    [   41.193633]  r5:00000001 r4:ee164a40
    [   41.193642] [<c0a094ec>] (preempt_schedule) from [<c0a0ccf8>] (_raw_spin_unlock_irqrestore+0x58/0x70)
    [   41.193650] [<c0a0cca0>] (_raw_spin_unlock_irqrestore) from [<c0255e98>] (try_to_wake_up+0x298/0x5d4)
    [   41.193659] [<c0255c00>] (try_to_wake_up) from [<c02561ec>] (wake_up_process+0x18/0x1c)
    [   41.193664]  r10:600d0113 r9:c02a3da0 r8:00000000 r7:eed5b840 r6:eed5b8e0 r5:ecc77648
    [   41.193668]  r4:eed5b938
    [   41.193677] [<c02561d4>] (wake_up_process) from [<c02a3dc8>] (hrtimer_wakeup+0x28/0x30)
    [   41.193685] [<c02a3da0>] (hrtimer_wakeup) from [<c02a4084>] (__hrtimer_run_queues+0x168/0x220)
    [   41.193694] [<c02a3f1c>] (__hrtimer_run_queues) from [<c02a41c4>] (hrtimer_run_softirq+0x88/0xbc)
    [   41.193699]  r10:00000008 r9:c105c464 r8:00000000 r7:eed5b9b0 r6:600d0113 r5:eed5b860
    [   41.193702]  r4:eed5b840
    [   41.193710] [<c02a413c>] (hrtimer_run_softirq) from [<c0231cf4>] (do_current_softirqs+0x200/0x2ac)
    [   41.193715]  r7:04208140 r6:00000020 r5:ffffe000 r4:c105c41c
    [   41.193723] [<c0231af4>] (do_current_softirqs) from [<c0231dd4>] (run_ksoftirqd+0x34/0x54)
    [   41.193728]  r10:00000000 r9:00000000 r8:c1207488 r7:c12174f0 r6:00000001 r5:ee877740
    [   41.193731]  r4:ffffe000
    [   41.193738] [<c0231da0>] (run_ksoftirqd) from [<c02504ac>] (smpboot_thread_fn+0x2d4/0x320)
    [   41.193741]  r5:ee877740 r4:ffffe000
    [   41.193748] [<c02501d8>] (smpboot_thread_fn) from [<c024c27c>] (kthread+0x160/0x168)
    [   41.193754]  r10:ee88fdac r9:c02501d8 r8:ee877740 r7:ee8e0000 r6:00000000 r5:ee8777c0
    [   41.193757]  r4:ee877800
    [   41.193764] [<c024c11c>] (kthread) from [<c02010e0>] (ret_from_fork+0x14/0x34)
    [   41.193768] Exception stack(0xee8e1fb0 to 0xee8e1ff8)
    [   41.193772] 1fa0:                                     00000000 00000000 00000000 00000000
    [   41.193777] 1fc0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
    [   41.193781] 1fe0: 00000000 00000000 00000000 00000000 00000013 00000000
    [   41.193787]  r10:00000000 r9:00000000 r8:00000000 r7:00000000 r6:00000000 r5:c024c11c
    [   41.193790]  r4:ee8777c0
    [   42.093350] sched: RT throttling activated
    i^H ^H^G^G
    root@am57xx-evm:~#
    root@am57xx-evm:~#
    root@am57xx-evm:~#










  • Is this with RT linux? If so, did you try with non RT linux for a test?

    Thanks