Other Parts Discussed in Thread: UNIFLASH
Using THE PEAP function of CC3235, the routing and RADIUS server have been configured and the mobile phone can use EAP method to connect the routing + RADIUS, but the same parameters as the mobile phone wifi send AT instruction AT+WlanConnect=" TP-link_6034 ", WPA_ENT,test, LKZ, LKZ,PEAP0_MSCHAPv2 but not connected, prompt missing certificate, does the WIFI use PEAP function must use a certificate