This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3120: CC3120: Access Web interface (WiFi AP) on Mac OS

Part Number: CC3120
Other Parts Discussed in Thread: UNIFLASH

Hello,

I am not able to run JavaScript from my web interface (WiFi AP CC3120) in Apple's environment (macOS and iOS).

Following are screenshots of the problem:

Safari version: 13.1.1

macOS Catalina 10.15.5

Uniflash Project:


teste-http_200706002158.zip

The same project works on Windows and Linux.

However, if I use the standard CC3120 provisioning project, the problem does not occur. It only happens when I record my project.

Seria algum parámetro de configuração ou gravação do projeto?