This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WL1837MOD: Linux

Part Number: WL1837MOD

hi :

I tried to turn on 5g AP on Linux. I've updated the latest WiFi driver processors.wiki.ti.com/.../WiLink8_ Linux_ Getting_ Started_ Guide, but when I start 5g AP, I need to start hostapd twice to start 5g AP successfully. When I am in the microwave darkroom, 5g AP will never start successfully at this time.

config file :

interface=wlan0
driver=nl80211
ctrl_interface=/var/run/hostapd
logger_syslog=-1
logger_syslog_level=2
logger_stdout=-1
logger_stdout_level=2
dump_file=/tmp/hostapd.dump

hw_mode=a
max_num_sta=255
beacon_int=100
dtim_period=2
preamble=1

macaddr_acl=0
accept_mac_file=/etc/hostapd/hostapd.accept
deny_mac_file=/etc/hostapd/hostapd.deny

ieee80211d=1
country_code=US

ieee80211n=1
#ht_capab=[SMPS-STATIC][RX-STBC1]

ieee8021x=0

# bit 0 = Open System Authentication
# bit 1 = Shared Key Authentication (requires WEP)
auth_algs=1

wpa_key_mgmt=WPA-PSK
wpa_pairwise=TKIP CCMP

#!
ssid=15435007
channel=0
wpa=0
wpa_passphrase=12345678
#wep_default_key=0
#*

The attachment is the kernel log and the boot log of hostapd

[10:21:45:367][20200807_10:21:45]
[10:21:46:310]
[10:21:52:384]root@hi-target:/mnt/p1/wg7833# cat hostapd.conf 
[10:21:52:411]interface=wlan0
[10:21:52:412]driver=nl80211
[10:21:52:412]ctrl_interface=/var/run/hostapd
[10:21:52:412]logger_syslog=-1
[10:21:52:412]logger_syslog_level=2
[10:21:52:412]logger_stdout=-1
[10:21:52:423]logger_stdout_level=2
[10:21:52:423]dump_file=/tmp/hostapd.dump
[10:21:52:423]
[10:21:52:423]hw_mode=a
[10:21:52:423]max_num_sta=255
[10:21:52:424]beacon_int=100
[10:21:52:424]dtim_period=2
[10:21:52:424]preamble=1
[10:21:52:424]
[10:21:52:433]macaddr_acl=0
[10:21:52:434]accept_mac_file=/etc/hostapd/hostapd.accept
[10:21:52:434]deny_mac_file=/etc/hostapd/hostapd.deny
[10:21:52:434]
[10:21:52:435]ieee80211d=1
[10:21:52:444]country_code=US
[10:21:52:444]
[10:21:52:444]ieee80211n=1
[10:21:52:444]#ht_capab=[SMPS-STATIC][RX-STBC1]
[10:21:52:444]
[10:21:52:444]ieee8021x=0
[10:21:52:444]
[10:21:52:445]# bit 0 = Open System Authentication
[10:21:52:455]# bit 1 = Shared Key Authentication (requires WEP)
[10:21:52:455]auth_algs=1
[10:21:52:455]
[10:21:52:455]wpa_key_mgmt=WPA-PSK
[10:21:52:455]wpa_pairwise=TKIP CCMP
[10:21:52:456]
[10:21:52:456]#!
[10:21:52:456]ssid=15435007
[10:21:52:456]channel=0
[10:21:52:468]wpa=0
[10:21:52:468]wpa_passphrase=12345678
[10:21:52:468]#wep_default_key=0
[10:21:52:468]#*
[10:21:53:375]root@hi-target:/mnt/p1/wg7833# 
[10:21:53:618]root@hi-target:/mnt/p1/wg7833# 
[10:21:53:827]root@hi-target:/mnt/p1/wg7833# 
[10:21:59:422]root@hi-target:/mnt/p1/wg7833# cat /proc/kmsg &
[10:21:59:442]root@hi-target:/mnt/p1/wg7833# <6>[    0.000000] Booting Linux on physical CPU 0x0
[10:21:59:465]<5>[    0.000000] Linux version 3.18.0-linux4sam_5.0-alpha7+ (wl@wanglei) (gcc version 4.7.3 20130328 (prerelease) (crosstool-NG linaro-1.13.1-4.7-2013.04-20130415 - Linaro GCC 2013.04) ) #304 Fri May 8 14:55:11 CST 2020
[10:21:59:465]<6>[    0.000000] CPU: ARMv7 Processor [410fc051] revision 1 (ARMv7), cr=10c53c7d
[10:21:59:476]<6>[    0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[10:21:59:476]<6>[    0.000000] Machine model: ZHD380_0101
[10:21:59:487]<6>[    0.000000] cma: Reserved 16 MiB at 0x27000000
[10:21:59:487]<6>[    0.000000] Memory policy: Data cache writeback
[10:21:59:501]<6>[    0.000000] AT91: Detected soc type: sama5d3
[10:21:59:501]<6>[    0.000000] AT91: Detected soc subtype: sama5d31
[10:21:59:502]<7>[    0.000000] On node 0 totalpages: 32768
[10:21:59:510]<7>[    0.000000] free_area_init_node: node 0, pgdat c054df88, node_mem_map c6ef2000
[10:21:59:520]<7>[    0.000000]   Normal zone: 256 pages used for memmap
[10:21:59:522]<7>[    0.000000]   Normal zone: 0 pages reserved
[10:21:59:526]<7>[    0.000000]   Normal zone: 32768 pages, LIFO batch:7
[10:21:59:535]<6>[    0.000000] CPU: All CPU(s) started in SVC mode.
[10:21:59:536]<7>[    0.000000] pcpu-alloc: s0 r0 d32768 u32768 alloc=1*32768
[10:21:59:547]<7>[    0.000000] pcpu-alloc: [0] 0 
[10:21:59:549]<4>[    0.000000] Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 32512
[10:21:59:555]<5>[    0.000000] Kernel command line: console=ttyS0,115200 root=/dev/ram ro initrd=0x23000000,6MB rootfstype=cramfs
[10:21:59:565]<6>[    0.000000] PID hash table entries: 512 (order: -1, 2048 bytes)
[10:21:59:582]<6>[    0.000000] Dentry cache hash table entries: 16384 (order: 4, 65536 bytes)
[10:21:59:583]<6>[    0.000000] Inode-cache hash table entries: 8192 (order: 3, 32768 bytes)
[10:21:59:589]<4>[    0.000000] Memory: 101512K/131072K available (4100K kernel code, 194K rwdata, 920K rodata, 184K init, 241K bss, 29560K reserved)
[10:21:59:602]<5>[    0.000000] Virtual kernel memory layout:
[10:21:59:603]<5>[    0.000000]     vector  : 0xffff0000 - 0xffff1000   (   4 kB)
[10:21:59:617]<5>[    0.000000]     fixmap  : 0xffc00000 - 0xffe00000   (2048 kB)
[10:21:59:618]<5>[    0.000000]     vmalloc : 0xc8800000 - 0xff000000   ( 872 MB)
[10:21:59:627]<5>[    0.000000]     lowmem  : 0xc0000000 - 0xc8000000   ( 128 MB)
[10:21:59:628]<5>[    0.000000]     modules : 0xbf000000 - 0xc0000000   (  16 MB)
[10:21:59:637]<5>[    0.000000]       .text : 0xc0008000 - 0xc04ef378   (5021 kB)
[10:21:59:638]<5>[    0.000000]       .init : 0xc04f0000 - 0xc051e000   ( 184 kB)
[10:21:59:652]<5>[    0.000000]       .data : 0xc051e000 - 0xc054e860   ( 195 kB)
[10:21:59:653]<5>[    0.000000]        .bss : 0xc054e860 - 0xc058b058   ( 242 kB)
[10:21:59:658]<6>[    0.000000] NR_IRQS:16 nr_irqs:16 16
[10:21:59:669]<6>[    0.000000] sched_clock: 32 bits at 100 Hz, resolution 10000000ns, wraps every 21474836480000000ns
[10:21:59:670]<6>[    0.050000] Calibrating delay loop... 351.43 BogoMIPS (lpj=1757184)
[10:21:59:682]<6>[    0.060000] pid_max: default: 32768 minimum: 301
[10:21:59:685]<6>[    0.060000] Security Framework initialized
[10:21:59:694]<6>[    0.060000] Mount-cache hash table entries: 1024 (order: 0, 4096 bytes)
[10:21:59:695]<6>[    0.060000] Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes)
[10:21:59:704]<6>[    0.060000] CPU: Testing write buffer coherency: ok
[10:21:59:710]<6>[    0.060000] Setting up static identity map for 0x203dea38 - 0x203dea90
[10:21:59:719]<6>[    0.060000] devtmpfs: initialized
[10:21:59:720]<6>[    0.060000] VFP support v0.3: implementor 41 architecture 2 part 30 variant 5 rev 1
[10:21:59:728]<6>[    0.060000] pinctrl core: initialized pinctrl subsystem
[10:21:59:729]<6>[    0.060000] regulator-dummy: no parameters
[10:21:59:738]<6>[    0.080000] NET: Registered protocol family 16
[10:21:59:743]<6>[    0.090000] DMA: preallocated 256 KiB pool for atomic coherent allocations
[10:21:59:753]<6>[    0.090000] cpuidle: using governor ladder
[10:21:59:754]<6>[    0.090000] cpuidle: using governor menu
[10:21:59:763]<6>[    0.110000] gpio-at91 fffff200.gpio: at address fefff200
[10:21:59:765]<6>[    0.120000] gpio-at91 fffff400.gpio: at address fefff400
[10:21:59:774]<6>[    0.120000] gpio-at91 fffff600.gpio: at address fefff600
[10:21:59:779]<6>[    0.120000] gpio-at91 fffff800.gpio: at address fefff800
[10:21:59:788]<6>[    0.120000] gpio-at91 fffffa00.gpio: at address fefffa00
[10:21:59:789]<6>[    0.120000] pinctrl-at91 ahb:apb:pinctrl@fffff200: initialized AT91 pinctrl driver
[10:21:59:795]<7>[    0.120000] tcb_clksrc: tc0 at 16.000 MHz
[10:21:59:804]<6>[    1.360000] at_hdmac ffffe600.dma-controller: Atmel AHB DMA Controller ( cpy slave sg-cpy ), 8 channels
[10:21:59:805]<6>[    1.360000] at_hdmac ffffe800.dma-controller: Atmel AHB DMA Controller ( cpy slave sg-cpy ), 8 channels
[10:21:59:817]<6>[    1.360000] wlan-en-regulator: 3300 mV 
[10:21:59:818]<5>[    1.370000] SCSI subsystem initialized
[10:21:59:826]<6>[    1.370000] usbcore: registered new interface driver usbfs
[10:21:59:828]<6>[    1.370000] usbcore: registered new interface driver hub
[10:21:59:837]<6>[    1.370000] usbcore: registered new device driver usb
[10:21:59:838]<6>[    1.370000] ### input_init
[10:21:59:852]<6>[    1.370000] at91_i2c f0018000.i2c: using dma0chan0 (tx) and dma0chan1 (rx) for DMA transfers
[10:21:59:853]<6>[    1.390000] at91_i2c f0018000.i2c: AT91 i2c bus driver (hw version: 0x402).
[10:21:59:862]<6>[    1.400000] i2c-gpio ahb:apb:i2c@0: using pins 133 (SDA) and 134 (SCL)
[10:21:59:863]<6>[    1.400000] pps_core: LinuxPPS API ver. 1 registered
[10:21:59:869]<6>[    1.400000] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[10:21:59:881]<6>[    1.400000] Advanced Linux Sound Architecture Driver Initialized.
[10:21:59:882]<6>[    1.400000] Switched to clocksource tcb_clksrc
[10:21:59:894]<6>[    1.410000] input: gpio_otg_polled as /devices/virtual/input/input0
[10:21:59:895]<4>[    1.410000] bq25700 temp limit:temp-adc-channel:[2]
[10:21:59:905]<4>[    1.410000] bq25700 temp limit:temp-adc-max-value:[2634]
[10:21:59:910]<4>[    1.410000] bq25700 temp limit:temp-adc-min-value:[1185]
[10:21:59:919]<4>[    1.410000] bq25700 temp limit:temp-adc-bus:[f8018000.adc]
[10:21:59:920]<4>[    1.410000] bq25700 ti,zhd_of_current:[25]
[10:21:59:929]<4>[    1.420000] ##################wl test POWER_STATUS_GPIO is low,Continue!
[10:21:59:930]<4>[    1.420000] TUSB422 UNATTACHED_SRC
[10:21:59:939]<4>[    1.420000] TUSB422 Port[0]: addr: 0x20, DRP, Rp: default, Flags: Try-SNK.
[10:21:59:939]<4>[    1.420000] TUSB422 VID: 0x0451
[10:21:59:944]<4>[    1.420000] TUSB422 PID: 0x0422
[10:21:59:952]<4>[    1.420000] TUSB422 DID: 0x0100
[10:21:59:953]<4>[    1.430000] TUSB422 REV: 0x02
[10:21:59:955]<6>[    1.430000] NET: Registered protocol family 2
[10:21:59:961]<6>[    1.430000] TCP established hash table entries: 1024 (order: 0, 4096 bytes)
[10:21:59:970]<6>[    1.430000] TCP bind hash table entries: 1024 (order: 0, 4096 bytes)
[10:21:59:971]<6>[    1.430000] TCP: Hash tables configured (established 1024 bind 1024)
[10:21:59:983]<6>[    1.430000] TCP: reno registered
[10:21:59:984]<6>[    1.430000] UDP hash table entries: 256 (order: 0, 4096 bytes)
[10:21:59:994]<6>[    1.430000] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
[10:21:59:996]<6>[    1.430000] NET: Registered protocol family 1
[10:22:00:006]<6>[    1.430000] Trying to unpack rootfs image as initramfs...
[10:22:00:012]<6>[    1.430000] rootfs image is not initramfs (junk in compressed archive); looks like an initrd
[10:22:00:021]<4>[    1.440000] TUSB422 usb_pd_pal_disable_vbus
[10:22:00:022]<4>[    1.440000] BQ25700 pd_dpm_handle_pe_event : Disable VBUS Control
[10:22:00:030]<4>[    1.440000] ###bq25700 usb_pd_pal_disable_vbus  66
[10:22:00:031]<4>[    1.440000] TUSB422 usb_pd_pal_disable_vbus
[10:22:00:055]<4>[    1.440000] BQ25700 pd_dpm_handle_pe_event : Disable VBUS Control
[10:22:00:056]<4>[    1.440000] ###bq25700 usb_pd_pal_disable_vbus  66
[10:22:00:066]<4>[    1.440000] ############wl test UNATTACHED_SNK
[10:22:00:066]<4>[    1.440000] TUSB422 PE_UNATTACHED
[10:22:00:066]<4>[    1.440000] TUSB422 usb_pd_pal_notify_connect_state: TYPEC_UNATTACHED
[10:22:00:067]<4>[    1.450000] ###bq25700 typec_disconnect_handler  ####1  753
[10:22:00:075]<6>[    1.510000] Freeing initrd memory: 6144K (c3000000 - c3600000)
[10:22:00:081]<6>[    1.510000] futex hash table entries: 256 (order: -1, 3072 bytes)
[10:22:00:090]<6>[    1.510000] msgmni has been set to 242
[10:22:00:092]<6>[    1.520000] io scheduler noop registered (default)
[10:22:00:098]<6>[    1.530000] atmel_usart f001c000.serial: ttyS1 at MMIO 0xf001c000 (irq = 30, base_baud = 4125000) is a ATMEL_SERIAL
[10:22:00:103]<6>[    1.530000] atmel_usart f0020000.serial: ttyS2 at MMIO 0xf0020000 (irq = 31, base_baud = 4125000) is a ATMEL_SERIAL
[10:22:00:113]<6>[    1.530000] atmel_usart f0024000.serial: ttyS5 at MMIO 0xf0024000 (irq = 32, base_baud = 4125000) is a ATMEL_SERIAL
[10:22:00:124]<6>[    1.530000] atmel_usart f8028000.serial: ttyS6 at MMIO 0xf8028000 (irq = 33, base_baud = 4125000) is a ATMEL_SERIAL
[10:22:00:137]<6>[    1.530000] atmel_usart f8020000.serial: ttyS3 at MMIO 0xf8020000 (irq = 37, base_baud = 4125000) is a ATMEL_SERIAL
[10:22:00:148]<6>[    1.530000] atmel_usart f8024000.serial: ttyS4 at MMIO 0xf8024000 (irq = 38, base_baud = 4125000) is a ATMEL_SERIAL
[10:22:00:162]<6>[    1.540000] atmel_usart ffffee00.serial: ttyS0 at MMIO 0xffffee00 (irq = 41, base_baud = 8250000) is a ATMEL_SERIAL
[10:22:00:162]<6>[    1.540000] console [ttyS0] enabled
[10:22:00:163]<4>[    1.540000] ##### zg init #########
[10:22:00:179]<6>[    1.550000] brd: module loaded
[10:22:00:179]<6>[    1.560000] loop: module loaded
[10:22:00:180]<6>[    1.570000] ### request ssc pins...
[10:22:00:190]<6>[    1.570000] ok
[10:22:00:191]<6>[    1.570000] ssc f0008000.ssc: Atmel SSC device at 0xc8828000 (irq 27)
[10:22:00:200]<6>[    1.570000] atmel_spi f0004000.spi: version: 0x213
[10:22:00:201]<3>[    1.570000] atmel_spi f0004000.spi: DMA TX channel not available, SPI unable to use DMA
[10:22:00:210]<6>[    1.570000] atmel_spi f0004000.spi: Atmel SPI Controller using PIO only
[10:22:00:219]<6>[    1.570000] atmel_spi f0004000.spi: Atmel SPI Controller at 0xf0004000 (irq 26)
[10:22:00:220]<6>[    1.570000] atmel_spi f8008000.spi: version: 0x213
[10:22:00:230]<6>[    1.570000] atmel_spi f8008000.spi: Using dma1chan0 (tx) and dma1chan1 (rx) for DMA transfers
[10:22:00:232]<6>[    1.570000] #############  ZG USE SPI DMA TRAMFER! ##############
[10:22:00:237]<6>[    1.570000] atmel_spi f8008000.spi: Atmel SPI Controller at 0xf8008000 (irq 35)
[10:22:00:252]<6>[    1.570000] PPP generic driver version 2.4.2
[10:22:00:252]<6>[    1.570000] PPP BSD Compression module registered
[10:22:00:253]<6>[    1.570000] PPP Deflate Compression module registered
[10:22:00:260]<6>[    1.570000] usbcore: registered new interface driver asix
[10:22:00:274]<6>[    1.570000] usbcore: registered new interface driver ax88179_178a
[10:22:00:280]<6>[    1.570000] usbcore: registered new interface driver cdc_ether
[10:22:00:288]<6>[    1.570000] usbcore: registered new interface driver net1080
[10:22:00:288]<6>[    1.570000] usbcore: registered new interface driver rndis_host
[10:22:00:297]<6>[    1.570000] usbcore: registered new interface driver cdc_subset
[10:22:00:298]<6>[    1.570000] usbcore: registered new interface driver zaurus
[10:22:00:309]<6>[    1.570000] usbcore: registered new interface driver cdc_ncm
[10:22:00:314]<6>[    1.570000] usbcore: registered new interface driver cdc_mbim
[10:22:00:323]<6>[    1.570000] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[10:22:00:324]<6>[    1.570000] ehci-atmel: EHCI Atmel driver
[10:22:00:329]<6>[    1.580000] atmel-ehci 700000.ehci: EHCI Host Controller
[10:22:00:346]<6>[    1.580000] atmel-ehci 700000.ehci: new USB bus registered, assigned bus number 1
[10:22:00:347]<6>[    1.580000] atmel-ehci 700000.ehci: irq 49, io mem 0x00700000
[10:22:00:357]<6>[    1.600000] atmel-ehci 700000.ehci: USB 2.0 started, EHCI 1.00
[10:22:00:358]<6>[    1.600000] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
[10:22:00:366]<6>[    1.600000] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[10:22:00:366]<6>[    1.600000] usb usb1: Product: EHCI Host Controller
[10:22:00:372]<6>[    1.600000] usb usb1: Manufacturer: Linux 3.18.0-linux4sam_5.0-alpha7+ ehci_hcd
[10:22:00:386]<6>[    1.600000] usb usb1: SerialNumber: 700000.ehci
[10:22:00:386]<6>[    1.600000] hub 1-0:1.0: USB hub found
[10:22:00:390]<6>[    1.600000] hub 1-0:1.0: 3 ports detected
[10:22:00:399]<6>[    1.600000] ohci_hcd: USB 1.1 'Open' Host Controller (OHCI) Driver
[10:22:00:400]<6>[    1.600000] ohci-atmel: OHCI Atmel driver
[10:22:00:412]<6>[    1.600000] at91_ohci 600000.ohci: USB Host Controller
[10:22:00:413]<6>[    1.600000] at91_ohci 600000.ohci: new USB bus registered, assigned bus number 2
[10:22:00:419]<6>[    1.600000] at91_ohci 600000.ohci: irq 49, io mem 0x00600000
[10:22:00:430]<6>[    1.660000] usb usb2: New USB device found, idVendor=1d6b, idProduct=0001
[10:22:00:431]<6>[    1.660000] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[10:22:00:442]<6>[    1.660000] usb usb2: Product: USB Host Controller
[10:22:00:451]<6>[    1.660000] usb usb2: Manufacturer: Linux 3.18.0-linux4sam_5.0-alpha7+ ohci_hcd
[10:22:00:460]<6>[    1.660000] usb usb2: SerialNumber: at91
[10:22:00:460]<6>[    1.660000] hub 2-0:1.0: USB hub found
[10:22:00:461]<6>[    1.660000] hub 2-0:1.0: 3 ports detected
[10:22:00:467]<6>[    1.660000] usbcore: registered new interface driver cdc_acm
[10:22:00:475]<6>[    1.660000] cdc_acm: USB Abstract Control Model driver for USB modems and ISDN adapters
[10:22:00:481]<6>[    1.660000] usbcore: registered new interface driver cdc_wdm
[10:22:00:490]<6>[    1.660000] usbcore: registered new interface driver usb-storage
[10:22:00:492]<6>[    1.660000] usbcore: registered new interface driver usbserial
[10:22:00:499]<6>[    1.660000] usbcore: registered new interface driver usbserial_generic
[10:22:00:512]<6>[    1.660000] usbserial: USB Serial support registered for generic
[10:22:00:513]<6>[    1.660000] usbcore: registered new interface driver option
[10:22:00:522]<6>[    1.660000] usbserial: USB Serial support registered for GSM modem (1-port)
[10:22:00:523]<6>[    1.670000] usbcore: registered new interface driver sierra
[10:22:00:528]<6>[    1.670000] usbserial: USB Serial support registered for Sierra USB modem
[10:22:00:552]<6>[    1.670000] atmel_usba_udc 500000.gadget: MMIO registers at 0xf8030000 mapped at c8830000
[10:22:00:553]<6>[    1.670000] atmel_usba_udc 500000.gadget: FIFO at 0x00500000 mapped at c8e00000
[10:22:00:561]<4>[    1.670000] rtc (null): invalid alarm value: 1900-1-1 0:0:0
[10:22:00:562]<6>[    1.670000] at91_rtc fffffeb0.rtc: rtc core: registered fffffeb0.rtc as rtc0
[10:22:00:571]<6>[    1.670000] at91_rtc fffffeb0.rtc: AT91 Real Time Clock driver.
[10:22:00:572]<6>[    1.670000] i2c /dev entries driver
[10:22:00:586]<6>[    1.680000] pps pps0: new PPS source pps.-1
[10:22:00:587]<6>[    1.680000] pps pps0: Registered IRQ 83 as PPS source
[10:22:00:596]<6>[    1.680000] AT91: Starting after software reset
[10:22:00:597]<6>[    1.680000] atmel_mci f0000000.mmc: version: 0x505
[10:22:00:605]<6>[    1.680000] atmel_mci f0000000.mmc: using dma0chan2 for DMA transfers
[10:22:00:610]<6>[    1.680000] atmel_mci f0000000.mmc: No vmmc regulator found
[10:22:00:615]<6>[    1.680000] atmel_mci f0000000.mmc: No vqmmc regulator found
[10:22:00:624]<6>[    1.720000] atmel_mci f0000000.mmc: Atmel MCI controller at 0xf0000000 irq 25, 1 slots
[10:22:00:625]<6>[    1.720000] atmel_mci f8000000.mmc: version: 0x505
[10:22:00:633]<6>[    1.720000] atmel_mci f8000000.mmc: using dma1chan2 for DMA transfers
[10:22:00:635]<6>[    1.720000] atmel_mci f8000000.mmc: No vmmc regulator found
[10:22:00:647]<6>[    1.720000] atmel_mci f8000000.mmc: No vqmmc regulator found
[10:22:00:648]<6>[    1.760000] atmel_mci f8000000.mmc: Atmel MCI controller at 0xf8000000 irq 34, 1 slots
[10:22:00:656]<6>[    1.760000] atmel_mci f8004000.mmc: version: 0x505
[10:22:00:657]<6>[    1.760000] atmel_mci f8004000.mmc: using dma1chan3 for DMA transfers
[10:22:00:665]<6>[    1.760000] atmel_mci f8004000.mmc: No vqmmc regulator found
[10:22:00:666]<6>[    1.780000] mmc0: BKOPS_EN bit is not set
[10:22:00:681]<6>[    1.780000] mmc0: new MMC card at address 0001
[10:22:00:684]<6>[    1.780000] mmcblk0: mmc0:0001 008G70 7.28 GiB 
[10:22:00:692]<6>[    1.780000] mmcblk0boot0: mmc0:0001 008G70 partition 1 4.00 MiB
[10:22:00:693]<6>[    1.780000] mmcblk0boot1: mmc0:0001 008G70 partition 2 4.00 MiB
[10:22:00:703]<6>[    1.790000]  mmcblk0: p1 p2 p3 p4
[10:22:00:704]<6>[    1.800000] atmel_mci f8004000.mmc: Atmel MCI controller at 0xf8004000 irq 47, 1 slots
[10:22:00:715]<6>[    1.800000] iio iio:device0: Resolution used: 12 bits
[10:22:00:716]<6>[    1.800000] iio iio:device0: ADC Touch screen is disabled.
[10:22:00:727]<4>[    1.820000] 1-001a supply DCVDD not found, using dummy regulator
[10:22:00:728]<4>[    1.820000] 1-001a supply DBVDD not found, using dummy regulator
[10:22:00:734]<4>[    1.820000] 1-001a supply AVDD not found, using dummy regulator
[10:22:00:747]<4>[    1.820000] 1-001a supply CPVDD not found, using dummy regulator
[10:22:00:748]<4>[    1.820000] 1-001a supply MICVDD not found, using dummy regulator
[10:22:00:757]<6>[    1.820000] wm8904 1-001a: revision A
[10:22:00:757]<6>[    1.830000] ### atmel_ssc_set_audio
[10:22:00:758]<6>[    1.830000] ### asoc_ssc_init
[10:22:00:767]<6>[    1.830000] ### machine_dai_ptr = 0xc0547678
[10:22:00:767]<6>[    1.830000] ### dmaengine_pcm_request_chan_of
[10:22:00:768]<1>[    1.830000] ### using dma dma0chan3 for ssc tx
[10:22:00:777]<1>[    1.830000] ### using dma dma0chan4 for ssc rx
[10:22:00:788]<6>[    1.830000] atmel-wm8904-audio sound_wm8904: wm8904-hifi <-> f0008000.ssc mapping ok
[10:22:00:788]<6>[    1.830000] Netfilter messages via NETLINK v0.30.
[10:22:00:788]<6>[    1.830000] nfnl_acct: registering with nfnetlink.
[10:22:00:799]<6>[    1.830000] nf_conntrack version 0.5.0 (1938 buckets, 7752 max)
[10:22:00:800]<6>[    1.840000] ctnetlink v0.93: registering with nfnetlink.
[10:22:00:811]<6>[    1.840000] nf_tables: (c) 2007-2009 Patrick McHardy <kaber@trash.net>
[10:22:00:821]<6>[    1.840000] nf_tables_compat: (c) 2012 Pablo Neira Ayuso <pablo@netfilter.org>
[10:22:00:821]<6>[    1.840000] xt_time: kernel timezone is -0000
[10:22:00:824]<6>[    1.840000] ip_set: protocol 6
[10:22:00:829]<6>[    1.840000] IPVS: Registered protocols (TCP, UDP, SCTP, AH, ESP)
[10:22:00:846]<6>[    1.840000] IPVS: Connection hash table configured (size=4096, memory=32Kbytes)
[10:22:00:847]<7>[    1.840000] IPVS: Each connection entry needs 192 bytes at least
[10:22:00:859]<6>[    1.840000] IPVS: Creating netns size=1136 id=0
[10:22:00:859]<6>[    1.840000] IPVS: ipvs loaded.
[10:22:00:860]<6>[    1.840000] IPVS: [rr] scheduler registered.
[10:22:00:868]<6>[    1.840000] IPVS: [wrr] scheduler registered.
[10:22:00:870]<6>[    1.840000] IPVS: [lc] scheduler registered.
[10:22:00:882]<6>[    1.840000] IPVS: [wlc] scheduler registered.
[10:22:00:882]<6>[    1.840000] IPVS: [fo] scheduler registered.
[10:22:00:883]<6>[    1.840000] IPVS: [lblc] scheduler registered.
[10:22:00:892]<6>[    1.840000] IPVS: [lblcr] scheduler registered.
[10:22:00:893]<6>[    1.840000] IPVS: [dh] scheduler registered.
[10:22:00:901]<6>[    1.840000] IPVS: [sh] scheduler registered.
[10:22:00:902]<6>[    1.840000] IPVS: [sed] scheduler registered.
[10:22:00:914]<6>[    1.840000] IPVS: [nq] scheduler registered.
[10:22:00:914]<6>[    1.840000] IPVS: ftp: loaded support on port[0] = 21
[10:22:00:915]<6>[    1.840000] IPVS: [sip] pe registered.
[10:22:00:925]<6>[    1.840000] ip_tables: (C) 2000-2006 Netfilter Core Team
[10:22:00:926]<6>[    1.840000] TCP: cubic registered
[10:22:00:931]<6>[    1.840000] NET: Registered protocol family 17
[10:22:00:946]<6>[    1.840000] bridge: automatic filtering via arp/ip/ip6tables has been deprecated. Update your scripts to load br_netfilter if you need this.
[10:22:00:947]<6>[    1.840000] Ebtables v2.0 registered
[10:22:00:958]<6>[    1.850000] input: gpio_keys as /devices/gpio_keys/input/input1
[10:22:00:959]<6>[    1.850000] at91_rtc fffffeb0.rtc: setting system clock to 2007-01-02 18:39:47 UTC (1167763187)
[10:22:00:969]<6>[    1.860000] ALSA device list:
[10:22:00:970]<6>[    1.860000]   #0: wm8904 @ SAMA5D3EK
[10:22:00:980]<5>[    1.860000] RAMDISK: cramfs filesystem found at block 0
[10:22:01:001]<5>[    1.860000] RAMDISK: Loading 4784KiB [1 disk] into ram disk... -
[10:22:01:002]<4>[    1.950000] atmel_mci f8004000.mmc: card claims to support voltages below defined range
[10:22:01:014]<4>[    1.950000] |
[10:22:01:014]<4>[    1.960000] sdio:f_max 25000000
[10:22:01:015]<4>[    1.960000] /
[10:22:01:024]<4>[    1.970000] mmc2: queuing unknown CIS tuple 0x91 (3 bytes)
[10:22:01:024]<4>[    1.970000] -
[10:22:01:024]<6>[    1.970000] mmc2: new high speed SDIO card at address 0001
[10:22:01:066]<4>[    1.970000] done.
[10:22:01:067]<6>[    2.110000] VFS: Mounted root (cramfs filesystem) readonly on device 1:0.
[10:22:01:067]<6>[    2.110000] devtmpfs: mounted
[10:22:01:084]<6>[    2.110000] Freeing unused kernel memory: 184K (c04f0000 - c051e000)
[10:22:01:089]<3>[    3.320000] EXT2-fs (mmcblk0p4): error: couldn't mount because of unsupported optional features (244)
[10:22:01:101]<3>[    3.320000] EXT4-fs (mmcblk0p4): couldn't mount as ext3 due to feature incompatibilities
[10:22:01:103]<6>[    3.600000] EXT4-fs (mmcblk0p4): recovery complete
[10:22:01:113]<6>[    3.600000] EXT4-fs (mmcblk0p4): mounted filesystem with ordered data mode. Opts: (null)
[10:22:01:126]<3>[    3.610000] EXT2-fs (mmcblk0p3): error: couldn't mount because of unsupported optional features (244)
[10:22:01:127]<3>[    3.620000] EXT4-fs (mmcblk0p3): couldn't mount as ext3 due to feature incompatibilities
[10:22:01:132]<6>[    6.690000] usb 1-2: new high-speed USB device number 2 using atmel-ehci
[10:22:01:146]<6>[    6.840000] usb 1-2: New USB device found, idVendor=12d1, idProduct=15c1
[10:22:01:147]<6>[    6.840000] usb 1-2: New USB device strings: Mfr=1, Product=2, SerialNumber=3
[10:22:01:159]<6>[    6.840000] usb 1-2: Product: HUAWEI Mobile V7R11
[10:22:01:160]<6>[    6.840000] usb 1-2: Manufacturer: Huawei Technologies Co., Ltd.
[10:22:01:165]<6>[    6.840000] usb 1-2: SerialNumber: 0123456789ABCDEF
[10:22:01:180]<6>[    6.850000] cdc_ether 1-2:2.0 usb0: register 'cdc_ether' at usb-700000.ehci-2, CDC Ethernet Device, 02:1e:10:1f:00:00
[10:22:01:181]<6>[    6.890000] option 1-2:2.2: GSM modem (1-port) converter detected
[10:22:01:187]<6>[    6.890000] usb 1-2: GSM modem (1-port) converter now attached to ttyUSB0
[10:22:01:202]<6>[    6.890000] option 1-2:2.3: GSM modem (1-port) converter detected
[10:22:01:203]<6>[    6.890000] usb 1-2: GSM modem (1-port) converter now attached to ttyUSB1
[10:22:01:215]<6>[    6.900000] option 1-2:2.4: GSM modem (1-port) converter detected
[10:22:01:216]<6>[    6.900000] usb 1-2: GSM modem (1-port) converter now attached to ttyUSB2
[10:22:01:221]<6>[    6.910000] option 1-2:2.5: GSM modem (1-port) converter detected
[10:22:01:237]<6>[    6.910000] usb 1-2: GSM modem (1-port) converter now attached to ttyUSB3
[10:22:01:238]<6>[    6.920000] option 1-2:2.6: GSM modem (1-port) converter detected
[10:22:01:250]<6>[    6.920000] usb 1-2: GSM modem (1-port) converter now attached to ttyUSB4
[10:22:01:251]<6>[    7.820000] EXT4-fs (mmcblk0p3): recovery complete
[10:22:01:256]<6>[    7.820000] EXT4-fs (mmcblk0p3): mounted filesystem with ordered data mode. Opts: (null)
[10:22:01:265]<4>[    7.850000] FAT-fs (mmcblk0p2): Volume was not properly unmounted. Some data may be corrupt. Please run fsck.
[10:22:01:277]<4>[    8.620000] FAT-fs (mmcblk0p2): Volume was not properly unmounted. Some data may be corrupt. Please run fsck.
[10:22:01:287]<3>[    8.640000] EXT2-fs (mmcblk0p3): error: couldn't mount because of unsupported optional features (240)
[10:22:01:302]<3>[    8.640000] EXT4-fs (mmcblk0p3): couldn't mount as ext3 due to feature incompatibilities
[10:22:01:303]<6>[    8.650000] EXT4-fs (mmcblk0p3): mounted filesystem with ordered data mode. Opts: (null)
[10:22:01:312]<4>[    8.730000] FAT-fs (loop0): Volume was not properly unmounted. Some data may be corrupt. Please run fsck.
[10:22:01:322]<3>[    8.750000] EXT2-fs (mmcblk0p4): error: couldn't mount because of unsupported optional features (240)
[10:22:01:335]<3>[    8.750000] EXT4-fs (mmcblk0p4): couldn't mount as ext3 due to feature incompatibilities
[10:22:01:336]<6>[    8.770000] EXT4-fs (mmcblk0p4): mounted filesystem with ordered data mode. Opts: (null)
[10:22:01:349]<5>[   10.680000] random: nonblocking pool is initialized
[10:22:01:349]<6>[   11.390000] Number of LUNs=8
[10:22:01:358]<6>[   11.390000] Mass Storage Function, version: 2009/09/11
[10:22:01:358]<6>[   11.390000] LUN: removable file: (no medium)
[10:22:01:359]<6>[   11.390000] Number of LUNs=1
[10:22:01:369]<6>[   11.390000] LUN: removable file: /dev/mmcblk0p2
[10:22:01:370]<6>[   11.390000] Number of LUNs=1
[10:22:01:382]<6>[   11.410000] g_acm_ms gadget: Composite Gadget (ACM + MS), version: 2011/10/10
[10:22:01:383]<6>[   11.410000] g_acm_ms gadget: g_acm_ms ready
[10:22:01:385]<1>[   11.610000] ### pck_dev_probe
[10:22:01:393]<6>[   11.610000] ### setting clock rate to 32768Hz
[10:22:01:394]<6>[   11.890000] Bluetooth: Core ver 2.19
[10:22:01:403]<6>[   11.890000] NET: Registered protocol family 31
[10:22:01:404]<6>[   11.890000] Bluetooth: HCI device and connection manager initialized
[10:22:01:417]<6>[   11.890000] Bluetooth: HCI socket layer initialized
[10:22:01:418]<6>[   11.890000] Bluetooth: L2CAP socket layer initialized
[10:22:01:429]<6>[   11.890000] Bluetooth: SCO socket layer initialized
[10:22:01:429]<6>[   11.900000] Bluetooth: BNEP (Ethernet Emulation) ver 1.3
[10:22:01:439]<6>[   11.900000] Bluetooth: BNEP filters: protocol multicast
[10:22:01:451]<6>[   11.900000] Bluetooth: BNEP socket layer initialized
[10:22:01:461]<6>[   11.990000] Bluetooth: RFCOMM TTY layer initialized
[10:22:01:461]<6>[   11.990000] Bluetooth: RFCOMM socket layer initialized
[10:22:01:461]<6>[   11.990000] Bluetooth: RFCOMM ver 1.11
[10:22:01:461]<6>[   12.060000] Bluetooth: HCI UART driver ver 2.2
[10:22:01:463]<6>[   12.060000] Bluetooth: HCI H4 protocol initialized
[10:22:01:471]<6>[   12.060000] Bluetooth: HCI BCSP protocol initialized
[10:22:01:472]<6>[   12.060000] Bluetooth: HCILL protocol initialized
[10:22:01:488]<6>[   12.100000] Bluetooth: Virtual HCI driver ver 1.5
[10:22:01:488]<4>[   12.170000] baud_rate = 115200
[10:22:01:489]<7>[   12.320000] hdev c68d5000
[10:22:01:497]<7>[   12.320000] HCI device registered (hdev c68d5000)
[10:22:01:497]<7>[   12.380000] hci0 c68d5000
[10:22:01:498]<6>[   12.380000] (stc):  chnl_id list empty :4 
[10:22:01:507]<6>[   12.820000] atmel_usart f0020000.serial: using dma0chan5 for rx DMA transfers
[10:22:01:514]<6>[   12.820000] (stc): st_tty_open 
[10:22:01:520]<6>[   12.820000] (stk) :line discipline installed(stk) :ti-connectivity/TIInit_11.8.32.bts
[10:22:01:529]<6>[   20.280000] (stc):  all chnl_ids unregistered (stk) :ldisc_install = 0
[10:22:01:530]<6>[   20.280000] (stc): st_tty_close <7>[   20.310000] hci0 c68d5000
[10:22:01:539]<6>[   20.310000] (stc):  chnl_id list empty :4 
[10:22:01:549]<6>[   20.710000] atmel_usart f0020000.serial: using dma0chan5 for rx DMA transfers
[10:22:01:559]<6>[   20.710000] (stc): st_tty_open 
[10:22:01:560]<6>[   20.710000] (stk) :line discipline installed(stk) :ti-connectivity/TIInit_11.8.32.bts
[10:22:01:568]<6>[   28.210000] Loading modules backported from Linux version R8.7_SP3-0-g8cbba96
[10:22:01:569]<6>[   28.210000] Backport generated by backports.git R8.7_SP3-0-gd4777ef
[10:22:01:581]<4>[   28.670000] wl debug(init)
[10:22:01:581]<4>[   28.670000] wl debug
[10:22:01:581]<4>[   28.670000] wl debug
[10:22:01:582]<4>[   28.670000] wl debug2
[10:22:01:590]<4>[   28.670000] wl debug1
[10:22:01:590]<4>[   28.940000] sdio:f_max 25000000
[10:22:01:591]<6>[   29.150000] wlcore: wl18xx HW: 183x or 180x, PG 2.2 (ROM 0x11)
[10:22:01:601]<6>[   29.150000] wlcore: loaded
[10:22:01:601]<6>[   29.150000] wlcore: driver version: R8.7_SP3
[10:22:01:601]<4>[   29.670000] sdio:f_max 25000000
[10:22:01:615]<6>[   30.250000] wlcore: PHY firmware version: Rev 8.2.0.0.243
[10:22:01:615]<6>[   30.360000] wlcore: firmware booted (Rev 8.9.0.0.81)
[10:22:02:589]
[10:22:03:121]root@hi-target:/mnt/p1/wg7833# 
[10:22:03:306]root@hi-target:/mnt/p1/wg7833# 
[10:22:03:512]root@hi-target:/mnt/p1/wg7833# 
[10:22:03:690]root@hi-target:/mnt/p1/wg7833# 
[10:22:03:870]root@hi-target:/mnt/p1/wg7833# 
[10:22:04:048]root@hi-target:/mnt/p1/wg7833# 
[10:22:04:382]root@hi-target:/mnt/p1/wg7833# 
[10:22:04:574]root@hi-target:/mnt/p1/wg7833# 
[10:22:04:732]root@hi-target:/mnt/p1/wg7833# 
[10:22:17:708]root@hi-target:/mnt/p1/wg7833# ./hostapd -dd hostapd.conf 
[10:22:18:035]random: Trying to read entropy from /dev/random
[10:22:18:068]Configuration file: hostapd.conf
[10:22:18:070]Line 8: DEPRECATED: 'dump_file' configuration variable is not used anymore
[10:22:18:084]nl80211: Supported cipher 00-0f-ac:1
[10:22:18:084]nl80211: Supported cipher 00-0f-ac:5
[10:22:18:085]nl80211: Supported cipher 00-0f-ac:2
[10:22:18:098]nl80211: Supported cipher 00-0f-ac:4
[10:22:18:098]nl80211: Supported cipher 00-14-72:1
[10:22:18:099]nl80211: Supports Probe Response offload in AP mode
[10:22:18:108]nl80211: Using driver-based off-channel TX
[10:22:18:112]nl80211: Supported vendor command: vendor_id=0x80028 subcmd=0
[10:22:18:119]nl80211: Supported vendor command: vendor_id=0x80028 subcmd=1
[10:22:18:120]nl80211: Supported vendor command: vendor_id=0x80028 subcmd=2
[10:22:18:132]nl80211: Supported vendor event: vendor_id=0x80028 subcmd=0
[10:22:18:133]nl80211: Supported vendor event: vendor_id=0x80028 subcmd=1
[10:22:18:147]nl80211: Use separate P2P group interface (driver advertised support)
[10:22:18:147]nl80211: Enable multi-channel concurrent (driver advertised support)
[10:22:18:148]nl80211: use P2P_DEVICE support
[10:22:18:157]nl80211: interface wlan0 in phy phy0
[10:22:18:157]nl80211: Set mode ifindex 3 iftype 3 (AP)
[10:22:18:161]<6>[   89.400000] wlcore: down
[10:22:18:170]nl80211: Setup AP(wlan0) - device_ap_sme=0 use_monitor=0
[10:22:18:171]nl80211: Subscribe to mgmt frames with AP handle 0x160938
[10:22:18:184]nl80211: Register frame type=0xb0 (WLAN_FC_STYPE_AUTH) nl_handle=0x160938 match=
[10:22:18:185]nl80211: Register frame type=0x0 (WLAN_FC_STYPE_ASSOC_REQ) nl_handle=0x160938 match=
[10:22:18:198]nl80211: Register frame type=0x20 (WLAN_FC_STYPE_REASSOC_REQ) nl_handle=0x160938 match=
[10:22:18:199]nl80211: Register frame type=0xa0 (WLAN_FC_STYPE_DISASSOC) nl_handle=0x160938 match=
[10:22:18:208]nl80211: Register frame type=0xc0 (WLAN_FC_STYPE_DEAUTH) nl_handle=0x160938 match=
[10:22:18:212]nl80211: Register frame type=0xd0 (WLAN_FC_STYPE_ACTION) nl_handle=0x160938 match=
[10:22:18:221]nl80211: Register frame type=0x40 (WLAN_FC_STYPE_PROBE_REQ) nl_handle=0x160938 match=
[10:22:18:222]rfkill: initial event: idx=1 type=1 op=0 soft=0 hard=0
[10:22:18:235]nl80211: Add own interface ifindex 3 (ifidx_reason -1)
[10:22:18:235]nl80211: if_indices[16]: 3(-1)
[10:22:18:235]phy: phy0
[10:22:18:236]BSS count 1, BSSID mask 00:00:00:00:00:00 (0 bits)
[10:22:18:248]wlan0: interface state UNINITIALIZED->COUNTRY_UPDATE
[10:22:18:249]Previous country code 00, new country code US 
[10:22:18:263]Continue interface setup after channel list update
[10:22:18:263]ctrl_iface not configured!
[10:22:18:264]random: Got 20/20 bytes from /dev/random
[10:22:23:168]Channel list update timeout - try to continue anyway
[10:22:23:169]nl80211: Regulatory information - country=00
[10:22:23:180]nl80211: 2402-2472 @ 40 MHz 20 mBm
[10:22:23:180]nl80211: 2457-2482 @ 40 MHz 20 mBm (no IR)
[10:22:23:181]nl80211: 2474-2494 @ 20 MHz 20 mBm (no OFDM) (no IR)
[10:22:23:191]nl80211: 5170-5250 @ 160 MHz 20 mBm (no IR)
[10:22:23:191]nl80211: 5250-5330 @ 160 MHz 20 mBm (DFS) (no IR)
[10:22:23:195]nl80211: 5490-5730 @ 160 MHz 20 mBm (DFS) (no IR)
[10:22:23:204]nl80211: 5735-5835 @ 80 MHz 20 mBm (no IR)
[10:22:23:205]nl80211: 57240-63720 @ 2160 MHz 0 mBm
[10:22:23:218]nl80211: Added 802.11b mode based on 802.11g information
[10:22:23:219]Allowed channel: mode=1 chan=1 freq=2412 MHz max_tx_power=20 dBm
[10:22:23:231]Allowed channel: mode=1 chan=2 freq=2417 MHz max_tx_power=20 dBm
[10:22:23:232]Allowed channel: mode=1 chan=3 freq=2422 MHz max_tx_power=20 dBm
[10:22:23:241]Allowed channel: mode=1 chan=4 freq=2427 MHz max_tx_power=20 dBm
[10:22:23:246]Allowed channel: mode=1 chan=5 freq=2432 MHz max_tx_power=20 dBm
[10:22:23:253]Allowed channel: mode=1 chan=6 freq=2437 MHz max_tx_power=20 dBm
[10:22:23:254]Allowed channel: mode=1 chan=7 freq=2442 MHz max_tx_power=20 dBm
[10:22:23:265]Allowed channel: mode=1 chan=8 freq=2447 MHz max_tx_power=20 dBm
[10:22:23:266]Allowed channel: mode=1 chan=9 freq=2452 MHz max_tx_power=20 dBm
[10:22:23:280]Allowed channel: mode=1 chan=10 freq=2457 MHz max_tx_power=20 dBm
[10:22:23:281]Allowed channel: mode=1 chan=11 freq=2462 MHz max_tx_power=20 dBm
[10:22:23:291]Allowed channel: mode=0 chan=1 freq=2412 MHz max_tx_power=20 dBm
[10:22:23:291]Allowed channel: mode=0 chan=2 freq=2417 MHz max_tx_power=20 dBm
[10:22:23:292]Allowed channel: mode=0 chan=3 freq=2422 MHz max_tx_power=20 dBm
[10:22:23:296]Allowed channel: mode=0 chan=4 freq=2427 MHz max_tx_power=20 dBm
[10:22:23:303]Allowed channel: mode=0 chan=5 freq=2432 MHz max_tx_power=20 dBm
[10:22:23:304]Allowed channel: mode=0 chan=6 freq=2437 MHz max_tx_power=20 dBm
[10:22:23:315]Allowed channel: mode=0 chan=7 freq=2442 MHz max_tx_power=20 dBm
[10:22:23:320]Allowed channel: mode=0 chan=8 freq=2447 MHz max_tx_power=20 dBm
[10:22:23:338]Allowed channel: mode=0 chan=9 freq=2452 MHz max_tx_power=20 dBm
[10:22:23:339]Allowed channel: mode=0 chan=10 freq=2457 MHz max_tx_power=20 dBm
[10:22:23:353]Allowed channel: mode=0 chan=11 freq=2462 MHz max_tx_power=20 dBm
[10:22:23:353]Scan for neighboring BSSes to select channel
[10:22:23:353]wlan0: nl80211: scan request
[10:22:23:353]nl80211: Passive scan requested
[10:22:23:354]Scan requested (ret=0) - scan timeout 10 seconds
[10:22:23:366]CONFIG_ACS was not set. use custom ACS
[10:22:23:366]Interface initialization will be completed in a callback (ACS)
[10:22:23:367]nl80211: Event message available
[10:22:23:379]nl80211: Drv Event 33 (NL80211_CMD_TRIGGER_SCAN) received for wlan0
[10:22:23:380]wlan0: nl80211: Scan trigger
[10:22:23:380]wlan0: Event SCAN_STARTED (47) received
[10:22:23:381]Unknown event 47
[10:22:24:670]nl80211: Event message available
[10:22:24:671]nl80211: Drv Event 42 (NL80211_CMD_REG_BEACON_HINT) received for wlan0
[10:22:24:682]nl80211: Regulatory beacon hint
[10:22:24:683]wlan0: Event CHANNEL_LIST_CHANGED (28) received
[10:22:25:298]nl80211: Event message available
[10:22:25:317]nl80211: Drv Event 42 (NL80211_CMD_REG_BEACON_HINT) received for wlan0
[10:22:25:319]nl80211: Regulatory beacon hint
[10:22:25:327]wlan0: Event CHANNEL_LIST_CHANGED (28) received
[10:22:25:490]nl80211: Event message available
[10:22:25:514]nl80211: Drv Event 42 (NL80211_CMD_REG_BEACON_HINT) received for wlan0
[10:22:25:515]nl80211: Regulatory beacon hint
[10:22:25:522]wlan0: Event CHANNEL_LIST_CHANGED (28) received
[10:22:25:588]nl80211: Event message available
[10:22:25:593]nl80211: Drv Event 42 (NL80211_CMD_REG_BEACON_HINT) received for wlan0
[10:22:25:605]nl80211: Regulatory beacon hint
[10:22:25:605]wlan0: Event CHANNEL_LIST_CHANGED (28) received
[10:22:28:068]nl80211: Event message available
[10:22:28:083]nl80211: Drv Event 34 (NL80211_CMD_NEW_SCAN_RESULTS) received for wlan0
[10:22:28:086]wlan0: nl80211: New scan results available
[10:22:28:102]nl80211: Scan included frequencies: 2412 2417 2422 2427 2432 2437 2442 2447 2452 2457 2462 2467 2472 2484 5180 5190 5200 5210 5220 5230 5240 5260 5280 5300 5320 5500 5520 5540 5560 5580 5600 5620 5640 5660 5680 5700 5745 5765 5785 5805 5825
[10:22:28:119]wlan0: Event SCAN_RESULTS (3) received
[10:22:28:120]nl80211: Received scan results (26 BSSes)
[10:22:28:120]1 BSSes on ch 36
[10:22:28:120]1 BSSes on ch 149
[10:22:28:121]2 BSSes on ch 149
[10:22:28:133]1 BSSes on ch 157
[10:22:28:133]1 BSSes on ch 161
[10:22:28:133]2 BSSes on ch 161
[10:22:28:133]Could not select channel automatically
[10:22:28:134]Interface initialization failed
[10:22:28:146]wlan0: interface state COUNTRY_UPDATE->DISABLED
[10:22:28:146]wlan0: AP-DISABLED 
[10:22:28:147]hostapd_interface_deinit_free(0x15f148)
[10:22:28:157]hostapd_interface_deinit_free: num_bss=1 conf->num_bss=1
[10:22:28:158]hostapd_interface_deinit(0x15f148)
[10:22:28:162]wlan0: interface state DISABLED->DISABLED
[10:22:28:171]hostapd_bss_deinit: deinit bss wlan0
[10:22:28:172]wlan0: Deauthenticate all stations
[10:22:28:185]nl80211: send_mlme - da= ff:ff:ff:ff:ff:ff noack=0 freq=0 no_cck=0 offchanok=0 wait_time=0 fc=0xc0 (WLAN_FC_STYPE_DEAUTH) nlmode=3
[10:22:28:186]nl80211: send_mlme -> send_frame
[10:22:28:186]nl80211: send_frame - Use bss->freq=0
[10:22:28:186]nl80211: send_frame -> send_frame_cmd
[10:22:28:187]nl80211: CMD_FRAME freq=0 wait=0 no_cck=0 no_ack=0 offchanok=0
[10:22:28:197]CMD_FRAME - hexdump(len=26): c0 00 00 00 ff ff ff ff ff ff 04 79 b7 fa 2d 73 04 79 b7 fa 2d 73 00 00 03 00
[10:22:28:206]nl80211: Frame command failed: ret=-22 (Invalid argument) (freq=0 wait=0)
[10:22:28:207]wlan0: AP-DISABLED 
[10:22:28:211]hostapd_cleanup(hapd=0x15fdc8 (wlan0))
[10:22:28:218]hostapd_free_hapd_data: Interface wlan0 wasn't started
[10:22:28:220]hostapd_interface_deinit_free: driver=0x116b9c drv_priv=0x160850 -> hapd_deinit
[10:22:28:233]nl80211: deinit ifname=wlan0 disabled_11b_rates=0
[10:22:28:233]nl80211: Remove monitor interface: refcount=0
[10:22:28:234]nl80211: Remove beacon (ifindex=3)
[10:22:28:246]netlink: Operstate: ifindex=3 linkmode=0 (kernel-control), operstate=6 (IF_OPER_UP)
[10:22:28:247]nl80211: Set mode ifindex 3 iftype 2 (STATION)
[10:22:28:257]<6>[   99.400000] wlcore: down
[10:22:28:261]nl80211: Teardown AP(wlan0) - device_ap_sme=0 use_monitor=0
[10:22:28:270]nl80211: Unsubscribe mgmt frames handle 0x889e81b1 (AP teardown)
[10:22:28:271]hostapd_interface_free(0x15f148)
[10:22:28:271]hostapd_interface_free: free hapd 0x15fdc8
[10:22:28:272]hostapd_cleanup_iface(0x15f148)
[10:22:28:283]hostapd_cleanup_iface_partial(0x15f148)
[10:22:28:284]hostapd_cleanup_iface: free iface=0x15f148
[10:22:29:404]root@hi-target:/mnt/p1/wg7833# 
[10:22:29:601]root@hi-target:/mnt/p1/wg7833# 
[10:22:29:766]root@hi-target:/mnt/p1/wg7833# 
[10:22:29:926]root@hi-target:/mnt/p1/wg7833# 
[10:22:30:073]root@hi-target:/mnt/p1/wg7833# 
[10:22:30:974]root@hi-target:/mnt/p1/wg7833# ./hostapd -dd hostapd.conf 
[10:22:31:015]random: Trying to read entropy from /dev/random
[10:22:31:016]Configuration file: hostapd.conf
[10:22:31:030]Line 8: DEPRECATED: 'dump_file' configuration variable is not used anymore
[10:22:31:030]nl80211: Supported cipher 00-0f-ac:1
[10:22:31:031]nl80211: Supported cipher 00-0f-ac:5
[10:22:31:040]nl80211: Supported cipher 00-0f-ac:2
[10:22:31:040]nl80211: Supported cipher 00-0f-ac:4
[10:22:31:045]nl80211: Supported cipher 00-14-72:1
[10:22:31:054]nl80211: Supports Probe Response offload in AP mode
[10:22:31:054]nl80211: Using driver-based off-channel TX
[10:22:31:055]nl80211: Supported vendor command: vendor_id=0x80028 subcmd=0
[10:22:31:069]nl80211: Supported vendor command: vendor_id=0x80028 subcmd=1
[10:22:31:069]nl80211: Supported vendor command: vendor_id=0x80028 subcmd=2
[10:22:31:069]nl80211: Supported vendor event: vendor_id=0x80028 subcmd=0
[10:22:31:070]nl80211: Supported vendor event: vendor_id=0x80028 subcmd=1
[10:22:31:080]nl80211: Use separate P2P group interface (driver advertised support)
[10:22:31:089]nl80211: Enable multi-channel concurrent (driver advertised support)
[10:22:31:090]nl80211: use P2P_DEVICE support
[10:22:31:090]nl80211: interface wlan0 in phy phy0
[10:22:31:095]nl80211: Set mode ifindex 3 iftype 3 (AP)
[10:22:31:106]<6>[  102.330000] wlcore: down
[10:22:31:110]nl80211: Setup AP(wlan0) - device_ap_sme=0 use_monitor=0
[10:22:31:120]nl80211: Subscribe to mgmt frames with AP handle 0x160938
[10:22:31:122]nl80211: Register frame type=0xb0 (WLAN_FC_STYPE_AUTH) nl_handle=0x160938 match=
[10:22:31:136]nl80211: Register frame type=0x0 (WLAN_FC_STYPE_ASSOC_REQ) nl_handle=0x160938 match=
[10:22:31:136]nl80211: Register frame type=0x20 (WLAN_FC_STYPE_REASSOC_REQ) nl_handle=0x160938 match=
[10:22:31:137]nl80211: Register frame type=0xa0 (WLAN_FC_STYPE_DISASSOC) nl_handle=0x160938 match=
[10:22:31:146]nl80211: Register frame type=0xc0 (WLAN_FC_STYPE_DEAUTH) nl_handle=0x160938 match=
[10:22:31:159]nl80211: Register frame type=0xd0 (WLAN_FC_STYPE_ACTION) nl_handle=0x160938 match=
[10:22:31:165]nl80211: Register frame type=0x40 (WLAN_FC_STYPE_PROBE_REQ) nl_handle=0x160938 match=
[10:22:31:173]rfkill: initial event: idx=1 type=1 op=0 soft=0 hard=0
[10:22:31:174]nl80211: Add own interface ifindex 3 (ifidx_reason -1)
[10:22:31:174]nl80211: if_indices[16]: 3(-1)
[10:22:31:180]phy: phy0
[10:22:31:189]BSS count 1, BSSID mask 00:00:00:00:00:00 (0 bits)
[10:22:31:194]wlan0: interface state UNINITIALIZED->COUNTRY_UPDATE
[10:22:31:203]Previous country code 00, new country code US 
[10:22:31:203]Continue interface setup after channel list update
[10:22:31:203]ctrl_iface not configured!
[10:22:31:204]random: Got 20/20 bytes from /dev/random
[10:22:36:069]Channel list update timeout - try to continue anyway
[10:22:36:084]nl80211: Regulatory information - country=00
[10:22:36:084]nl80211: 2402-2472 @ 40 MHz 20 mBm
[10:22:36:085]nl80211: 2457-2482 @ 40 MHz 20 mBm (no IR)
[10:22:36:098]nl80211: 2474-2494 @ 20 MHz 20 mBm (no OFDM) (no IR)
[10:22:36:099]nl80211: 5170-5250 @ 160 MHz 20 mBm (no IR)
[10:22:36:108]nl80211: 5250-5330 @ 160 MHz 20 mBm (DFS) (no IR)
[10:22:36:109]nl80211: 5490-5730 @ 160 MHz 20 mBm (DFS) (no IR)
[10:22:36:114]nl80211: 5735-5835 @ 80 MHz 20 mBm (no IR)
[10:22:36:123]nl80211: 57240-63720 @ 2160 MHz 0 mBm
[10:22:36:128]nl80211: Added 802.11b mode based on 802.11g information
[10:22:36:138]Allowed channel: mode=1 chan=1 freq=2412 MHz max_tx_power=20 dBm
[10:22:36:139]Allowed channel: mode=1 chan=2 freq=2417 MHz max_tx_power=20 dBm
[10:22:36:150]Allowed channel: mode=1 chan=3 freq=2422 MHz max_tx_power=20 dBm
[10:22:36:150]Allowed channel: mode=1 chan=4 freq=2427 MHz max_tx_power=20 dBm
[10:22:36:150]Allowed channel: mode=1 chan=5 freq=2432 MHz max_tx_power=20 dBm
[10:22:36:151]Allowed channel: mode=1 chan=6 freq=2437 MHz max_tx_power=20 dBm
[10:22:36:164]Allowed channel: mode=1 chan=7 freq=2442 MHz max_tx_power=20 dBm
[10:22:36:166]Allowed channel: mode=1 chan=8 freq=2447 MHz max_tx_power=20 dBm
[10:22:36:176]Allowed channel: mode=1 chan=9 freq=2452 MHz max_tx_power=20 dBm
[10:22:36:181]Allowed channel: mode=1 chan=10 freq=2457 MHz max_tx_power=20 dBm
[10:22:36:191]Allowed channel: mode=1 chan=11 freq=2462 MHz max_tx_power=20 dBm
[10:22:36:196]Allowed channel: mode=2 chan=36 freq=5180 MHz max_tx_power=20 dBm
[10:22:36:204]Allowed channel: mode=2 chan=149 freq=5745 MHz max_tx_power=20 dBm
[10:22:36:205]Allowed channel: mode=2 chan=157 freq=5785 MHz max_tx_power=20 dBm
[10:22:36:218]Allowed channel: mode=2 chan=161 freq=5805 MHz max_tx_power=20 dBm
[10:22:36:218]Allowed channel: mode=0 chan=1 freq=2412 MHz max_tx_power=20 dBm
[10:22:36:219]Allowed channel: mode=0 chan=2 freq=2417 MHz max_tx_power=20 dBm
[10:22:36:232]Allowed channel: mode=0 chan=3 freq=2422 MHz max_tx_power=20 dBm
[10:22:36:233]Allowed channel: mode=0 chan=4 freq=2427 MHz max_tx_power=20 dBm
[10:22:36:242]Allowed channel: mode=0 chan=5 freq=2432 MHz max_tx_power=20 dBm
[10:22:36:247]Allowed channel: mode=0 chan=6 freq=2437 MHz max_tx_power=20 dBm
[10:22:36:256]Allowed channel: mode=0 chan=7 freq=2442 MHz max_tx_power=20 dBm
[10:22:36:261]Allowed channel: mode=0 chan=8 freq=2447 MHz max_tx_power=20 dBm
[10:22:36:268]Allowed channel: mode=0 chan=9 freq=2452 MHz max_tx_power=20 dBm
[10:22:36:269]Allowed channel: mode=0 chan=10 freq=2457 MHz max_tx_power=20 dBm
[10:22:36:281]Allowed channel: mode=0 chan=11 freq=2462 MHz max_tx_power=20 dBm
[10:22:36:281]Scan for neighboring BSSes to select channel
[10:22:36:281]wlan0: nl80211: scan request
[10:22:36:282]nl80211: Passive scan requested
[10:22:36:292]Scan requested (ret=0) - scan timeout 10 seconds
[10:22:36:296]CONFIG_ACS was not set. use custom ACS
[10:22:36:308]Interface initialization will be completed in a callback (ACS)
[10:22:36:308]nl80211: Event message available
[10:22:36:308]nl80211: Drv Event 33 (NL80211_CMD_TRIGGER_SCAN) received for wlan0
[10:22:36:308]wlan0: nl80211: Scan trigger
[10:22:36:308]wlan0: Event SCAN_STARTED (47) received
[10:22:36:313]Unknown event 47
[10:22:37:262]nl80211: Event message available
[10:22:37:276]nl80211: Drv Event 42 (NL80211_CMD_REG_BEACON_HINT) received for wlan0
[10:22:37:277]nl80211: Regulatory beacon hint
[10:22:37:287]wlan0: Event CHANNEL_LIST_CHANGED (28) received
[10:22:40:913]nl80211: Event message available
[10:22:40:914]nl80211: Drv Event 34 (NL80211_CMD_NEW_SCAN_RESULTS) received for wlan0
[10:22:40:921]wlan0: nl80211: New scan results available
[10:22:40:932]nl80211: Scan included frequencies: 2412 2417 2422 2427 2432 2437 2442 2447 2452 2457 2462 2467 2472 2484 5180 5190 5200 5210 5220 5230 5240 5260 5280 5300 5320 5500 5520 5540 5560 5580 5600 5620 5640 5660 5680 5700 5745 5765 5785 5805 5825
[10:22:40:950]wlan0: Event SCAN_RESULTS (3) received
[10:22:40:951]nl80211: Received scan results (35 BSSes)
[10:22:40:952]1 BSSes on ch 36
[10:22:40:960]1 BSSes on ch 149
[10:22:40:960]2 BSSes on ch 149
[10:22:40:960]1 BSSes on ch 157
[10:22:40:960]1 BSSes on ch 161
[10:22:40:960]2 BSSes on ch 161
[10:22:40:963]Min APs found in channel 36 (AP count 1)
[10:22:40:971]Auto-selected channel: 36 secondary: 0
[10:22:40:971]Completing interface initialization
[10:22:40:979]Mode: IEEE 802.11a  Channel: 36  Frequency: 5180 MHz
[10:22:40:984]DFS 0 channels required radar detection
[10:22:40:992]nl80211: Set freq 5180 (ht_enabled=1, vht_enabled=0, bandwidth=20 MHz, cf1=5180 MHz, cf2=0 MHz)
[10:22:40:992]  * freq=5180
[10:22:40:992]  * vht_enabled=0
[10:22:40:992]  * ht_enabled=1
[10:22:40:992]  * sec_channel_offset=0
[10:22:40:995]  * channel_type=1
[10:22:41:004]RATE[0] rate=60 flags=0x1
[10:22:41:004]RATE[1] rate=90 flags=0x0
[10:22:41:004]RATE[2] rate=120 flags=0x1
[10:22:41:004]RATE[3] rate=180 flags=0x0
[10:22:41:005]RATE[4] rate=240 flags=0x1
[10:22:41:017]RATE[5] rate=360 flags=0x0
[10:22:41:017]RATE[6] rate=480 flags=0x0
[10:22:41:017]RATE[7] rate=540 flags=0x0
[10:22:41:018]hostapd_setup_bss(hapd=0x15fdc8 (wlan0), first=1)
[10:22:41:028]wlan0: Flushing old station entries
[10:22:41:028]nl80211: flush -> DEL_STATION wlan0 (all)
[10:22:41:029]wlan0: Deauthenticate all stations
[10:22:41:035]nl80211: send_mlme - da= ff:ff:ff:ff:ff:ff noack=0 freq=0 no_cck=0 offchanok=0 wait_time=0 fc=0xc0 (WLAN_FC_STYPE_DEAUTH) nlmode=3
[10:22:41:048]nl80211: send_mlme -> send_frame
[10:22:41:048]nl80211: send_frame - Use bss->freq=5180
[10:22:41:049]nl80211: send_frame -> send_frame_cmd
[10:22:41:057]nl80211: CMD_FRAME freq=5180 wait=0 no_cck=0 no_ack=0 offchanok=0
[10:22:41:071]CMD_FRAME - hexdump(len=26): c0 00 00 00 ff ff ff ff ff ff 04 79 b7 fa 2d 73 04 79 b7 fa 2d 73 00 00 02 00
[10:22:41:072]nl80211: Frame command failed: ret=-16 (Device or resource busy) (freq=5180 wait=0)
[10:22:41:082]wpa_driver_nl80211_set_key: ifindex=3 (wlan0) alg=0 addr=(nil) key_idx=0 set_tx=0 seq_len=0 key_len=0
[10:22:41:089]wpa_driver_nl80211_set_key: ifindex=3 (wlan0) alg=0 addr=(nil) key_idx=1 set_tx=0 seq_len=0 key_len=0
[10:22:41:103]wpa_driver_nl80211_set_key: ifindex=3 (wlan0) alg=0 addr=(nil) key_idx=2 set_tx=0 seq_len=0 key_len=0
[10:22:41:115]wpa_driver_nl80211_set_key: ifindex=3 (wlan0) alg=0 addr=(nil) key_idx=3 set_tx=0 seq_len=0 key_len=0
[10:22:41:115]Using interface wlan0 with hwaddr 04:79:b7:fa:2d:73 and ssid "15435007"
[10:22:41:116]Deriving WPA PSK based on passphrase
[10:22:41:126]SSID - hexdump_ascii(len=8):
[10:22:41:127]     31 35 34 33 35 30 30 37                           15435007        
[10:22:41:132]PSK (ASCII passphrase) - hexdump_ascii(len=8): [REMOVED]
[10:22:41:282]PSK (from passphrase) - hexdump(len=32): [REMOVED]
[10:22:41:293]nl80211: Set beacon (beacon_set=0)
[10:22:41:306]nl80211: Beacon head - hexdump(len=59): 80 00 00 00 ff ff ff ff ff ff 04 79 b7 fa 2d 73 04 79 b7 fa 2d 73 00 00 00 00 00 00 00 00 00 00 64 00 21 00 00 08 31 35 34 33 35 30 30 37 01 08 8c 12 98 24 b0 48 60 6c 03 01 24
[10:22:41:325]nl80211: Beacon tail - hexdump(len=106): 07 0c 55 53 20 24 01 14 95 01 14 9d 02 14 3b 02 73 00 2d 1a 0c 00 1d ff 00 00 00 00 00 00 00 00 00 96 00 01 00 00 00 00 00 00 00 00 00 00 3d 16 24 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 7f 08 04 00 00 00 00 00 00 40 dd 18 00 50 f2 02 01 01 00 00 03 a4 00 00 27 a4 00 00 42 43 5e 00 62 32 2f 00
[10:22:41:347]nl80211: ifindex=3
[10:22:41:355]nl80211: beacon_int=100
[10:22:41:356]nl80211: dtim_period=2
[10:22:41:357]nl80211: ssid - hexdump_ascii(len=8):
[10:22:41:365]     31 35 34 33 35 30 30 37                           15435007        
[10:22:41:367]  * beacon_int=100
[10:22:41:384]nl80211: proberesp (offload) - hexdump(len=165): 50 00 00 00 00 00 00 00 00 00 04 79 b7 fa 2d 73 04 79 b7 fa 2d 73 00 00 00 00 00 00 00 00 00 00 64 00 21 00 00 08 31 35 34 33 35 30 30 37 01 08 8c 12 98 24 b0 48 60 6c 03 01 24 07 0c 55 53 20 24 01 14 95 01 14 9d 02 14 3b 02 73 00 2d 1a 0c 00 1d ff 00 00 00 00 00 00 00 00 00 96 00 01 00 00 00 00 00 00 00 00 00 00 3d 16 24 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 7f 08 04 00 00 00 00 00 00 40 dd 18 00 50 f2 02 01 01 00 00 03 a4 00 00 27 a4 00 00 42 43 5e 00 62 32 2f 00
[10:22:41:415]nl80211: hidden SSID not in use
[10:22:41:423]nl80211: privacy=0
[10:22:41:423]nl80211: auth_algs=0x1
[10:22:41:423]nl80211: wpa_version=0x0
[10:22:41:423]nl80211: key_mgmt_suites=0x4
[10:22:41:424]nl80211: pairwise_ciphers=0x0
[10:22:41:435]nl80211: group_cipher=0x1
[10:22:41:435]nl80211: SMPS mode - off
[10:22:41:436]nl80211: beacon_ies - hexdump(len=10): 7f 08 04 00 00 00 00 00 00 40
[10:22:41:445]nl80211: proberesp_ies - hexdump(len=10): 7f 08 04 00 00 00 00 00 00 40
[10:22:41:454]nl80211: assocresp_ies - hexdump(len=10): 7f 08 04 00 00 00 00 00 00 40
[10:22:41:455]nl80211: Set wlan0 operstate 0->1 (UP)
[10:22:41:455]netlink: Operstate: ifindex=3 linkmode=-1 (no change), operstate=6 (IF_OPER_UP)
[10:22:41:464]wlan0: interface state COUNTRY_UPDATE->ENABLED
[10:22:41:465]wlan0: AP-ENABLED 
[10:22:41:466]wlan0: Setup of interface done.
[10:22:41:472]RTM_NEWLINK: ifi_index=3 ifname=wlan0 operstate=6 linkmode=0 ifi_family=0 ifi_flags=0x11043 ([UP][RUNNING][LOWER_UP])