Other Parts Discussed in Thread: TM4C1294NCPDT, , SEGGER, UNIFLASH
Hi Everyone,
I own a launchpad with the CC3235SF and on it there are two main chips, the CC3235SF itself and the TM4C1294NCPDT. My end goal is to make a slimmed-down version of the CC3235 on a smaller board but I'm wondering what the function of the TM4C1294NCPDT is? Judging from the document it seems this is just additional support for JTAG debugging? If I remove this and put the CC3235 on a custom board whatever software loading/debugging options do I have? Can I load firmware for the CC3235 onto a SPI chip via USB by a FTDI chip like an esp8266? If possible I would like the CC3235 to be on a standalone board with an SPI flash chip talking to an USB-to-COM to load my software from code studios. Thanks for any pointers!!! :)