This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS / CC3220SF-LAUNCHXL: Unable to connect the device to uniflash under Linux

Part Number: CC3220SF-LAUNCHXL
Other Parts Discussed in Thread: CC3220SF, UNIFLASH, CC2640R2F

Tool/software: Code Composer Studio

Recently I've been exploring routines for CC3220SF,Learn to program the external serial flash used by SimpleLink Wi-Fi CC32xx and CC31xx devices using UniFlash:

dev.ti.com/.../node

I noticed that my CC3220SF cannot connect to UniFlash (although UniFlash has recognized CC3220SF),whenever i tried connection the device using Uniflash it's going to load infinitely

Confirm that the SOP jumper is 010,When "Start Image Creator" is pressed, the interface of Uniflash does not change and is always under load.I tried several Linux PC, but failed to connect with Uniflash.

Later, I used Uniflash under Windows, and CC3220SF connected successfully!

1. I have downloaded Uniflash again and tried several versions, including the latest version, but failed to connect.

2. Other TI-Launchpad devices (such as CC2640R2F) can be recognized by USB and UNIFlash normally

3. what should I do ?  Some Settings not configured properly?