Hi,
I am using AWS_demo project. I would like to control GPIO_04. However, the system crash whenever I call GPIO_write( GPIOCC32XX_GPIO_04).
It is weird that if I change GPIO_04 to another pin GPIO_17, it works well.
Following is my code of GPIO configuration for using GPIO_04. This cause system crash. If I remark GPIO_04 and unremark GPIO_17, the system works well when calling GPIO_write( GPIOCC32XX_GPIO_17).
GPIO_PinConfig gpioPinConfigs[] = {
/* input pins with callbacks */
/* CC3220SF_LAUNCHXL_GPIO_SW2 */
GPIOCC32XX_GPIO_13 | GPIO_CFG_INPUT | GPIO_CFG_IN_INT_NONE,
/* CC3220SF_LAUNCHXL_GPIO_SW3 */
// GPIOCC32XX_GPIO_04 | GPIO_CFG_INPUT | GPIO_CFG_IN_INT_NONE,
/* output pins */
/* CC3220SF_LAUNCHXL_GPIO_LED_D6 */
// GPIOCC32XX_GPIO_17 | GPIO_CFG_OUT_STD | GPIO_CFG_OUT_STR_HIGH | GPIO_CFG_OUT_LOW,
/* CC3220SF_LAUNCHXL_GPIO_LED_D7 */
GPIOCC32XX_GPIO_04 | GPIO_CFG_OUT_STD | GPIO_CFG_OUT_STR_HIGH | GPIO_CFG_OUT_LOW,
/* CC3220SF_LAUNCHXL_GPIO_LED_D5 */
GPIOCC32XX_GPIO_11 | GPIO_CFG_OUT_STD | GPIO_CFG_OUT_STR_HIGH | GPIO_CFG_OUT_LOW,
};
Martin