Hello,
I am doing a test on new hardware based on cc3200R1 ,i face a problem of General event and Wlan error here the scenario:
**I reset the device many times (it closes tcp sockets then it disconnect from router) i do that sevral times then i start to have connection issue
1-it takes time to connect showing the General event error many times
2-when it connects it doesn't get stable and the connection get broken again and again with WLAN ERROR and General event when it tries to connect again.
**If i do not do multiple reset the device is more stable but from time to time i get WLAN ERROR and the connection get lost
Remarks;
the device is close to the router
and here is the RF schematic design