Other Parts Discussed in Thread: CC3220SF
Hello Champs,
In CC3220SF datasheet there is below description for UART:
--------------------------------------------------------------------------------------------------------
5.15.6.8 UART
The CC3220x device includes two UARTs with the following features:
• Programmable baud-rate generator allowing speeds up to 3 Mbps
---------------------------------------------------------------------------------------------
But in CC3220MODASF datasheet, there is no such description for UART maximum baud rate.
So my questions are:
1) Is the maximum baud rate for CC3220MODASF the same as CC3220SF, that is to say, up to 3 Mbps?
2) If yes, is there any test report or document to show whether 3M bps can be reached or not in applications?
Would you please kindly help? Thanks!
Best Regards,
Linda