1. i am using SDK 1.5 Mqtt client example and it is not re connecting after disconnect from mqtt server because of network disconnection.Please refer the below console logs and attched Main.c file.
2. Same code some times hangup in sl_ExtLib_MqttClientDisconnect function when it fails in subscribe
*************************************************
CC3200 MQTT_Client Application
*************************************************
Host Driver Version: 1.0.1.14
Build Version 2.0.7.0.31.0.0.4.1.1.5.3.3
Device is configured in default state
Started SimpleLink Device: STA Mode
[WLAN EVENT] STA Connected to the AP: TREQ-1783 , BSSID: b0:b9:8a:b4:17:83
[NETAPP EVENT] IP acquired by the device
Device has connected to TREQ-1783
Device IP Address is 192.168.1.55
Version: Client LIB 1.4.0, Common LIB 1.5.0.
C: Alloc for 1 200266e4
C: FH-B1 0x10 to net 16, Sent (45 Bytes) [@ 159]
C: Alloc for 0 200266e4
C: Rcvd msg Fix-Hdr (Byte1) 0x20 from net 16 [@ 159]
C: Cleaning session for net 16
C: Msg w/ ID 0x0000, processing status: Good
C: Alloc for 0 200266e4
Success: conn to Broker no. 1
C: Alloc for 8 200266c0
C: FH-B1 0x82 to net 16, Sent (79 Bytes) [@ 159]
C: Rcvd msg Fix-Hdr (Byte1) 0x90 from net 16 [@ 159]
C: Msg w/ ID 0x0001, processing status: Good
C: Alloc for 0 200266e4
Client subscribed on following topics:
/cc3200/ToggleLEDCmdL1
/cc3200/ToggleLEDCmdL2
/cc3200/ToggleLEDCmdL3
[WLAN ERROR]Device disconnected from the AP AP: TREQ-1783, BSSID: b0:b9:8a:b4:17:83 on an ERROR..!!
C: Net 16, Raw Error -1, Time Out: Y [184]
C: FH-B1 0xc0 to net 16, Sent (2 Bytes) [@ 184]
C: Net 16, Raw Error -1, Time Out: N [194]
C: RX closing Net 16 [-1]
C: Cleaning session for net 16
C: Net 16 now closed
disconnect from broker mqtt.eclipse.org
device has disconnected from AP
retry connection to the AP
[WLAN EVENT] STA Connected to the AP: TREQ-1783 , BSSID: b0:b9:8a:b4:17:83
[NETAPP EVENT] IP acquired by the device
C: Alloc for 1 200266e4
Broker connect fail for conn no. 1
//***************************************************************************** // Copyright (C) 2014 Texas Instruments Incorporated // // All rights reserved. Property of Texas Instruments Incorporated. // Restricted rights to use, duplicate or disclose this code are // granted through contract. // The program may not be used without the written permission of // Texas Instruments Incorporated or against the terms and conditions // stipulated in the agreement under which this program has been supplied, // and under no circumstances can it be used with non-TI connectivity device. // //***************************************************************************** //***************************************************************************** // // Application Name - MQTT Client // Application Overview - This application acts as a MQTT client and connects // to the IBM MQTT broker, simultaneously we can // connect a web client from a web browser. Both // clients can inter-communicate using appropriate // topic names. // //***************************************************************************** //***************************************************************************** // //! \addtogroup mqtt_client //! @{ // //***************************************************************************** // Standard includes #include <stdlib.h> // simplelink includes #include "simplelink.h" // driverlib includes #include "hw_types.h" #include "hw_ints.h" #include "hw_memmap.h" #include "interrupt.h" #include "rom_map.h" #include "prcm.h" #include "uart.h" #include "timer.h" // common interface includes #include "network_if.h" #ifndef NOTERM #include "uart_if.h" #endif #include "button_if.h" #include "gpio_if.h" #include "timer_if.h" #include "common.h" #include "utils.h" #include "sl_mqtt_client.h" // application specific includes #include "pinmux.h" #define APPLICATION_VERSION "1.4.0" /*Operate Lib in MQTT 3.1 mode.*/ #define MQTT_3_1_1 false /*MQTT 3.1.1 */ #define MQTT_3_1 true /*MQTT 3.1*/ #define WILL_TOPIC "Client" #define WILL_MSG "Client Stopped" #define WILL_QOS QOS2 #define WILL_RETAIN false /*Defining Broker IP address and port Number*/ #define SERVER_ADDRESS "mqtt.eclipse.org" #define SERVER_IP_ADDRESS "192.168.178.67" #define PORT_NUMBER 1883 #define SECURED_PORT_NUMBER 8883 #define LOOPBACK_PORT 1882 #define MAX_BROKER_CONN 1 #define SERVER_MODE MQTT_3_1 /*Specifying Receive time out for the Receive task*/ #define RCV_TIMEOUT 30 /*Background receive task priority*/ #define TASK_PRIORITY 3 /* Keep Alive Timer value*/ #define KEEP_ALIVE_TIMER 25 /*Clean session flag*/ #define CLEAN_SESSION true /*Retain Flag. Used in publish message. */ #define RETAIN 1 /*Defining Publish Topic*/ #define PUB_TOPIC_FOR_SW3 "/cc3200/ButtonPressEvtSw3" #define PUB_TOPIC_FOR_SW2 "/cc3200/ButtonPressEvtSw2" /*Defining Number of topics*/ #define TOPIC_COUNT 3 /*Defining Subscription Topic Values*/ #define TOPIC1 "/cc3200/ToggleLEDCmdL1" #define TOPIC2 "/cc3200/ToggleLEDCmdL2" #define TOPIC3 "/cc3200/ToggleLEDCmdL3" /*Defining QOS levels*/ #define QOS0 0 #define QOS1 1 #define QOS2 2 /*Spawn task priority and OSI Stack Size*/ #define OSI_STACK_SIZE 2048 #define UART_PRINT Report typedef struct connection_config{ SlMqttClientCtxCfg_t broker_config; void *clt_ctx; unsigned char *client_id; unsigned char *usr_name; unsigned char *usr_pwd; bool is_clean; unsigned int keep_alive_time; SlMqttClientCbs_t CallBAcks; int num_topics; char *topic[TOPIC_COUNT]; unsigned char qos[TOPIC_COUNT]; SlMqttWill_t will_params; bool is_connected; }connect_config; typedef enum { PUSH_BUTTON_SW2_PRESSED, PUSH_BUTTON_SW3_PRESSED, BROKER_DISCONNECTION }events; typedef struct { void * hndl; events event; }event_msg; //***************************************************************************** // LOCAL FUNCTION PROTOTYPES //***************************************************************************** static void Mqtt_Recv(void *app_hndl, const char *topstr, long top_len, const void *payload, long pay_len, bool dup,unsigned char qos, bool retain); static void sl_MqttEvt(void *app_hndl,long evt, const void *buf, unsigned long len); static void sl_MqttDisconnect(void *app_hndl); void pushButtonInterruptHandler2(); void pushButtonInterruptHandler3(); void ToggleLedState(ledEnum LedNum); void TimerPeriodicIntHandler(void); void LedTimerConfigNStart(); void LedTimerDeinitStop(); void BoardInit(void); static void DisplayBanner(char * AppName); void MqttClient(void *pvParameters); //***************************************************************************** // GLOBAL VARIABLES -- Start //***************************************************************************** #ifdef USE_FREERTOS #if defined(ewarm) extern uVectorEntry __vector_table; #endif #if defined(ccs) extern void (* const g_pfnVectors[])(void); #endif #endif unsigned short g_usTimerInts; /* AP Security Parameters */ SlSecParams_t SecurityParams = {0}; /*Message Queue*/ OsiMsgQ_t g_PBQueue; /* connection configuration */ connect_config usr_connect_config[] = { { { { SL_MQTT_NETCONN_URL, SERVER_ADDRESS, PORT_NUMBER, 0, 0, 0, NULL }, SERVER_MODE, true, }, NULL, "user1", NULL, NULL, true, KEEP_ALIVE_TIMER, {Mqtt_Recv, sl_MqttEvt, sl_MqttDisconnect}, TOPIC_COUNT, {TOPIC1, TOPIC2, TOPIC3}, {QOS2, QOS2, QOS2}, {WILL_TOPIC,WILL_MSG,WILL_QOS,WILL_RETAIN}, false } }; /* library configuration */ SlMqttClientLibCfg_t Mqtt_Client={ 0, TASK_PRIORITY, 30, true, (long(*)(const char *, ...))UART_PRINT }; /*Publishing topics and messages*/ const char *pub_topic_sw2 = PUB_TOPIC_FOR_SW2; const char *pub_topic_sw3 = PUB_TOPIC_FOR_SW3; unsigned char *data_sw2={"Push button sw2 is pressed on CC32XX device"}; unsigned char *data_sw3={"Push button sw3 is pressed on CC32XX device"}; void *app_hndl = (void*)usr_connect_config; //***************************************************************************** // GLOBAL VARIABLES -- End //***************************************************************************** //**************************************************************************** //! Defines Mqtt_Pub_Message_Receive event handler. //! Client App needs to register this event handler with sl_ExtLib_mqtt_Init //! API. Background receive task invokes this handler whenever MQTT Client //! receives a Publish Message from the broker. //! //!\param[out] topstr => pointer to topic of the message //!\param[out] top_len => topic length //!\param[out] payload => pointer to payload //!\param[out] pay_len => payload length //!\param[out] retain => Tells whether its a Retained message or not //!\param[out] dup => Tells whether its a duplicate message or not //!\param[out] qos => Tells the Qos level //! //!\return none //**************************************************************************** static void Mqtt_Recv(void *app_hndl, const char *topstr, long top_len, const void *payload, long pay_len, bool dup,unsigned char qos, bool retain) { char *output_str=(char*)malloc(top_len+1); memset(output_str,'\0',top_len+1); strncpy(output_str, (char*)topstr, top_len); output_str[top_len]='\0'; if(strncmp(output_str,TOPIC1, top_len) == 0) { ToggleLedState(LED1); } else if(strncmp(output_str,TOPIC2, top_len) == 0) { ToggleLedState(LED2); } else if(strncmp(output_str,TOPIC3, top_len) == 0) { ToggleLedState(LED3); } UART_PRINT("\n\rPublish Message Received"); UART_PRINT("\n\rTopic: "); UART_PRINT("%s",output_str); free(output_str); UART_PRINT(" [Qos: %d] ",qos); if(retain) UART_PRINT(" [Retained]"); if(dup) UART_PRINT(" [Duplicate]"); output_str=(char*)malloc(pay_len+1); memset(output_str,'\0',pay_len+1); strncpy(output_str, (char*)payload, pay_len); output_str[pay_len]='\0'; UART_PRINT("\n\rData is: "); UART_PRINT("%s",(char*)output_str); UART_PRINT("\n\r"); free(output_str); return; } //**************************************************************************** //! Defines sl_MqttEvt event handler. //! Client App needs to register this event handler with sl_ExtLib_mqtt_Init //! API. Background receive task invokes this handler whenever MQTT Client //! receives an ack(whenever user is in non-blocking mode) or encounters an error. //! //! param[out] evt => Event that invokes the handler. Event can be of the //! following types: //! MQTT_ACK - Ack Received //! MQTT_ERROR - unknown error //! //! //! \param[out] buf => points to buffer //! \param[out] len => buffer length //! //! \return none //**************************************************************************** static void sl_MqttEvt(void *app_hndl, long evt, const void *buf,unsigned long len) { int i; switch(evt) { case SL_MQTT_CL_EVT_PUBACK: UART_PRINT("PubAck:\n\r"); UART_PRINT("%s\n\r",buf); break; case SL_MQTT_CL_EVT_SUBACK: UART_PRINT("\n\rGranted QoS Levels are:\n\r"); for(i=0;i<len;i++) { UART_PRINT("QoS %d\n\r",((unsigned char*)buf)[i]); } break; case SL_MQTT_CL_EVT_UNSUBACK: UART_PRINT("UnSub Ack \n\r"); UART_PRINT("%s\n\r",buf); break; default: break; } } //**************************************************************************** // //! callback event in case of MQTT disconnection //! //! \param app_hndl is the handle for the disconnected connection //! //! return none // //**************************************************************************** static void sl_MqttDisconnect(void *app_hndl) { connect_config *local_con_conf; event_msg msg; local_con_conf = app_hndl; msg.hndl = app_hndl; msg.event = BROKER_DISCONNECTION; UART_PRINT("disconnect from broker %s\r\n", (local_con_conf->broker_config).server_info.server_addr); local_con_conf->is_connected = false; // // write message indicating publish message // osi_MsgQWrite(&g_PBQueue,&msg,OSI_NO_WAIT); } //**************************************************************************** // //! Push Button Handler1(GPIOS2). Press push button2 (GPIOSW2) Whenever user //! wants to publish a message. Write message into message queue signaling the //! event publish messages //! //! \param none //! //! return none // //**************************************************************************** void pushButtonInterruptHandler2() { event_msg msg; msg.event = PUSH_BUTTON_SW2_PRESSED; msg.hndl = NULL; // // write message indicating publish message // osi_MsgQWrite(&g_PBQueue,&msg,OSI_NO_WAIT); } //**************************************************************************** // //! Push Button Handler3(GPIOS3). Press push button3 (GPIOSW3) Whenever user //! wants to publish a message. Write message into message queue signaling the //! event publish messages //! //! \param none //! //! return none // //**************************************************************************** void pushButtonInterruptHandler3() { event_msg msg; msg.event = PUSH_BUTTON_SW3_PRESSED; msg.hndl = NULL; // // write message indicating exit from sending loop // osi_MsgQWrite(&g_PBQueue,&msg,OSI_NO_WAIT); } //**************************************************************************** // //! Toggles the state of GPIOs(LEDs) //! //! \param LedNum is the enumeration for the GPIO to be toggled //! //! \return none // //**************************************************************************** void ToggleLedState(ledEnum LedNum) { unsigned char ledstate = 0; switch(LedNum) { case LED1: ledstate = GPIO_IF_LedStatus(MCU_RED_LED_GPIO); if(!ledstate) { GPIO_IF_LedOn(MCU_RED_LED_GPIO); } else { GPIO_IF_LedOff(MCU_RED_LED_GPIO); } break; case LED2: ledstate = GPIO_IF_LedStatus(MCU_ORANGE_LED_GPIO); if(!ledstate) { GPIO_IF_LedOn(MCU_ORANGE_LED_GPIO); } else { GPIO_IF_LedOff(MCU_ORANGE_LED_GPIO); } break; case LED3: ledstate = GPIO_IF_LedStatus(MCU_GREEN_LED_GPIO); if(!ledstate) { GPIO_IF_LedOn(MCU_GREEN_LED_GPIO); } else { GPIO_IF_LedOff(MCU_GREEN_LED_GPIO); } break; default: break; } } //***************************************************************************** // //! Periodic Timer Interrupt Handler //! //! \param None //! //! \return None // //***************************************************************************** void TimerPeriodicIntHandler(void) { unsigned long ulInts; // // Clear all pending interrupts from the timer we are // currently using. // ulInts = MAP_TimerIntStatus(TIMERA0_BASE, true); MAP_TimerIntClear(TIMERA0_BASE, ulInts); // // Increment our interrupt counter. // g_usTimerInts++; if(!(g_usTimerInts & 0x1)) { // // Off Led // GPIO_IF_LedOff(MCU_RED_LED_GPIO); } else { // // On Led // GPIO_IF_LedOn(MCU_RED_LED_GPIO); } } //**************************************************************************** // //! Function to configure and start timer to blink the LED while device is //! trying to connect to an AP //! //! \param none //! //! return none // //**************************************************************************** void LedTimerConfigNStart() { // // Configure Timer for blinking the LED for IP acquisition // Timer_IF_Init(PRCM_TIMERA0,TIMERA0_BASE,TIMER_CFG_PERIODIC,TIMER_A,0); Timer_IF_IntSetup(TIMERA0_BASE,TIMER_A,TimerPeriodicIntHandler); Timer_IF_Start(TIMERA0_BASE,TIMER_A,100); } //**************************************************************************** // //! Disable the LED blinking Timer as Device is connected to AP //! //! \param none //! //! return none // //**************************************************************************** void LedTimerDeinitStop() { // // Disable the LED blinking Timer as Device is connected to AP // Timer_IF_Stop(TIMERA0_BASE,TIMER_A); Timer_IF_DeInit(TIMERA0_BASE,TIMER_A); } //***************************************************************************** // //! Board Initialization & Configuration //! //! \param None //! //! \return None // //***************************************************************************** void BoardInit(void) { /* In case of TI-RTOS vector table is initialize by OS itself */ #ifndef USE_TIRTOS // // Set vector table base // #if defined(ccs) IntVTableBaseSet((unsigned long)&g_pfnVectors[0]); #endif #if defined(ewarm) IntVTableBaseSet((unsigned long)&__vector_table); #endif #endif // // Enable Processor // MAP_IntMasterEnable(); MAP_IntEnable(FAULT_SYSTICK); PRCMCC3200MCUInit(); } //***************************************************************************** // //! Application startup display on UART //! //! \param none //! //! \return none //! //***************************************************************************** static void DisplayBanner(char * AppName) { UART_PRINT("\n\n\n\r"); UART_PRINT("\t\t *************************************************\n\r"); UART_PRINT("\t\t CC3200 %s Application \n\r", AppName); UART_PRINT("\t\t *************************************************\n\r"); UART_PRINT("\n\n\n\r"); } extern volatile unsigned long g_ulStatus; //***************************************************************************** // //! Task implementing MQTT client communication to other web client through //! a broker //! //! \param none //! //! This function //! 1. Initializes network driver and connects to the default AP //! 2. Initializes the mqtt library and set up MQTT connection configurations //! 3. set up the button events and their callbacks(for publishing) //! 4. handles the callback signals //! //! \return None //! //***************************************************************************** void MqttClient(void *pvParameters) { long lRetVal = -1; int iCount = 0; int iNumBroker = 0; int iConnBroker = 0; event_msg RecvQue; unsigned char policyVal; connect_config *local_con_conf = (connect_config *)app_hndl; // // Configure LED // GPIO_IF_LedConfigure(LED1|LED2|LED3); GPIO_IF_LedOff(MCU_RED_LED_GPIO); GPIO_IF_LedOff(MCU_GREEN_LED_GPIO); // // Reset The state of the machine // Network_IF_ResetMCUStateMachine(); // // Start the driver // lRetVal = Network_IF_InitDriver(ROLE_STA); if(lRetVal < 0) { UART_PRINT("Failed to start SimpleLink Device\n\r",lRetVal); LOOP_FOREVER(); } // switch on Green LED to indicate Simplelink is properly up GPIO_IF_LedOn(MCU_ON_IND); // Start Timer to blink Red LED till AP connection LedTimerConfigNStart(); // Initialize AP security params SecurityParams.Key = (signed char *)SECURITY_KEY; SecurityParams.KeyLen = strlen(SECURITY_KEY); SecurityParams.Type = SECURITY_TYPE; // // Connect to the Access Point // lRetVal = Network_IF_ConnectAP(SSID_NAME, SecurityParams); if(lRetVal < 0) { UART_PRINT("Connection to an AP failed\n\r"); LOOP_FOREVER(); } lRetVal = sl_WlanProfileAdd(SSID_NAME,strlen(SSID_NAME),0,&SecurityParams,0,1,0); //set AUTO policy lRetVal = sl_WlanPolicySet(SL_POLICY_CONNECTION, SL_CONNECTION_POLICY(1,0,0,0,0), &policyVal, 1 /*PolicyValLen*/); // // Disable the LED blinking Timer as Device is connected to AP // LedTimerDeinitStop(); // // Switch ON RED LED to indicate that Device acquired an IP // GPIO_IF_LedOn(MCU_IP_ALLOC_IND); UtilsDelay(20000000); GPIO_IF_LedOff(MCU_RED_LED_GPIO); GPIO_IF_LedOff(MCU_ORANGE_LED_GPIO); GPIO_IF_LedOff(MCU_GREEN_LED_GPIO); // // Register Push Button Handlers // Button_IF_Init(pushButtonInterruptHandler2,pushButtonInterruptHandler3); // // Initialze MQTT client lib // lRetVal = sl_ExtLib_MqttClientInit(&Mqtt_Client); if(lRetVal != 0) { // lib initialization failed UART_PRINT("MQTT Client lib initialization failed\n\r"); LOOP_FOREVER(); } /******************* connection to the broker ***************************/ iNumBroker = sizeof(usr_connect_config)/sizeof(connect_config); if(iNumBroker > MAX_BROKER_CONN) { UART_PRINT("Num of brokers are more then max num of brokers\n\r"); LOOP_FOREVER(); } connect_to_broker: while(iCount < iNumBroker) { //create client context local_con_conf[iCount].clt_ctx = sl_ExtLib_MqttClientCtxCreate(&local_con_conf[iCount].broker_config, &local_con_conf[iCount].CallBAcks, &(local_con_conf[iCount])); // // Set Client ID // sl_ExtLib_MqttClientSet((void*)local_con_conf[iCount].clt_ctx, SL_MQTT_PARAM_CLIENT_ID, local_con_conf[iCount].client_id, strlen((char*)(local_con_conf[iCount].client_id))); // // Set will Params // if(local_con_conf[iCount].will_params.will_topic != NULL) { sl_ExtLib_MqttClientSet((void*)local_con_conf[iCount].clt_ctx, SL_MQTT_PARAM_WILL_PARAM, &(local_con_conf[iCount].will_params), sizeof(SlMqttWill_t)); } // // setting username and password // if(local_con_conf[iCount].usr_name != NULL) { sl_ExtLib_MqttClientSet((void*)local_con_conf[iCount].clt_ctx, SL_MQTT_PARAM_USER_NAME, local_con_conf[iCount].usr_name, strlen((char*)local_con_conf[iCount].usr_name)); if(local_con_conf[iCount].usr_pwd != NULL) { sl_ExtLib_MqttClientSet((void*)local_con_conf[iCount].clt_ctx, SL_MQTT_PARAM_PASS_WORD, local_con_conf[iCount].usr_pwd, strlen((char*)local_con_conf[iCount].usr_pwd)); } } // // connectin to the broker // if((sl_ExtLib_MqttClientConnect((void*)local_con_conf[iCount].clt_ctx, local_con_conf[iCount].is_clean, local_con_conf[iCount].keep_alive_time) & 0xFF) != 0) { UART_PRINT("\n\rBroker connect fail for conn no. %d \n\r",iCount+1); //delete the context for this connection sl_ExtLib_MqttClientCtxDelete(local_con_conf[iCount].clt_ctx); break; } else { UART_PRINT("\n\rSuccess: conn to Broker no. %d\n\r ", iCount+1); local_con_conf[iCount].is_connected = true; iConnBroker++; } // // Subscribe to topics // if(sl_ExtLib_MqttClientSub((void*)local_con_conf[iCount].clt_ctx, local_con_conf[iCount].topic, local_con_conf[iCount].qos, TOPIC_COUNT) < 0) { UART_PRINT("\n\r Subscription Error for conn no. %d\n\r", iCount+1); UART_PRINT("Disconnecting from the broker\r\n"); sl_ExtLib_MqttClientDisconnect(local_con_conf[iCount].clt_ctx); local_con_conf[iCount].is_connected = false; //delete the context for this connection sl_ExtLib_MqttClientCtxDelete(local_con_conf[iCount].clt_ctx); iConnBroker--; break; } else { int iSub; UART_PRINT("Client subscribed on following topics:\n\r"); for(iSub = 0; iSub < local_con_conf[iCount].num_topics; iSub++) { UART_PRINT("%s\n\r", local_con_conf[iCount].topic[iSub]); } } iCount++; } if(iConnBroker < 1) { // // no succesful connection to broker // goto end; } iCount = 0; for(;;) { osi_MsgQRead( &g_PBQueue, &RecvQue, OSI_WAIT_FOREVER); if(PUSH_BUTTON_SW2_PRESSED == RecvQue.event) { Button_IF_EnableInterrupt(SW2); // // send publish message // sl_ExtLib_MqttClientSend((void*)local_con_conf[iCount].clt_ctx, pub_topic_sw2,data_sw2,strlen((char*)data_sw2),QOS2,RETAIN); UART_PRINT("\n\r CC3200 Publishes the following message \n\r"); UART_PRINT("Topic: %s\n\r",pub_topic_sw2); UART_PRINT("Data: %s\n\r",data_sw2); } else if(PUSH_BUTTON_SW3_PRESSED == RecvQue.event) { Button_IF_EnableInterrupt(SW3); // // send publish message // sl_ExtLib_MqttClientSend((void*)local_con_conf[iCount].clt_ctx, pub_topic_sw3,data_sw3,strlen((char*)data_sw3),QOS2,RETAIN); UART_PRINT("\n\r CC3200 Publishes the following message \n\r"); UART_PRINT("Topic: %s\n\r",pub_topic_sw3); UART_PRINT("Data: %s\n\r",data_sw3); } else if(BROKER_DISCONNECTION == RecvQue.event) { iConnBroker--; /* Derive the value of the local_con_conf or clt_ctx from the message */ sl_ExtLib_MqttClientCtxDelete(((connect_config*)(RecvQue.hndl))->clt_ctx); if(!IS_CONNECTED(g_ulStatus)) { UART_PRINT("device has disconnected from AP \n\r"); UART_PRINT("retry connection to the AP\n\r"); while(!(IS_CONNECTED(g_ulStatus)) || !(IS_IP_ACQUIRED(g_ulStatus))) { osi_Sleep(10); } goto connect_to_broker; } if(iConnBroker < 1) { // // device not connected to any broker // goto end; } } } end: // // Deinitializating the client library // sl_ExtLib_MqttClientExit(); UART_PRINT("\n\r Exiting the Application\n\r"); LOOP_FOREVER(); } //***************************************************************************** // //! Main //! //! \param none //! //! This function //! 1. Invokes the SLHost task //! 2. Invokes the MqttClient //! //! \return None //! //***************************************************************************** void main() { long lRetVal = -1; // // Initialize the board configurations // BoardInit(); // // Pinmux for UART // PinMuxConfig(); // // Configuring UART // InitTerm(); // // Display Application Banner // DisplayBanner("MQTT_Client"); // // Start the SimpleLink Host // lRetVal = VStartSimpleLinkSpawnTask(SPAWN_TASK_PRIORITY); if(lRetVal < 0) { ERR_PRINT(lRetVal); LOOP_FOREVER(); } // // Start the MQTT Client task // osi_MsgQCreate(&g_PBQueue,"PBQueue",sizeof(event_msg),10); lRetVal = osi_TaskCreate(MqttClient, (const signed char *)"Mqtt Client App", OSI_STACK_SIZE, NULL, 2, NULL ); if(lRetVal < 0) { ERR_PRINT(lRetVal); LOOP_FOREVER(); } // // Start the task scheduler // osi_start(); }
Exiting the Application