Part Number: CC3200
Hello ,
I am testing our new hardware based on cc3200 where i found that the connection to the AP is not always stable comparing to our previous hardware,sometimes i face many 110 error of disconnection and -102 general event sometimes it goes ok and it seems to be more stable when i use .however it is unpredictible and there is no difference between the software used in the old hardware version and the new one the same SDK the same servicepack,it is weird,
-can i say it is rf path problem?if yes why it happens sometimes with high frequence and sometimes it is more stable?
-or can i say it is linked to power rail problem
what are the tests i can do to assert the source of problem
PS : i did RSSI it is close to -25db when it is close to the router
best regards