Other Parts Discussed in Thread: CC3235MODSF, CC3235SF, UNIFLASH, TM4C1294NCPDT
Hi Experts,
I received some inquiries about LAUNCHCC3235MOD.
1. Restoring the factory default image
According to CC3235MODSF SimpleLink With MCU LaunchPad Hardware User Guide (https://www.ti.com/lit/pdf/swru548) "2.2.12 Push-Buttons and LED Indicators", Pressing SW4 and toggling RESET restores the factory default image on the serial flash. Customer tried to do so, however, it does not seem working well. I attached this serial-log(
======================================= out of box Example Ver: 1.00.00.09 ============================================ CHIP: 0x31100019 MAC: 3.1.0.5 PHY: 3.1.0.17 NWP: 4.1.0.27 ROM: 8738 HOST: 3.0.1.45 MAC address: 34:03:de:11:35:51 ============================================ [Provisioning task] Wake up on Power ON ============================================ out of box Example Ver: 1.00.00.09 ============================================ CHIP: 0x31100019 MAC: 3.1.0.5 PHY: 3.1.0.17 NWP: 4.1.0.27 ROM: 8738 HOST: 3.0.1.45 MAC address: 34:03:de:11:35:51 ============================================ [Provisioning task] Wake up on Power ON [Provisioning task] Cannot connect to AP or profile does not exist [Provisioning task] detected device is CC323xSF [NETAPP EVENT] IP Acquired: IP=10.123.45.1 , Gateway=10.123.45.1 [Provisioning task] Device is configured in default state [Provisioning task] Device started in [NETAPP EVENT] IP Acquired: IP=10.123.45.1 , Gateway=10.123.45.1 ============================================ out of box Example Ver: 1.00.00.09 ============================================ CHIP: 0x31100019 MAC: 3.1.0.5 PHY: 3.1.0.17 NWP: 4.1.0.27 ROM: 8738 HOST: 3.0.1.45 MAC address: 34:03:de:11:35:51 ============================================ [Provisioning task] Wake up on Power ON [NETAPP EVENT] IP Acquired: IP=10.123.45.1 , Gateway=10.123.45.1 [Provisioning task] Device started as STATION [Provisioning task] Cannot connect to AP or profile does not exist [Provisioning task] detected device is CC323xSF [NETAPP EVENT] IP Acquired: IP=10.123.45.1 , Gateway=10.123.45.1 [Provisioning task] Device is configured in default state [Provisioning task] Device started in AP role [NETAPP EVENT] IP Acquired: IP=10.123.45.1 , Gateway=10.123.45.1 [Provisioning task] Host Driver Version: 3.0.1.45 [Provisioning task] Build Version 4.1.0.27.31.3.1.0.5.3.1.0.17 [Provisioning task] Starting Provisioning - [Provisioning task] in mode 2 (0 = AP, 1 = SC, 2 = AP+SC) [Provisioning task] Provisioning Started. Waiting to be provisioned..!!
2. The factory default firmware
Customer was looking for the User Manual of the factory default firmware, however, they were not able to reach it. Could you share this information(How-to-use), please?
3. LAUNCHCC3235MOD LAUNCHCC3235MOD
Customer has two type LAUNCHCC3235MOD EVM, one of them is Revision ES2, other is Rev.A.
Regarding Rev.A EVM, we are able to see the schematic(https://www.ti.com/lit/zip/swra633). However, customer would like to know the difference between Rev.A and Rev.ES2. would you elaborate it, please?
4. RSSI
Customer would like to check RSSI. Therefore, customer would like to know what sample-code is better. Can we have your Expert's advice/comments on this please?
Best regards,
Miyazaki