Hi there,
I have a issue about stack size in TIRTOS.
I have several task running, if i changed the stack size in one of the task, it runs and if i roll back to previous stack size. There is a problem in wifi connection.
1. osi_TaskCreate( Wifi_Task, (const signed char*)"Wi-Fi Task", 2048, NULL, 1, NULL ) 2. osi_TaskCreate(T1_Task, "T1_Task", 1024, NULL, 6, NULL) 3. osi_TaskCreate( T2_Task, "T2_Task", 2048, NULL, 1, NULL ); 4. osi_TaskCreate(T3_Task, "T3_Task", 2048, NULL, 10, NULL) 5. osi_TaskCreate(T4_Task, "T4_Task", 2048, NULL, 10, NULL)
If i changed the stack size of T1_Task to 512 then all task works but if i changed back to 1024 then there is no wifi connectivity.
Is there any memory setting for TIRTOS library?