Hi team,
Our customer is developing their system with WL1837MOD(Antenna: W3006, https://productfinder.pulseeng.com/product/W3006). WL1837MOD and W3006 was certified for FCC, IC, ETSI/CE, and Japan MIC(TELEC). Therefore, customer understand that they don't need to re-test RF certification as their system. Is that correct?
They mean, according to the following URL, customer believes their system(WL1837MOD+ W3006) can be used without Re-certification test. For FCC/ETSI region, Customer should only file in each country for certification using the FCC/ETSI reports. Is that correct? it will be appreciated if you will share Expert's advice/comments on this, please?
And then, if there are additional countries which accepts FCC/IC/CE/ETSI/MIC Certification, would you share the latest countries lists, please?
Best regards,
Miyazaki