This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/CC3220SF-LAUNCHXL: SysConfig only one IP Network Service Available

Part Number: CC3220SF-LAUNCHXL
Other Parts Discussed in Thread: SYSCONFIG

Tool/software: Code Composer Studio

Hi All

I have started an empty project and add up MQTT Client functionality to the project.

On empty.syscfg file , I can only see IP NETWORK SERVICES (NS) (1) , only one service available SlNet. Can not see others such as :

Connection Manager

HTTP Client

HTTP Server

MQTT

SNTP

as is shown on example SimpleLink CC32XX (4.30.00.06) / Wi-Fi/WiFi MQTT

I have imported an RTOS empty project , I followed the instructions but not able to see available all Network Services (NS)

All the best 

F Dias