This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3120MOD: AWS MQTT using CC3120MOD and MSP432P1111

Part Number: CC3120MOD
Other Parts Discussed in Thread: CC3120

We need to implement MQTT on a CC3120 with a MSP432P1111.  I downloaded the CC3220 AWS SDK which I plan to migrate to the CC3120.  Has anyone done this before?  Is the SDK up-to-date with AWS?

  • Hi,

    The CC3220 AWS SDK is somewhat out of date with the main AWS SDK - the TI plugin incorporates version 3.0.1 while the latest release is version 3.1.1. That being said, you can still connect with the SDK and use AWS-specific MQTT functionality such as device shadows without issue.

    We do not currently have examples of the AWS SDK running on a MSP432 + CC3120, but it should definitely be doable. I advise you look at the differences between examples present in both the CC31xx plugin and the CC32xx SDK such as the network_terminal example to see what changes should be made when porting a project from CC32xx to MSP432 + CC3120.

    Let me know if you have any issues getting the AWS plugin examples working on the MSP432.

    Regards,

    Michael