Other Parts Discussed in Thread: CC3120, CC3100, UNIFLASH, CC3200
Hello,
I designed an automation system that has both ethernet and WiFi connectivity using the CC3100 WiFi module, TM4C129E MCU, TIVA-TI-RTOS using the NDK and Wifi framework. My system works well and I am pleased by how the overall TIVA TI-RTOS, with NDK and WiFi SDK made development work so convenient. I understand that there are new CC31xx modules in the market, the CC3120 for instance, which, correct me if I am wrong, is a pin to pin replacement for the CC3100. I thought it was also firmware compatible with regards to TIVA TI-RTOS and its WiFi Stack. I just found out (and please correct me if I am wrong) that the current WiFi framework on the TIVA-TIRTOS for the CC3100 doesn't work with the CC3120 or the latest CC31xx modules. Seems like TI is promoting the simplelink SDK to be used on the latest CC31xx modules. The question is, how long will TI be producing the CC3100? Will it be around to stay for the next 5, 10, 15 years? I am worried about its longevity. Furthermore, I would like to avoid switching from the TM4C to another MCU because, aside from the fact that I have already designed a working system, I am really pleased with the TIVA product line and with TI-RTOS TIVA and NDK. In addition, switching to say an MSP432 and learning about the simplelink platform would hold my timeline back. Any thoughts on CC3100 longevity? Is it even worth continuing my current design and bringing it to production?
Any response is much appreciated.
Regards,
AJ