Other Parts Discussed in Thread: UNIFLASH
Dear support,
Based on Application Note "CC3120 Production Line Guide" SWRA569 there are two possibilities to program the exetrnal serial memory connected to CC3120: Direct SPI and UART via Bootloader.
We have decided to program it via "Direct SPI" programming on pins of serial memory. For us this the faster solution since our ISP tool programmer already supports the SPI serial memory.
But we have a problem:
If we readback a programmed board (via UART bootloader) and then with the same content we program a second board via Direct SPI, the second board doesn't work. If we program the first board via Direct SPI it works. It seams that the content depends of the board.. Is it possible? Is this a right behaviour? In case how can we program the memory via Direct SPI using a generic ISP programmer?
Can you also give me the programming specification for UART via bootloader, in case the Direct SPI programming is not possible using a universal ISP programmer like ours WriteNow!
Thanks & Best Regards,
--Pietro Poletto
www.algocraft.com